Microchip® Advanced Software Framework

flashLoader.h File Reference

Declaration api of flash loader.

Copyright (c) 2020 Microchip Technology Inc. and its subsidiaries.

#include <eepromLoader.h>

Macros

#define CMD_KEY   0xA5
 
#define FLASH_MAIN_ADDRESS_SPACE   (0x00)
 
#define FLASH_PAGESIZE   256u
 
#define MCU_EEPROM_START_ADDR   0x3F000
 
#define MCU_PAGE_SIZE   64
 
#define NO_OF_HALF_WORDS_PER_PAGE   32
 
#define NO_OF_PAGES_PER_ROW   4
 
#define PAGE_NUMBER_SHIFT   8
 
#define PAGE_POSITION_OFFSET_MASK   0x000000FF
 
#define ROW_SIZE   (4 * MCU_PAGE_SIZE)
 
#define ROW_SIZE_IN_HALF_WORDS   (ROW_SIZE / 2)
 

Functions

void flashFlushPage (void)
 Flush unloaded data before exit from bootloader. More...
 
void flashPacketToPage (void)
 Load received date to the flash. More...
 
void flashUpdateAppStartAddr (void)
 Updates application start address in end of flash. More...
 
void hwEraseFlashPage (uint32_t pageStartAddress)
 Erases specified flash page. More...
 
void hwFillFlashPageBuffer (uint32_t startOffset, uint16_t length, uint8_t *data)
 Writes data to the page buffer. More...
 
INLINE uint8_t hwFlashRead (uint16_t address)
 Reads byte from EEPROM. More...
 
void hwFlashWriteEepromPage (HW_EepromParams_t *eeprom)
 Writes a page to the EEPROM. More...
 
void hwWriteFlashPage (uint32_t pageStartAddress)
 Writes flash page buffer without erasing. More...
 
void nvm_init (void)
 

Variables

uint32_t appStartAddr
 

#define CMD_KEY   0xA5
#define FLASH_MAIN_ADDRESS_SPACE   (0x00)
#define MCU_EEPROM_START_ADDR   0x3F000

Referenced by hwFlashRead().

#define MCU_PAGE_SIZE   64

Referenced by hwWriteFlashPage().

#define NO_OF_HALF_WORDS_PER_PAGE   32
#define NO_OF_PAGES_PER_ROW   4

Referenced by hwWriteFlashPage().

#define PAGE_NUMBER_SHIFT   8
#define PAGE_POSITION_OFFSET_MASK   0x000000FF

Referenced by flashPacketToPage().

#define ROW_SIZE   (4 * MCU_PAGE_SIZE)
#define ROW_SIZE_IN_HALF_WORDS   (ROW_SIZE / 2)

Referenced by hwFillFlashPageBuffer().

void flashFlushPage ( void  )

Flush unloaded data before exit from bootloader.

References currentPage, FLASH_PAGESIZE, flashUpdateAppStartAddr(), hwEraseFlashPage(), hwFillFlashPageBuffer(), hwWriteFlashPage(), and temporaryPageBuffer.

Referenced by srecProtocol().

void flashUpdateAppStartAddr ( void  )

Updates application start address in end of flash.

References appStartAddr, FLASH_PAGESIZE, hwEraseFlashPage(), hwFillFlashPageBuffer(), hwWriteFlashPage(), and memcpy_P.

Referenced by clear_updateaction(), and flashFlushPage().

void hwEraseFlashPage ( uint32_t  pageStartAddress)

Erases specified flash page.

Parameters
[in]pageStartAddress- address within the target page

References nvm_erase_row().

Referenced by flashFlushPage(), flashPacketToPage(), flashUpdateAppStartAddr(), hwFlashWriteEepromPage(), memcopy(), update_boot_info(), and writeapp_infotable().

void hwFillFlashPageBuffer ( uint32_t  startOffset,
uint16_t  length,
uint8_t *  data 
)

Writes data to the page buffer.

Parameters
[in]startOffset- start position for writing within the page
[in]length- data to write length in bytes
[in]data- pointer to data to write

References pageBufferToFill, ROW_SIZE, and ROW_SIZE_IN_HALF_WORDS.

Referenced by flashFlushPage(), flashPacketToPage(), flashUpdateAppStartAddr(), hwFlashWriteEepromPage(), memcopy(), update_boot_info(), and writeapp_infotable().

INLINE uint8_t hwFlashRead ( uint16_t  address)

Reads byte from EEPROM.

Parameters
[in]address- address of a byte.
Returns
read value.

References MCU_EEPROM_START_ADDR.

Referenced by eepromReadData().

void hwFlashWriteEepromPage ( HW_EepromParams_t eeprom)

Writes a page to the EEPROM.

Parameters
[in]address- address of data byte.
[in]data- data for saving.
[in]length- No of bytes.
[in]address- address of data byte.
[in]data- data for saving.

References HW_EepromParams_t::address, HW_EepromParams_t::data, hwEraseFlashPage(), hwFillFlashPageBuffer(), hwWriteFlashPage(), HW_EepromParams_t::length, memcpy_P, and ROW_SIZE.

Referenced by eepromPacketToPage().

void hwWriteFlashPage ( uint32_t  pageStartAddress)

Writes flash page buffer without erasing.

Parameters
[in]pageStartAddress- address within the target page

References MCU_PAGE_SIZE, NO_OF_PAGES_PER_ROW, nvm_write_buffer(), pageBufferToFill, and ROW_SIZE.

Referenced by flashFlushPage(), flashPacketToPage(), flashUpdateAppStartAddr(), hwFlashWriteEepromPage(), memcopy(), update_boot_info(), and writeapp_infotable().

uint32_t appStartAddr