Microchip® Advanced Software Framework

usart_sam_ba.c File Reference

USART functions for SAM-BA on SAM0.

Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "usart_sam_ba.h"
#include "conf_board.h"
#include "conf_clocks.h"
#include "conf_bootloader.h"

Functions

unsigned short add_crc (char ptr, unsigned short crc)
 Compute the CRC. More...
 
static uint16_t getbytes (uint8_t *ptr_data, uint16_t length)
 
uint8_t getPacket (uint8_t *ptr_data, uint8_t sno)
 Used by Xdown to retrieve packets. More...
 
static int putPacket (uint8_t *tmppkt, uint8_t sno)
 Used by Xup to send packets. More...
 
void usart_close (void)
 Close the given USART. More...
 
int usart_getc (void)
 Waits and gets a value on usart line. More...
 
uint32_t usart_getdata (void *data, uint32_t length)
 Get data from com device. More...
 
uint32_t usart_getdata_xmd (void *data, uint32_t length)
 Called when a transfer from host to target is being made (considered an download). More...
 
bool usart_is_rx_ready (void)
 This function checks if a character has been received on the usart line. More...
 
void usart_open ()
 Open the given USART. More...
 
int usart_putc (int value)
 Puts a byte on usart line The type int is used to support printf redirection from compiler LIB. More...
 
uint32_t usart_putdata (void const *data, uint32_t length)
 Send given data (polling) More...
 
uint32_t usart_putdata_xmd (void const *data, uint32_t length)
 Called when a transfer from target to host is being made(considered an upload). More...
 
int usart_readc (void)
 Gets a value on usart line. More...
 
int usart_sharp_received (void)
 Returns true if the SAM-BA Uart received the sharp char. More...
 

Variables

volatile uint8_t b_sharp_received
 
volatile uint8_t buffer_rx_usart [USART_BUFFER_SIZE]
 
volatile uint8_t buffer_tx_usart [USART_BUFFER_SIZE]
 
uint8_t error_timeout
 
volatile uint8_t idx_rx_read
 
volatile uint8_t idx_rx_write
 
volatile uint8_t idx_tx_read
 
volatile uint8_t idx_tx_write
 
uint8_t mode_of_transfer
 
uint16_t size_of_data
 
struct usart_module usart_sam_ba
 

unsigned short add_crc ( char  ptr,
unsigned short  crc 
)

Compute the CRC.

Gets data from usart line using Xmodem protocol.

References CRC16POLY.

Referenced by getbytes(), and putPacket().

static uint16_t getbytes ( uint8_t *  ptr_data,
uint16_t  length 
)
static
uint8_t getPacket ( uint8_t *  ptr_data,
uint8_t  sno 
)

Used by Xdown to retrieve packets.

References ACK, CAN, error_timeout, getbytes(), PKTLEN_128, usart_getc(), and usart_putc().

Referenced by usart_getdata_xmd().

static int putPacket ( uint8_t *  tmppkt,
uint8_t  sno 
)
static

Used by Xup to send packets.

References add_crc(), data, i, mode_of_transfer, PKTLEN_128, size_of_data, SOH, usart_getc(), and usart_putc().

Referenced by usart_putdata_xmd().

void usart_close ( void  )

Close the given USART.

Stops the USART.

References usart_disable(), usart_disable_transceiver(), usart_sam_ba, USART_TRANSCEIVER_RX, and USART_TRANSCEIVER_TX.

int usart_getc ( void  )

Waits and gets a value on usart line.

Returns
value read on usart line

References usart_is_rx_ready(), usart_read_wait(), and usart_sam_ba.

Referenced by getbytes(), getPacket(), putPacket(), usart_getdata(), usart_getdata_xmd(), usart_putdata_xmd(), and usart_sharp_received().

uint32_t usart_getdata ( void *  data,
uint32_t  length 
)

Get data from com device.

Gets data from usart line.

References usart_getc().

uint32_t usart_getdata_xmd ( void *  data,
uint32_t  length 
)

Called when a transfer from host to target is being made (considered an download).

Gets data from usart line using Xmodem protocol.

References ACK, b_run, CAN, EOT, error_timeout, ESC, getPacket(), length, mode_of_transfer, PKTLEN_128, ptr_data, size_of_data, SOH, system_clock_source_get_hz(), usart_getc(), usart_is_rx_ready(), and usart_putc().

bool usart_is_rx_ready ( void  )

This function checks if a character has been received on the usart line.

Returns
1 if a byte is ready to be read.

Referenced by usart_getc(), usart_getdata_xmd(), and usart_sharp_received().

int usart_putc ( int  value)

Puts a byte on usart line The type int is used to support printf redirection from compiler LIB.

Puts a byte on usart line.

Parameters
valueValue to put
Returns
1 if function was successfully done, otherwise 0.

References usart_sam_ba, and usart_write_wait().

Referenced by getPacket(), putPacket(), usart_getdata_xmd(), usart_putdata(), and usart_putdata_xmd().

uint32_t usart_putdata ( void const *  data,
uint32_t  length 
)

Send given data (polling)

Send buffer on usart line.

References i, length, and usart_putc().

uint32_t usart_putdata_xmd ( void const *  data,
uint32_t  length 
)

Called when a transfer from target to host is being made(considered an upload).

Send buffer on usart line using Xmodem protocol.

References ACK, CAN, EOT, error_timeout, length, mode_of_transfer, NAK, PKTLEN_128, ptr_data, putPacket(), size_of_data, usart_getc(), and usart_putc().

int usart_readc ( void  )

Gets a value on usart line.

Returns
value read on usart line

References buffer_rx_usart, idx_rx_read, and USART_BUFFER_SIZE.

int usart_sharp_received ( void  )

Returns true if the SAM-BA Uart received the sharp char.

Returns
Returns true if the SAM-BA Uart received the sharp char

References SHARP_CHARACTER, usart_getc(), and usart_is_rx_ready().

Referenced by main().

volatile uint8_t b_sharp_received

Referenced by usart_open().

volatile uint8_t buffer_rx_usart[USART_BUFFER_SIZE]

Referenced by usart_readc().

volatile uint8_t buffer_tx_usart[USART_BUFFER_SIZE]
uint8_t error_timeout
volatile uint8_t idx_rx_read

Referenced by usart_open(), and usart_readc().

volatile uint8_t idx_rx_write

Referenced by usart_open().

volatile uint8_t idx_tx_read

Referenced by usart_open().

volatile uint8_t idx_tx_write

Referenced by usart_open().

uint8_t mode_of_transfer
uint16_t size_of_data
struct usart_module usart_sam_ba