WINC1500 AP Scan Example.
Copyright (c) 2020 Microchip Technology Inc. and its subsidiaries.
#include "asf.h"
#include "main.h"
#include "driver/include/m2m_wifi.h"
#include "driver/source/nmasic.h"
Macros | |
#define | STRING_EOL "\r\n" |
#define | STRING_HEADER |
Functions | |
static void | configure_console (void) |
Configure UART console. More... | |
int | main (void) |
Main application function. More... | |
static void | wifi_cb (uint8_t u8MsgType, void *pvMsg) |
Callback to get the Wi-Fi status update. More... | |
Variables | |
static struct usart_module | cdc_uart_module |
UART module for debug. More... | |
static uint8_t | num_founded_ap = 0 |
Number of APs found. More... | |
static uint8_t | scan_request_index = 0 |
Index of scan list to request scan result. More... | |
#define STRING_EOL "\r\n" |
#define STRING_HEADER |
Referenced by main().
|
static |
Configure UART console.
References usart_config::baudrate, cdc_uart_module, usart_config::mux_setting, usart_config::pinmux_pad0, usart_config::pinmux_pad1, usart_config::pinmux_pad2, usart_config::pinmux_pad3, usart_enable(), and usart_get_config_defaults().
Referenced by main().
int main | ( | void | ) |
Main application function.
Application entry point.
References configure_console(), M2M_SUCCESS, M2M_WIFI_CH_ALL, m2m_wifi_handle_events(), m2m_wifi_init(), m2m_wifi_request_scan(), nm_bsp_init(), NULL, tstrWifiInitParam::pfAppWifiCb, STRING_HEADER, system_init(), and wifi_cb().
|
static |
Callback to get the Wi-Fi status update.
[in] | u8MsgType | type of Wi-Fi notification. Possible types are: |
[in] | pvMsg | A pointer to a buffer containing the notification parameters (if any). It should be casted to the correct data type corresponding to the notification type. |
References tstrM2mWifiscanResult::au8SSID, M2M_WIFI_CH_ALL, m2m_wifi_connect(), M2M_WIFI_CONNECTED, M2M_WIFI_DISCONNECTED, m2m_wifi_get_num_ap_found(), M2M_WIFI_REQ_DHCP_CONF, m2m_wifi_req_scan_result(), m2m_wifi_request_dhcp_client(), m2m_wifi_request_scan(), M2M_WIFI_RESP_CON_STATE_CHANGED, M2M_WIFI_RESP_SCAN_DONE, M2M_WIFI_RESP_SCAN_RESULT, MAIN_WLAN_AUTH, MAIN_WLAN_PSK, MAIN_WLAN_SSID, num_founded_ap, scan_request_index, tstrM2mWifiStateChanged::u8CurrState, and tstrM2mScanDone::u8NumofCh.
Referenced by main().
|
static |
UART module for debug.
|
static |
Number of APs found.
Referenced by wifi_cb().
|
static |
Index of scan list to request scan result.
Referenced by wifi_cb().