Driver for the Static Memory Controller.
It provides functions for configuring and using the on-chip SMC.
Macros | |
#define | ECC_STATUS_MASK 0x07 |
#define | NFC_BUSY_FLAG 0x8000000 |
#define | NFCADDR_CMD_ACYCLE (0x7u << 19) /* Number of Address required for the current command */ |
#define | NFCADDR_CMD_ACYCLE_FIVE (0x5u << 19) /* Five address cycles */ |
#define | NFCADDR_CMD_ACYCLE_FOUR (0x4u << 19) /* Four address cycles */ |
#define | NFCADDR_CMD_ACYCLE_NONE (0x0u << 19) /* No address cycle */ |
#define | NFCADDR_CMD_ACYCLE_ONE (0x1u << 19) /* One address cycle */ |
#define | NFCADDR_CMD_ACYCLE_THREE (0x3u << 19) /* Three address cycles */ |
#define | NFCADDR_CMD_ACYCLE_TWO (0x2u << 19) /* Two address cycles */ |
#define | NFCADDR_CMD_CMD1 (0xFFu << 2) /* Command Register Value for Cycle 1 */ |
#define | NFCADDR_CMD_CMD2 (0xFFu << 10) /* Command Register Value for Cycle 2 */ |
#define | NFCADDR_CMD_CSID(value) ((NFCADDR_CMD_CSID_Msk & ((value) << NFCADDR_CMD_CSID_Pos))) |
#define | NFCADDR_CMD_CSID_Msk (0x7u << NFCADDR_CMD_CSID_Pos) /* Chip Select Identifier */ |
#define | NFCADDR_CMD_CSID_Pos 22 |
#define | NFCADDR_CMD_NFC_READ (0x0u << 26) /* NFC Write Enable */ |
#define | NFCADDR_CMD_NFC_WIRTE (0x1u << 26) /* NFC Write Enable */ |
#define | NFCADDR_CMD_NFCCMD (0x1u << 27) /* NFC Command Enable */ |
#define | NFCADDR_CMD_NFCEN (0x1u << 25) /* NFC Enable */ |
#define | NFCADDR_CMD_VCMD2 (0x1u << 18) /* Valid Cycle 2 Command */ |
Functions | |
uint32_t | smc_ecc_get_status (Smc *p_smc, uint32_t ul_parity_number) |
Get ECC status by giving ecc number. More... | |
void | smc_ecc_get_value (Smc *p_smc, uint32_t *p_ecc) |
Get all ECC parity registers value. More... | |
void | smc_ecc_init (Smc *p_smc, uint32_t ul_type, uint32_t ul_pagesize) |
Initialize ECC mode. More... | |
void | smc_enable_writeprotect (Smc *p_smc, uint32_t ul_enable) |
Set write protection of SMC registers. More... | |
uint32_t | smc_get_mode (Smc *p_smc, uint32_t ul_cs) |
Get the SMC mode of the specified Chip Select. More... | |
uint32_t | smc_get_writeprotect_status (Smc *p_smc) |
Get the status of SMC write protection register. More... | |
void | smc_nfc_disable (Smc *p_smc) |
Disable NFC controller. More... | |
void | smc_nfc_disable_interrupt (Smc *p_smc, uint32_t ul_sources) |
Disable SMC interrupts. More... | |
void | smc_nfc_disable_spare_read (Smc *p_smc) |
Prevent NFC controller from reading the spare area in read mode. More... | |
void | smc_nfc_disable_spare_write (Smc *p_smc) |
Prevent NFC controller from writing the spare area in read mode. More... | |
void | smc_nfc_enable (Smc *p_smc) |
Enable NFC controller. More... | |
void | smc_nfc_enable_interrupt (Smc *p_smc, uint32_t ul_sources) |
Enable SMC interrupts. More... | |
void | smc_nfc_enable_spare_read (Smc *p_smc) |
Enable NFC controller to read both main and spare area in read mode. More... | |
void | smc_nfc_enable_spare_write (Smc *p_smc) |
Enable NFC controller to write both main and spare area in write mode. More... | |
uint32_t | smc_nfc_get_interrupt_mask (Smc *p_smc) |
Get the interrupt mask. More... | |
uint32_t | smc_nfc_get_status (Smc *p_smc) |
Get the NFC Status. More... | |
void | smc_nfc_init (Smc *p_smc, uint32_t ul_config) |
Initialize NFC configuration. More... | |
void | smc_nfc_send_command (Smc *p_smc, uint32_t ul_cmd, uint32_t ul_address_cycle, uint32_t ul_cycle0) |
Use the HOST nandflash controller to send a command. More... | |
void | smc_nfc_set_address0 (Smc *p_smc, uint8_t uc_address0) |
Set flash cycle 0 address. More... | |
void | smc_nfc_set_bank (Smc *p_smc, uint32_t ul_bank) |
Set NFC sram bank. More... | |
void | smc_nfc_set_page_size (Smc *p_smc, uint32_t ul_page_size) |
Set NFC page size. More... | |
void | smc_set_cycle_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_cycle_timing) |
Configure the SMC cycle timing for the specified Chip Select. More... | |
void | smc_set_mode (Smc *p_smc, uint32_t ul_cs, uint32_t ul_mode) |
Configure the SMC mode for the specified Chip Select. More... | |
void | smc_set_nand_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_nand_timing) |
Configure the SMC nand timing for the specified Chip Select. More... | |
void | smc_set_pulse_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_pulse_timing) |
Configure the SMC pulse timing for the specified Chip Select. More... | |
void | smc_set_setup_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_setup_timing) |
Configure the SMC Setup timing for the specified Chip Select. More... | |
#define ECC_STATUS_MASK 0x07 |
Referenced by smc_ecc_get_status().
#define NFC_BUSY_FLAG 0x8000000 |
Referenced by smc_nfc_send_command().
#define NFCADDR_CMD_ACYCLE (0x7u << 19) /* Number of Address required for the current command */ |
#define NFCADDR_CMD_ACYCLE_FIVE (0x5u << 19) /* Five address cycles */ |
#define NFCADDR_CMD_ACYCLE_FOUR (0x4u << 19) /* Four address cycles */ |
#define NFCADDR_CMD_ACYCLE_NONE (0x0u << 19) /* No address cycle */ |
#define NFCADDR_CMD_ACYCLE_ONE (0x1u << 19) /* One address cycle */ |
#define NFCADDR_CMD_ACYCLE_THREE (0x3u << 19) /* Three address cycles */ |
#define NFCADDR_CMD_ACYCLE_TWO (0x2u << 19) /* Two address cycles */ |
#define NFCADDR_CMD_CMD1 (0xFFu << 2) /* Command Register Value for Cycle 1 */ |
#define NFCADDR_CMD_CMD2 (0xFFu << 10) /* Command Register Value for Cycle 2 */ |
#define NFCADDR_CMD_CSID | ( | value | ) | ((NFCADDR_CMD_CSID_Msk & ((value) << NFCADDR_CMD_CSID_Pos))) |
#define NFCADDR_CMD_CSID_Msk (0x7u << NFCADDR_CMD_CSID_Pos) /* Chip Select Identifier */ |
#define NFCADDR_CMD_CSID_Pos 22 |
#define NFCADDR_CMD_NFC_READ (0x0u << 26) /* NFC Write Enable */ |
#define NFCADDR_CMD_NFC_WIRTE (0x1u << 26) /* NFC Write Enable */ |
#define NFCADDR_CMD_NFCCMD (0x1u << 27) /* NFC Command Enable */ |
Referenced by smc_nfc_send_command().
#define NFCADDR_CMD_NFCEN (0x1u << 25) /* NFC Enable */ |
#define NFCADDR_CMD_VCMD2 (0x1u << 18) /* Valid Cycle 2 Command */ |
uint32_t smc_ecc_get_status | ( | Smc * | p_smc, |
uint32_t | ul_parity_number | ||
) |
Get ECC status by giving ecc number.
p_smc | Pointer to an SMC instance. |
ul_parity_number | ECC parity number from 0 to 15. |
References ECC_STATUS_MASK, and status.
void smc_ecc_get_value | ( | Smc * | p_smc, |
uint32_t * | p_ecc | ||
) |
Get all ECC parity registers value.
p_smc | Pointer to an SMC instance. |
p_ecc | Pointer to a parity buffer. |
void smc_ecc_init | ( | Smc * | p_smc, |
uint32_t | ul_type, | ||
uint32_t | ul_pagesize | ||
) |
Initialize ECC mode.
p_smc | Pointer to an SMC instance. |
ul_type | Type of correction, use pattern defined in the device header file. |
ul_pagesize | Page size of NAND Flash device, use pattern defined in the device header file. |
void smc_enable_writeprotect | ( | Smc * | p_smc, |
uint32_t | ul_enable | ||
) |
Set write protection of SMC registers.
p_smc | Pointer to an SMC instance. |
ul_enable | 1 to enable, 0 to disable. |
References SMC_WPKEY_VALUE.
uint32_t smc_get_mode | ( | Smc * | p_smc, |
uint32_t | ul_cs | ||
) |
Get the SMC mode of the specified Chip Select.
p_smc | Pointer to an SMC instance. |
ul_cs | Chip select number to be set. |
uint32_t smc_get_writeprotect_status | ( | Smc * | p_smc | ) |
Get the status of SMC write protection register.
p_smc | Pointer to an SMC instance. |
void smc_nfc_disable | ( | Smc * | p_smc | ) |
Disable NFC controller.
p_smc | Pointer to an SMC instance. |
void smc_nfc_disable_interrupt | ( | Smc * | p_smc, |
uint32_t | ul_sources | ||
) |
Disable SMC interrupts.
p_smc | Pointer to an SMC instance. |
ul_sources | Interrupt source bitmap. |
void smc_nfc_disable_spare_read | ( | Smc * | p_smc | ) |
Prevent NFC controller from reading the spare area in read mode.
p_smc | Pointer to an SMC instance. |
void smc_nfc_disable_spare_write | ( | Smc * | p_smc | ) |
Prevent NFC controller from writing the spare area in read mode.
p_smc | Pointer to an SMC instance. |
void smc_nfc_enable | ( | Smc * | p_smc | ) |
Enable NFC controller.
p_smc | Pointer to an SMC instance. |
void smc_nfc_enable_interrupt | ( | Smc * | p_smc, |
uint32_t | ul_sources | ||
) |
Enable SMC interrupts.
p_smc | Pointer to an SMC instance. |
ul_sources | Interrupt source bitmap. |
void smc_nfc_enable_spare_read | ( | Smc * | p_smc | ) |
Enable NFC controller to read both main and spare area in read mode.
p_smc | Pointer to an SMC instance. |
void smc_nfc_enable_spare_write | ( | Smc * | p_smc | ) |
Enable NFC controller to write both main and spare area in write mode.
p_smc | Pointer to an SMC instance. |
uint32_t smc_nfc_get_interrupt_mask | ( | Smc * | p_smc | ) |
Get the interrupt mask.
p_smc | Pointer to an SMC instance. |
uint32_t smc_nfc_get_status | ( | Smc * | p_smc | ) |
Get the NFC Status.
p_smc | Pointer to an SMC instance. |
void smc_nfc_init | ( | Smc * | p_smc, |
uint32_t | ul_config | ||
) |
Initialize NFC configuration.
p_smc | Pointer to an SMC instance. |
ul_config | SMC NFC Configuration. |
void smc_nfc_send_command | ( | Smc * | p_smc, |
uint32_t | ul_cmd, | ||
uint32_t | ul_address_cycle, | ||
uint32_t | ul_cycle0 | ||
) |
Use the HOST nandflash controller to send a command.
p_smc | Pointer to an SMC instance. |
ul_cmd | Command to send. |
ul_address_cycle | Address cycle when command access is decoded. |
ul_cycle0 | Address at first cycle. |
References BOARD_NF_DATA_ADDR, NFC_BUSY_FLAG, and NFCADDR_CMD_NFCCMD.
void smc_nfc_set_address0 | ( | Smc * | p_smc, |
uint8_t | uc_address0 | ||
) |
Set flash cycle 0 address.
p_smc | Pointer to an SMC instance. |
uc_address0 | Address cycle 0 in 5 address cycles. |
void smc_nfc_set_bank | ( | Smc * | p_smc, |
uint32_t | ul_bank | ||
) |
Set NFC sram bank.
p_smc | Pointer to an SMC instance. |
ul_bank | NFC sram bank. |
void smc_nfc_set_page_size | ( | Smc * | p_smc, |
uint32_t | ul_page_size | ||
) |
Set NFC page size.
p_smc | Pointer to an SMC instance. |
ul_page_size | Use pattern defined in the device header file. |
void smc_set_cycle_timing | ( | Smc * | p_smc, |
uint32_t | ul_cs, | ||
uint32_t | ul_cycle_timing | ||
) |
Configure the SMC cycle timing for the specified Chip Select.
p_smc | Pointer to an SMC instance. |
ul_cs | Chip Select number to be set. |
ul_cycle_timing | Cycle timing for NWE and NRD. |
Referenced by gfx_init().
void smc_set_mode | ( | Smc * | p_smc, |
uint32_t | ul_cs, | ||
uint32_t | ul_mode | ||
) |
Configure the SMC mode for the specified Chip Select.
p_smc | Pointer to an SMC instance. |
ul_cs | Chip select number to be set. |
ul_mode | SMC mode. |
Referenced by gfx_init().
void smc_set_nand_timing | ( | Smc * | p_smc, |
uint32_t | ul_cs, | ||
uint32_t | ul_nand_timing | ||
) |
Configure the SMC nand timing for the specified Chip Select.
p_smc | Pointer to an SMC instance. |
ul_cs | Chip Select number to be set. |
ul_nand_timing | nand timing for related signal. |
void smc_set_pulse_timing | ( | Smc * | p_smc, |
uint32_t | ul_cs, | ||
uint32_t | ul_pulse_timing | ||
) |
Configure the SMC pulse timing for the specified Chip Select.
p_smc | Pointer to an SMC instance. |
ul_cs | Chip Select number to be set. |
ul_pulse_timing | Pulse timing for NWE,NCS,NRD. |
Referenced by gfx_init().
void smc_set_setup_timing | ( | Smc * | p_smc, |
uint32_t | ul_cs, | ||
uint32_t | ul_setup_timing | ||
) |
Configure the SMC Setup timing for the specified Chip Select.
p_smc | Pointer to an SMC instance. |
ul_cs | Chip Select number to be set. |
ul_setup_timing | Setup timing for NWE, NCS, NRD. |
Referenced by gfx_init().