AVR477 is a Unique reference design with true integration of RF, Touch & MEMS
This application is targeted for the ATmega128RFA1 MCU on the AVR477 Touch Remote Control board.
For the Demo scenario,a Target application that sends QDebug Data,received over air, to QTouch Studio is used. Target Application can be run on the ATUC3A3256S MCU RZ600 board or on the ATmega128RFA1 MCU on the Sensor Terminal Board,when used along with the QT600.
This software was written for the GNU GCC,IAR for AVR,IAR for AVR32.
Supported Versions : AVR Studio 4,AVR Studio 5,IAR for AVR 6.10,IAR for AVR32 4.10 or higher.
Other compilers may or may not work.
For further information, visit Atmel AVR.
Support and FAQ: https://www.microchip.com/support/