Microchip® Advanced Software Framework

pal_mcu_generic.h File Reference

PAL configuration generic for ATmega128RFA1.

This header file contains generic configuration parameters for ATmega128RFA1.

Id:
pal_mcu_generic.h 22792 2010-08-09 06:22:00Z uwalter
Author
Microchip Technology Inc: http://www.microchip.com
Support: https://www.microchip.com/support/
#include "pal_types.h"
#include <string.h>

Macros

#define _pal_trx_bit_read(addr, mask, pos)   (((*(volatile uint8_t *)(addr)) & (mask)) >> (pos))
 
#define _pal_trx_bit_write(addr, mask, pos, val)
 
#define CLEAR_TRX_IRQ_AMI()   (IRQ_STATUS = _BV(AMI))
 Clear AMI interrupt. More...
 
#define CLEAR_TRX_IRQ_AWAKE()   (IRQ_STATUS = _BV(AWAKE))
 Clear TRX AWAKE interrupt. More...
 
#define CLEAR_TRX_IRQ_BATMON()   (BATMON = _BV(BAT_LOW))
 Clear TRX BAT LOW interrupt. More...
 
#define CLEAR_TRX_IRQ_CCA_ED()   (IRQ_STATUS = _BV(CCA_ED_DONE_EN))
 Clear TRX CCA_ED_DONE interrupt. More...
 
#define CLEAR_TRX_IRQ_PLL_LOCK()   (IRQ_STATUS = _BV(PLL_LOCK))
 Clear TRX PLL LOCK interrupt. More...
 
#define CLEAR_TRX_IRQ_PLL_UNLOCK()   (IRQ_STATUS = _BV(PLL_UNLOCK))
 Clear TRX PLL UNLOCK interrupt. More...
 
#define CLEAR_TRX_IRQ_RX_END()   (IRQ_STATUS = _BV(RX_END))
 Clear TRX RX_END interrupt. More...
 
#define CLEAR_TRX_IRQ_TSTAMP()   (IRQ_STATUS = _BV(RX_START))
 Clear RX TIME STAMP interrupt. More...
 
#define CLEAR_TRX_IRQ_TX_END()   (IRQ_STATUS = _BV(TX_END))
 Clears TRX TX_END interrupt. More...
 
#define DISABLE_GLOBAL_IRQ()   cli()
 Disables the global interrupts. More...
 
#define ENABLE_GLOBAL_IRQ()   sei()
 Enables the global interrupts. More...
 
#define ENTER_CRITICAL_REGION()   {uint8_t sreg = SREG; cli()
 This macro saves the global interrupt status. More...
 
#define LEAVE_CRITICAL_REGION()   SREG = sreg;}
 This macro restores the global interrupt status. More...
 
#define MAX_NO_OF_TIMERS   (25)
 Maximum numbers of software timers running at a time. More...
 
#define MAX_TIMEOUT   (0x7FFFFFFF)
 The largest timeout in microseconds. More...
 
#define MIN_TIMEOUT   (0x80)
 The smallest timeout in microseconds. More...
 
#define pal_trx_bit_read(arg)   _pal_trx_bit_read(arg)
 Subregister read. More...
 
#define pal_trx_bit_write(arg1, val)   _pal_trx_bit_write(arg1, val)
 Subregister write. More...
 
#define pal_trx_frame_read(data, length)   memcpy((data), (void *)&TRXFBST, (length))
 Reads frame buffer of the transceiver. More...
 
#define pal_trx_frame_write(data, length)   memcpy((void *)&TRXFBST, (data), (length))
 Writes data into frame buffer of the transceiver. More...
 
#define pal_trx_reg_read(addr)   (*(volatile uint8_t *)(addr))
 Reads current value from a transceiver register. More...
 
#define pal_trx_reg_write(addr, data)   (*(volatile uint8_t *)(addr)) = (data)
 Writes data into a transceiver register. More...
 
#define RST_HIGH()   (TRXPR |= _BV(TRXRST))
 Set Reset Bit. More...
 
#define RST_LOW()   (TRXPR &= ~_BV(TRXRST))
 Clear Reset Bit. More...
 
#define SLP_TR_HIGH()   (TRXPR |= _BV(SLPTR))
 Set Sleep/TR Bit. More...
 
#define SLP_TR_LOW()   (TRXPR &= ~_BV(SLPTR))
 Clear Sleep/TR Bit. More...
 

Typedefs

typedef enum
port_pin_direction_type_tag 
port_pin_direction_type_t
 Enumerations used to identify port directions Note: ports A and C are not present on the ATmega128RFA1. More...
 
typedef enum port_type_tag port_type_t
 Enumerations used to identify ports Note: ports A and C are not present on the ATmega128RFA1. More...
 

Enumerations

enum  port_pin_direction_type_tag {
  DDR_B,
  DDR_D,
  DDR_E,
  DDR_F,
  DDR_G
}
 Enumerations used to identify port directions Note: ports A and C are not present on the ATmega128RFA1. More...
 
enum  port_type_tag {
  PORT_B,
  PORT_D,
  PORT_E,
  PORT_F,
  PORT_G
}
 Enumerations used to identify ports Note: ports A and C are not present on the ATmega128RFA1. More...
 

#define _pal_trx_bit_read (   addr,
  mask,
  pos 
)    (((*(volatile uint8_t *)(addr)) & (mask)) >> (pos))
#define _pal_trx_bit_write (   addr,
  mask,
  pos,
  val 
)
Value:
do { \
(*(volatile uint8_t *)(addr)) = \
((*(volatile uint8_t *)(addr)) & ~(mask)) | \
(((val) << (pos)) & (mask)); \
} while (0)
#define CLEAR_TRX_IRQ_AMI ( )    (IRQ_STATUS = _BV(AMI))

Clear AMI interrupt.

#define CLEAR_TRX_IRQ_AWAKE ( )    (IRQ_STATUS = _BV(AWAKE))

Clear TRX AWAKE interrupt.

#define CLEAR_TRX_IRQ_BATMON ( )    (BATMON = _BV(BAT_LOW))

Clear TRX BAT LOW interrupt.

#define CLEAR_TRX_IRQ_CCA_ED ( )    (IRQ_STATUS = _BV(CCA_ED_DONE_EN))

Clear TRX CCA_ED_DONE interrupt.

#define CLEAR_TRX_IRQ_PLL_LOCK ( )    (IRQ_STATUS = _BV(PLL_LOCK))

Clear TRX PLL LOCK interrupt.

#define CLEAR_TRX_IRQ_PLL_UNLOCK ( )    (IRQ_STATUS = _BV(PLL_UNLOCK))

Clear TRX PLL UNLOCK interrupt.

#define CLEAR_TRX_IRQ_RX_END ( )    (IRQ_STATUS = _BV(RX_END))

Clear TRX RX_END interrupt.

#define CLEAR_TRX_IRQ_TSTAMP ( )    (IRQ_STATUS = _BV(RX_START))

Clear RX TIME STAMP interrupt.

#define CLEAR_TRX_IRQ_TX_END ( )    (IRQ_STATUS = _BV(TX_END))

Clears TRX TX_END interrupt.

#define DISABLE_GLOBAL_IRQ ( )    cli()

Disables the global interrupts.

Referenced by pal_global_irq_disable().

#define ENABLE_GLOBAL_IRQ ( )    sei()

Enables the global interrupts.

Referenced by pal_global_irq_enable().

#define ENTER_CRITICAL_REGION ( )    {uint8_t sreg = SREG; cli()

This macro saves the global interrupt status.

#define LEAVE_CRITICAL_REGION ( )    SREG = sreg;}

This macro restores the global interrupt status.

#define MAX_NO_OF_TIMERS   (25)

Maximum numbers of software timers running at a time.

#define MAX_TIMEOUT   (0x7FFFFFFF)

The largest timeout in microseconds.

#define MIN_TIMEOUT   (0x80)

The smallest timeout in microseconds.

#define pal_trx_bit_read (   arg)    _pal_trx_bit_read(arg)

Subregister read.

Parameters
argSubregister
Returns
Value of the read subregister
#define pal_trx_bit_write (   arg1,
  val 
)    _pal_trx_bit_write(arg1, val)

Subregister write.

Parameters
[in]arg1Subregister
[out]valData, which is muxed into the register
#define pal_trx_frame_read (   data,
  length 
)    memcpy((data), (void *)&TRXFBST, (length))

Reads frame buffer of the transceiver.

This macro reads the frame buffer of the transceiver.

Parameters
[out]dataPointer to the location to store frame
[in]lengthNumber of bytes to be read from the frame buffer.
#define pal_trx_frame_write (   data,
  length 
)    memcpy((void *)&TRXFBST, (data), (length))

Writes data into frame buffer of the transceiver.

This macro writes data into the frame buffer of the transceiver

Parameters
[in]dataPointer to data to be written into frame buffer
[in]lengthNumber of bytes to be written into frame buffer
#define pal_trx_reg_read (   addr)    (*(volatile uint8_t *)(addr))

Reads current value from a transceiver register.

This macro reads the current value from a transceiver register.

Parameters
addrSpecifies the address of the trx register from which the data shall be read
Returns
value of the register read
#define pal_trx_reg_write (   addr,
  data 
)    (*(volatile uint8_t *)(addr)) = (data)

Writes data into a transceiver register.

This macro writes a value into transceiver register.

Parameters
addrAddress of the trx register
dataData to be written to trx register
#define RST_HIGH ( )    (TRXPR |= _BV(TRXRST))

Set Reset Bit.

#define RST_LOW ( )    (TRXPR &= ~_BV(TRXRST))

Clear Reset Bit.

#define SLP_TR_HIGH ( )    (TRXPR |= _BV(SLPTR))

Set Sleep/TR Bit.

#define SLP_TR_LOW ( )    (TRXPR &= ~_BV(SLPTR))

Clear Sleep/TR Bit.

Enumerations used to identify port directions Note: ports A and C are not present on the ATmega128RFA1.

typedef enum port_type_tag port_type_t

Enumerations used to identify ports Note: ports A and C are not present on the ATmega128RFA1.

Enumerations used to identify port directions Note: ports A and C are not present on the ATmega128RFA1.

Enumerator
DDR_B 
DDR_D 
DDR_E 
DDR_F 
DDR_G 

Enumerations used to identify ports Note: ports A and C are not present on the ATmega128RFA1.

Enumerator
PORT_B 
PORT_D 
PORT_E 
PORT_F 
PORT_G