Declarations of API functions to access vendor specific data functionality.
Data Structures | |
struct | fw_data_frame_tag |
Structure handling firmware data frames. More... | |
Macros | |
#define | MAX_NWK_VENDOR_DATA_SIZE 90 |
The maximum size of a vendor-specific data frame; i.e. More... | |
Typedefs | |
typedef struct fw_data_frame_tag | fw_data_frame_t |
Structure handling firmware data frames. More... | |
typedef enum vendor_cmd_id_tag | vendor_cmd_id_t |
Enum Ids for vendor-specific commands. More... | |
typedef enum vendor_status_tag | vendor_status_t |
Enum Ids for vendor status code. More... | |
Enumerations | |
enum | vendor_cmd_id_tag { BATTERY_STATUS_REQ, BATTERY_STATUS_RESP, ALIVE_REQ, ALIVE_RESP, FW_VERSION_REQ, FW_VERSION_RESP, RX_ON_REQ, RX_ON_RESP, FW_DATA_REQ, FW_DATA_RESP, FW_SWAP_REQ, FW_SWAP_RESP } |
Enum Ids for vendor-specific commands. More... | |
enum | vendor_status_tag { VD_SUCCESS, VD_NOT_SUPPORTED_ATTRIBUTE, VD_UNSUPPORTED_SIZE, VD_INVALID_CHECKSUM } |
Enum Ids for vendor status code. More... | |
Functions | |
void | vendor_app_alive_req (void) |
Vendor data alive request. More... | |
void | vendor_data_confirm (nwk_enum_t Status, uint8_t PairingRef) |
Vendor data confirm. More... | |
void | vendor_data_ind (uint8_t PairingRef, profile_id_t ProfileId, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags) |
Vendor data indication. More... | |
bool | vendor_data_request (uint8_t PairingRef, profile_id_t ProfileId, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t TxOptions) |
Vendor data request. More... | |
#define MAX_NWK_VENDOR_DATA_SIZE 90 |
The maximum size of a vendor-specific data frame; i.e.
maximum MSDU - header and footer overhead: aMxMACSafePayloadSize - 12
typedef struct fw_data_frame_tag fw_data_frame_t |
Structure handling firmware data frames.
typedef enum vendor_cmd_id_tag vendor_cmd_id_t |
Enum Ids for vendor-specific commands.
typedef enum vendor_status_tag vendor_status_t |
Enum Ids for vendor status code.
enum vendor_cmd_id_tag |
enum vendor_status_tag |
void vendor_app_alive_req | ( | void | ) |
Vendor data alive request.
Hook for the application indicating that an alive request command was received.
void vendor_data_confirm | ( | nwk_enum_t | Status, |
uint8_t | PairingRef | ||
) |
Vendor data confirm.
Callback function indicating status of the request
Status | Status of the request |
PairingRef | Pairing reference used for the transmission |
Vendor data confirm.
status | nwk status (constants defined by nwk layer) |
PairingRef | Pairing reference |
References UNUSED.
void vendor_data_ind | ( | uint8_t | PairingRef, |
profile_id_t | ProfileId, | ||
uint16_t | VendorId, | ||
uint8_t | nsduLength, | ||
uint8_t * | nsdu, | ||
uint8_t | RxLinkQuality, | ||
uint8_t | RxFlags | ||
) |
Vendor data indication.
Callback function indicating incoming vendor data.
PairingRef | Pairing reference of the sender |
ProfileId | Profile id used for the transmission |
VendorId | Vendor id used for the transmission |
nsduLength | Length of the payload data |
nsdu | Pointer to the payload data |
RxLinkQuality | LQI of the incoming frame |
RxFlags | Options used for transmission |
Vendor data indication.
PairingRef | Pairing reference |
ProfileId | Profile id. |
VendorId | Vendor ID. |
nsduLength | Length of the payload. |
nsdu | Actual payload |
RxLinkQuality | Link quality of received packet. |
RxFlags | Rx Flags. |
References UNUSED.
bool vendor_data_request | ( | uint8_t | PairingRef, |
profile_id_t | ProfileId, | ||
uint16_t | VendorId, | ||
uint8_t | nsduLength, | ||
uint8_t * | nsdu, | ||
uint8_t | TxOptions | ||
) |
Vendor data request.
The vendor data request allows a device to send a vendor specific data frame.
PairingRef | Pairing reference of the recipient of the transmission |
ProfileId | Profile id used for the transmission |
VendorId | Vendor id used for the transmission |
nsduLength | Length of the payload data |
nsdu | Pointer to the payload data |
TxOptions | Transit options |
References nlde_data_request(), PROFILE_ID_VENDOR_DATA, and UNUSED.
Referenced by app_task().