Main of TAL Examples - Performance Analyzer application for AT86RF215.
Copyright (c) 2015-2018 Microchip Technology Inc. and its subsidiaries.
|
void | app_alert () |
|
static void | app_task (void) |
| Application task. More...
|
|
retval_t | app_transmit_frame (trx_id_t trx, uint8_t dst_addr_mode, uint8_t *dst_addr, uint8_t src_addr_mode, uint8_t msdu_handle, uint8_t *payload, uint16_t payload_length, uint8_t ack_req) |
| Function to transmit frames as per 802.15.4 std. More...
|
|
void | config_node_ib (trx_id_t trx) |
| Function to init the information base for device. More...
|
|
void | get_chat_input (char input) |
|
void | performance_analyzer_init (void) |
| Init function of the Performance Analyzer application. More...
|
|
void | performance_analyzer_task (void) |
| This task needs to be called in a while(1) for performing Performance Analyzer tasks. More...
|
|
void | set_main_state (trx_id_t trx, main_state_t state, void *arg) |
| Function to set the main state of state machine. More...
|
|
void | tal_ed_end_cb (trx_id_t trx, uint8_t energy_level) |
|
void | tal_rx_frame_cb (trx_id_t trx, frame_info_t *frame) |
| User call back function for frame reception. More...
|
|
void | tal_tx_frame_done_cb (trx_id_t trx, retval_t status, frame_info_t *frame) |
| User call back function for frame transmission. More...
|
|