Microchip® Advanced Software Framework

nwkFrame.h File Reference

Frame buffers management interface.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <stdint.h>
#include "compiler.h"

Data Structures

struct  NwkFrame_t
 
struct  NwkFrameHeader_t
 
struct  NwkFrameMulticastHeader_t
 

Macros

#define NWK_FRAME_MAX_PAYLOAD_SIZE   127
 

Typedefs

typedef struct NwkFrame_t NwkFrame_t
 
typedef struct NwkFrameHeader_t NwkFrameHeader_t
 
typedef struct
NwkFrameMulticastHeader_t 
NwkFrameMulticastHeader_t
 

Functions

NwkFrame_tnwkFrameAlloc (void)
 Allocates an empty frame from the buffer pool. More...
 
void nwkFrameCommandInit (NwkFrame_t *frame)
 Sets default parameters for the the command frame. More...
 
void nwkFrameFree (NwkFrame_t *frame)
 Frees a frame and returns it to the buffer pool. More...
 
void nwkFrameInit (void)
 Initializes the Frame module. More...
 
NwkFrame_tnwkFrameNext (NwkFrame_t *frame)
 Cycles through the allocated frames starting from the specified frame. More...
 
static uint8_t nwkFramePayloadSize (NwkFrame_t *frame)
 

#define NWK_FRAME_MAX_PAYLOAD_SIZE   127

typedef struct NwkFrame_t NwkFrame_t

NwkFrame_t* nwkFrameAlloc ( void  )

Allocates an empty frame from the buffer pool.

Returns
Pointer to the frame or NULL if there are no free frames

References NwkFrame_t::data, NwkIb_t::lock, NWK_BUFFERS_AMOUNT, NWK_FRAME_STATE_FREE, nwkIb, NwkFrame_t::payload, NwkFrame_t::size, and NWK_DataReq_t::state.

Referenced by nwkDataReqSendFrame(), nwkRxSendAck(), nwkTxBroadcastFrame(), and PHY_DataInd().

void nwkFrameCommandInit ( NwkFrame_t frame)

Sets default parameters for the the command frame.

Parameters
[in]framePointer to the command frame

References NwkIb_t::addr, NwkFrame_t::header, NWK_SUCCESS_STATUS, NwkFrameHeader_t::nwkFcf, nwkIb, NwkFrameHeader_t::nwkSeq, NwkIb_t::nwkSeqNum, NwkFrameHeader_t::nwkSrcAddr, NwkFrameHeader_t::security, and NwkFrame_t::tx.

Referenced by nwkRxSendAck().

void nwkFrameFree ( NwkFrame_t frame)

Frees a frame and returns it to the buffer pool.

Parameters
[in]framePointer to the frame to be freed

References NwkIb_t::lock, NWK_FRAME_STATE_FREE, nwkIb, and NwkFrame_t::state.

Referenced by nwkDataReqTxConf(), nwkRxTaskHandler(), and nwkTxTaskHandler().

void nwkFrameInit ( void  )

Initializes the Frame module.

References NWK_BUFFERS_AMOUNT, NWK_FRAME_STATE_FREE, and NwkFrame_t::state.

Referenced by NWK_Init().

NwkFrame_t* nwkFrameNext ( NwkFrame_t frame)

Cycles through the allocated frames starting from the specified frame.

Parameters
[in]framePointer to the current frame or NULL for the first frame
Returns
Next allocated frame or NULL if there are no more frames

References NWK_DataReq_t::frame, NWK_BUFFERS_AMOUNT, NWK_FRAME_STATE_FREE, nwkFrameFrames, and NwkFrame_t::state.

Referenced by nwkRxTaskHandler(), nwkTxAckReceived(), nwkTxAckWaitTimerHandler(), nwkTxDelayTimerHandler(), and nwkTxTaskHandler().

static uint8_t nwkFramePayloadSize ( NwkFrame_t frame)
inlinestatic

Referenced by nwkRxIndicateFrame().