Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Contiki processes

A process in Contiki consists of a single protothread.

Data Structures

struct  event_data
 
struct  process
 

Files

file  process.c
 
    Implementation of the Contiki process kernel.

 
file  process.h
 Header file for the Contiki process interface.
 

Macros

#define _DEBUG_   0
 
#define PRINTF(...)
 
#define PROCESS_BROADCAST   NULL
 
#define PROCESS_CONF_NUMEVENTS   32
 
#define PROCESS_EVENT_COM   0x89
 
#define PROCESS_EVENT_CONTINUE   0x85
 
#define PROCESS_EVENT_EXIT   0x83
 
#define PROCESS_EVENT_EXITED   0x87
 
#define PROCESS_EVENT_INIT   0x81
 
#define PROCESS_EVENT_MAX   0x8a
 
#define PROCESS_EVENT_MSG   0x86
 
#define PROCESS_EVENT_NONE   0x80
 
#define PROCESS_EVENT_POLL   0x82
 
#define PROCESS_EVENT_SERVICE_REMOVED   0x84
 
#define PROCESS_EVENT_TIMER   0x88
 
#define PROCESS_LIST()   process_list
 
#define PROCESS_NONE   NULL
 
#define PROCESS_STATE_CALLED   2
 
#define PROCESS_STATE_NONE   0
 
#define PROCESS_STATE_RUNNING   1
 
#define PROCESS_ZOMBIE   ((struct process *)0x1)
 

Typedefs

typedef void * process_data_t
 
typedef unsigned char process_event_t
 
typedef unsigned char process_num_events_t
 

Functions

static void call_process (struct process *p, process_event_t ev, process_data_t data)
 
static void do_event (void)
 
static void do_poll (void)
 
static void exit_process (struct process *p, struct process *fromprocess)
 

Variables

static struct event_data events [PROCESS_CONF_NUMEVENTS]
 
static process_num_events_t fevent
 
static process_event_t lastevent
 
static process_num_events_t nevents
 
static volatile unsigned char poll_requested
 
struct processprocess_current = NULL
 
struct processprocess_list = NULL
 
CCIF struct processprocess_list
 

Return values

#define PROCESS_ERR_OK   0
 Return value indicating that an operation was successful. More...
 
#define PROCESS_ERR_FULL   1
 Return value indicating that the event queue was full. More...
 

Process protothread functions

#define PROCESS_BEGIN()
 Define the beginning of a process. More...
 
#define PROCESS_END()
 Define the end of a process. More...
 
#define PROCESS_WAIT_EVENT()
 Wait for an event to be posted to the process. More...
 
#define PROCESS_WAIT_EVENT_UNTIL(c)
 Wait for an event to be posted to the process, with an extra condition. More...
 
#define PROCESS_YIELD()
 Yield the currently running process. More...
 
#define PROCESS_YIELD_UNTIL(c)
 Yield the currently running process until a condition occurs. More...
 
#define PROCESS_WAIT_UNTIL(c)
 Wait for a condition to occur. More...
 
#define PROCESS_WAIT_WHILE(c)   PT_WAIT_WHILE(process_pt, c)
 
#define PROCESS_EXIT()
 Exit the currently running process. More...
 
#define PROCESS_PT_SPAWN(pt, thread)
 Spawn a protothread from the process. More...
 
#define PROCESS_PAUSE()
 Yield the process for a short while. More...
 

Poll and exit handlers

#define PROCESS_POLLHANDLER(handler)
 Specify an action when a process is polled. More...
 
#define PROCESS_EXITHANDLER(handler)
 Specify an action when a process exits. More...
 

Process declaration and definition

#define PROCESS_THREAD(name, ev, data)
 Define the body of a process. More...
 
#define PROCESS_NAME(name)
 Declare the name of a process. More...
 
#define PROCESS(name, strname)
 Declare a process. More...
 

Functions called from application programs

CCIF struct processprocess_current
 
process_event_t process_alloc_event (void)
 Allocate a global event number. More...
 
void process_start (struct process *p, const char *arg)
 Start a process. More...
 
void process_exit (struct process *p)
 Cause a process to exit. More...
 
int process_post (struct process *p, process_event_t ev, void *data)
 Post an asynchronous event. More...
 
void process_post_synch (struct process *p, process_event_t ev, void *data)
 Post a synchronous event to a process. More...
 
#define PROCESS_CURRENT()
 Get a pointer to the currently running process. More...
 
#define PROCESS_CONTEXT_BEGIN(p)
 Switch context to another process. More...
 
#define PROCESS_CONTEXT_END(p)   process_current = tmp_current; }
 End a context switch. More...
 

Functions called from device drivers

void process_poll (struct process *p)
 Request a process to be polled. More...
 

Functions called by the system and boot-up code

void process_init (void)
 Initialize the process module. More...
 
int process_run (void)
 Run the system once - call poll handlers and process one event. More...
 
int process_nevents (void)
 Number of events waiting to be processed. More...
 
int process_is_running (struct process *p)
 Check if a process is running. More...
 

#define _DEBUG_   0
#define PRINTF (   ...)
#define PROCESS (   name,
  strname 
)

Declare a process.

This macro declares a process. The process has two names: the variable of the process structure, which is used by the C program, and a human readable string name, which is used when debugging. A configuration option allows removal of the readable name to save RAM.

Parameters
nameThe variable name of the process structure.
strnameThe string representation of the process' name.
#define PROCESS_BEGIN ( )

Define the beginning of a process.

This macro defines the beginning of a process, and must always appear in a PROCESS_THREAD() definition. The PROCESS_END() macro must come at the end of the process.

Referenced by PROCESS_THREAD().

#define PROCESS_BROADCAST   NULL
#define PROCESS_CONF_NUMEVENTS   32

Referenced by do_event(), and process_post().

#define PROCESS_CONTEXT_BEGIN (   p)
Value:
{\
struct process *tmp_current = PROCESS_CURRENT();\
Definition: process.h:315
#define PROCESS_CURRENT()
Get a pointer to the currently running process.
Definition: process.h:402
struct process * process_current
Definition: process.c:55

Switch context to another process.

This function switch context to the specified process and executes the code as if run by that process. Typical use of this function is to switch context in services, called by other processes. Each PROCESS_CONTEXT_BEGIN() must be followed by the PROCESS_CONTEXT_END() macro to end the context switch.

Example:

Parameters
pThe process to use as context
See Also
PROCESS_CONTEXT_END()
PROCESS_CURRENT()

Referenced by ctimer_reset(), ctimer_restart(), ctimer_set(), PROCESS_THREAD(), simple_udp_register(), tcp_socket_connect(), tcp_socket_listen(), tcp_socket_unlisten(), and udp_socket_register().

#define PROCESS_CONTEXT_END (   p)    process_current = tmp_current; }

End a context switch.

This function ends a context switch and changes back to the previous process.

Parameters
pThe process used in the context switch
See Also
PROCESS_CONTEXT_START()

Referenced by ctimer_reset(), ctimer_restart(), ctimer_set(), PROCESS_THREAD(), simple_udp_register(), tcp_socket_connect(), tcp_socket_listen(), tcp_socket_unlisten(), and udp_socket_register().

#define PROCESS_CURRENT ( )

Get a pointer to the currently running process.

This macro get a pointer to the currently running process. Typically, this macro is used to post an event to the current process with process_post().

Referenced by add_timer(), ctimer_set(), icmp6_new(), process_exit(), process_post(), PROCESS_THREAD(), tcp_attach(), tcp_connect(), tcp_listen(), tcp_unlisten(), udp_attach(), udp_new(), and udp_socket_register().

#define PROCESS_END ( )

Define the end of a process.

This macro defines the end of a process. It must appear in a PROCESS_THREAD() definition and must always be included. The process exits when the PROCESS_END() macro is reached.

Referenced by PROCESS_THREAD().

#define PROCESS_ERR_FULL   1

Return value indicating that the event queue was full.

This value is returned from process_post() to indicate that the event queue was full and that an event could not be posted.

Referenced by process_post().

#define PROCESS_ERR_OK   0

Return value indicating that an operation was successful.

This value is returned to indicate that an operation was successful.

Referenced by process_post(), and PROCESS_THREAD().

#define PROCESS_EVENT_COM   0x89
#define PROCESS_EVENT_CONTINUE   0x85

Referenced by PROCESS_THREAD().

#define PROCESS_EVENT_EXIT   0x83

Referenced by call_process(), and exit_process().

#define PROCESS_EVENT_EXITED   0x87
#define PROCESS_EVENT_INIT   0x81

Referenced by do_event(), and process_start().

#define PROCESS_EVENT_MAX   0x8a

Referenced by process_init().

#define PROCESS_EVENT_MSG   0x86
#define PROCESS_EVENT_NONE   0x80

Referenced by dhcpc_request().

#define PROCESS_EVENT_POLL   0x82

Referenced by do_poll(), and PROCESS_THREAD().

#define PROCESS_EVENT_SERVICE_REMOVED   0x84
#define PROCESS_EVENT_TIMER   0x88
#define PROCESS_EXIT ( )

Exit the currently running process.

#define PROCESS_EXITHANDLER (   handler)

Specify an action when a process exits.

Note
This declaration must come immediately before the PROCESS_BEGIN() macro.
Parameters
handlerThe action to be performed.

Referenced by PROCESS_THREAD().

#define PROCESS_LIST ( )    process_list
#define PROCESS_NAME (   name)

Declare the name of a process.

This macro is typically used in header files to declare the name of a process that is implemented in the C file.

#define PROCESS_PAUSE ( )

Yield the process for a short while.

This macro yields the currently running process for a short while, thus letting other processes run before the process continues.

#define PROCESS_POLLHANDLER (   handler)

Specify an action when a process is polled.

Note
This declaration must come immediately before the PROCESS_BEGIN() macro.
Parameters
handlerThe action to be performed.
#define PROCESS_PT_SPAWN (   pt,
  thread 
)

Spawn a protothread from the process.

Parameters
ptThe protothread state (struct pt) for the new protothread
threadThe call to the protothread function.
See Also
PT_SPAWN()
#define PROCESS_STATE_CALLED   2

Referenced by call_process(), and process_poll().

#define PROCESS_STATE_NONE   0

Referenced by exit_process(), and process_is_running().

#define PROCESS_STATE_RUNNING   1
#define PROCESS_THREAD (   name,
  ev,
  data 
)

Define the body of a process.

This macro is used to define the body (protothread) of a process. The process is called whenever an event occurs in the system, A process always start with the PROCESS_BEGIN() macro and end with the PROCESS_END() macro.

#define PROCESS_WAIT_EVENT ( )

Wait for an event to be posted to the process.

This macro blocks the currently running process until the process receives an event.

Referenced by PROCESS_THREAD().

#define PROCESS_WAIT_EVENT_UNTIL (   c)

Wait for an event to be posted to the process, with an extra condition.

This macro is similar to PROCESS_WAIT_EVENT() in that it blocks the currently running process until the process receives an event. But PROCESS_WAIT_EVENT_UNTIL() takes an extra condition which must be true for the process to continue.

Parameters
cThe condition that must be true for the process to continue.
See Also
PT_WAIT_UNTIL()

Referenced by PROCESS_THREAD().

#define PROCESS_WAIT_UNTIL (   c)

Wait for a condition to occur.

This macro does not guarantee that the process yields, and should therefore be used with care. In most cases, PROCESS_WAIT_EVENT(), PROCESS_WAIT_EVENT_UNTIL(), PROCESS_YIELD() or PROCESS_YIELD_UNTIL() should be used instead.

Parameters
cThe condition to wait for.
#define PROCESS_WAIT_WHILE (   c)    PT_WAIT_WHILE(process_pt, c)
#define PROCESS_YIELD ( )

Yield the currently running process.

Referenced by PROCESS_THREAD().

#define PROCESS_YIELD_UNTIL (   c)

Yield the currently running process until a condition occurs.

This macro is different from PROCESS_WAIT_UNTIL() in that PROCESS_YIELD_UNTIL() is guaranteed to always yield at least once. This ensures that the process does not end up in an infinite loop and monopolizing the CPU.

Parameters
cThe condition to wait for.

Referenced by PROCESS_THREAD().

#define PROCESS_ZOMBIE   ((struct process *)0x1)

typedef void* process_data_t
typedef unsigned char process_event_t
typedef unsigned char process_num_events_t

static void do_poll ( void  )
static
static void exit_process ( struct process p,
struct process fromprocess 
)
static
CCIF process_event_t process_alloc_event ( void  )

Allocate a global event number.

Returns
The allocated event number
        In Contiki, event numbers above 128 are global and may
        be posted from one process to another. This function
        allocates one such event number.
Note
There currently is no way to deallocate an allocated event number.

References lastevent.

Referenced by PROCESS_THREAD().

CCIF void process_exit ( struct process p)

Cause a process to exit.

Parameters
pThe process that is to be exited
        This function causes a process to exit. The process can
        either be the currently executing process, or another
        process that is currently running.
See Also
PROCESS_CURRENT()

References exit_process(), and PROCESS_CURRENT.

Referenced by autostart_exit(), and start_name_collision_check().

void process_init ( void  )

Initialize the process module.

This function initializes the process module and should be called by the system boot-up code.

References fevent, lastevent, nevents, NULL, and PROCESS_EVENT_MAX.

Referenced by main().

CCIF int process_is_running ( struct process p)

Check if a process is running.

This function checks if a specific process is running.

Parameters
pThe process.
Return values
Non-zeroif the process is running.
Zeroif the process is not running.

References PROCESS_STATE_NONE, and state.

Referenced by exit_process().

int process_nevents ( void  )

Number of events waiting to be processed.

Returns
The number of events that are currently waiting to be processed.

References nevents, and poll_requested.

CCIF void process_poll ( struct process p)

Request a process to be polled.

This function typically is called from an interrupt handler to cause a process to be polled.

Parameters
pA pointer to the process' process structure.

References needspoll, NULL, poll_requested, PROCESS_STATE_CALLED, PROCESS_STATE_RUNNING, and state.

Referenced by etimer_request_poll(), rf233_interrupt_poll(), sensors_changed(), serial_line_input_byte(), slip_input_byte(), and slip_poll_handler().

CCIF int process_post ( struct process p,
process_event_t  ev,
void *  data 
)

Post an asynchronous event.

This function posts an asynchronous event to one or more processes. The handing of the event is deferred until the target process is scheduled by the kernel. An event can be broadcast to all processes, in which case all processes in the system will be scheduled to handle the event.

Parameters
evThe event to be posted.
dataThe auxiliary data to be sent with the event
pThe process to which the event should be posted, or PROCESS_BROADCAST if the event should be posted to all processes.
Return values
PROCESS_ERR_OKThe event could be posted.
PROCESS_ERR_FULLThe event queue was full and the event could not be posted.

References event_data::data, event_data::ev, events, fevent, nevents, NULL, event_data::p, printf, PRINTF, PROCESS_BROADCAST, PROCESS_CONF_NUMEVENTS, PROCESS_CURRENT, PROCESS_ERR_FULL, PROCESS_ERR_OK, and PROCESS_NAME_STRING.

Referenced by mdns_found(), mdns_query(), PROCESS_THREAD(), resolv_found(), resolv_query(), tcpip_poll_tcp(), tcpip_poll_udp(), uaodv_bad_dest(), and uaodv_request_route_to().

CCIF void process_post_synch ( struct process p,
process_event_t  ev,
void *  data 
)

Post a synchronous event to a process.

Parameters
pA pointer to the process' process structure.
evThe event to be posted.
dataA pointer to additional data that is posted together with the event.

References call_process(), and process_current.

Referenced by process_start(), tcpip_icmp6_call(), tcpip_input(), and tcpip_uipcall().

int process_run ( void  )

Run the system once - call poll handlers and process one event.

This function should be called repeatedly from the main() program to actually run the Contiki system. It calls the necessary poll handlers, and processes one event. The function returns the number of events that are waiting in the event queue so that the caller may choose to put the CPU to sleep when there are no pending events.

Returns
The number of events that are currently waiting in the event queue.

References do_event(), do_poll(), nevents, and poll_requested.

Referenced by main().

CCIF void process_start ( struct process p,
const char *  arg 
)

Start a process.

Parameters
pA pointer to a process structure.
argAn argument pointer that can be passed to the new process

References next, NULL, PRINTF, PROCESS_EVENT_INIT, process_list, PROCESS_NAME_STRING, process_post_synch(), PROCESS_STATE_RUNNING, pt, PT_INIT, and state.

Referenced by autostart_start(), ctimer_init(), init(), init_simple_udp(), ledctrl_init(), main(), mdns_init(), procinit_init(), rf233_init(), serial_line_init(), and start_name_collision_check().

struct event_data events[PROCESS_CONF_NUMEVENTS]
static
process_num_events_t fevent
static
process_event_t lastevent
static
volatile unsigned char poll_requested
static
struct process* process_current = NULL

Referenced by exit_process(), and process_post_synch().

CCIF struct process* process_current

Referenced by exit_process(), and process_post_synch().

struct process* process_list = NULL

Referenced by process_start().

CCIF struct process* process_list

Referenced by process_start().