Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
The Contiki/uIP interface

TCP/IP support in Contiki is implemented using the uIP TCP/IP stack.

For sending and receiving data, Contiki uses the functions provided by the uIP module, but Contiki adds a set of functions for connection management. The connection management functions make sure that the uIP TCP/IP connections are connected to the correct process.

Contiki also includes an optional protosocket library that provides an API similar to the BSD socket API.

See Also
The uIP TCP/IP stack
Protosockets library

Data Structures

struct  tcpip_uipstate
 

Files

file  tcpip.h
 
     Header for the Contiki/uIP interface.

 

Macros

#define UIP_APPCALL   tcpip_uipcall
 The name of the application function that uIP should call in response to TCP/IP events. More...
 
#define UIP_ICMP6_APPCALL   tcpip_icmp6_call
 
#define UIP_UDP_APPCALL   tcpip_uipcall
 

Typedefs

typedef struct tcpip_uipstate uip_icmp6_appstate_t
 

Functions

 PROCESS_NAME (tcpip_process)
 
void tcpip_uipcall (void)
 

Variables

CCIF process_event_t tcpip_event
 The uIP event. More...
 

TCP functions

CCIF void tcp_attach (struct uip_conn *conn, void *appstate)
 Attach a TCP connection to the current process. More...
 
CCIF void tcp_listen (uint16_t port)
 Open a TCP port. More...
 
CCIF void tcp_unlisten (uint16_t port)
 Close a listening TCP port. More...
 
CCIF struct uip_conntcp_connect (uip_ipaddr_t *ripaddr, uint16_t port, void *appstate)
 Open a TCP connection to the specified IP address and port. More...
 
void tcpip_poll_tcp (struct uip_conn *conn)
 Cause a specified TCP connection to be polled. More...
 
#define tcp_markconn(conn, appstate)   tcp_attach(conn, appstate)
 

UDP functions

void udp_attach (struct uip_udp_conn *conn, void *appstate)
 Attach the current process to a UDP connection. More...
 
CCIF struct uip_udp_connudp_new (const uip_ipaddr_t *ripaddr, uint16_t port, void *appstate)
 Create a new UDP connection. More...
 
struct uip_udp_connudp_broadcast_new (uint16_t port, void *appstate)
 Create a new UDP broadcast connection. More...
 
CCIF void tcpip_poll_udp (struct uip_udp_conn *conn)
 Cause a specified UDP connection to be polled. More...
 
#define udp_markconn(conn, appstate)   udp_attach(conn, appstate)
 
#define udp_bind(conn, port)   uip_udp_bind(conn, port)
 Bind a UDP connection to a local port. More...
 

ICMPv6 functions

CCIF process_event_t tcpip_icmp6_event
 The ICMP6 event. More...
 
uint8_t icmp6_new (void *appstate)
 register an ICMPv6 callback More...
 
void tcpip_icmp6_call (uint8_t type)
 This function is called at reception of an ICMPv6 packet If an application registered as an ICMPv6 listener (with icmp6_new), it will be called through a process_post_synch() More...
 

TCP/IP packet processing

unsigned char tcpip_do_forwarding
 Is forwarding generally enabled? More...
 
unsigned char tcpip_is_forwarding
 
CCIF void tcpip_input (void)
 Deliver an incoming packet to the TCP/IP stack. More...
 
uint8_t tcpip_output (const uip_lladdr_t *)
 Output packet to layer 2 The eventual parameter is the MAC address of the destination. More...
 
void tcpip_set_outputfunc (uint8_t(*f)(const uip_lladdr_t *))
 
void tcpip_ipv6_output (void)
 This function does address resolution and then calls tcpip_output. More...
 
#define tcpip_set_forwarding(forwarding)   tcpip_do_forwarding = (forwarding)
 

#define tcp_markconn (   conn,
  appstate 
)    tcp_attach(conn, appstate)

Referenced by appcall().

#define tcpip_set_forwarding (   forwarding)    tcpip_do_forwarding = (forwarding)
#define udp_bind (   conn,
  port 
)    uip_udp_bind(conn, port)

Bind a UDP connection to a local port.

This function binds a UDP connection to a specified local port.

When a connection is created with udp_new(), it gets a local port number assigned automatically. If the application needs to bind the connection to a specified local port, this function should be used.

Note
The port number must be provided in network byte order so a conversion with UIP_HTONS() usually is necessary.
Parameters
connA pointer to the UDP connection that is to be bound.
portThe port number in network byte order to which to bind the connection.

Referenced by dhcpc_init(), simple_udp_register(), udp_broadcast_new(), and udp_socket_bind().

#define udp_markconn (   conn,
  appstate 
)    udp_attach(conn, appstate)
define UIP_APPCALL   tcpip_uipcall

The name of the application function that uIP should call in response to TCP/IP events.

Referenced by uip_process().

#define UIP_ICMP6_APPCALL   tcpip_icmp6_call

Referenced by uip_process().

#define UIP_UDP_APPCALL   tcpip_uipcall

Referenced by uip_process().

uint8_t icmp6_new ( void *  appstate)

register an ICMPv6 callback

Returns
0 if success, 1 if failure (one application already registered)

This function just registers a process to be polled when an ICMPv6 message is received. If no application registers, some ICMPv6 packets will be processed by the "kernel" as usual (NS, NA, RS, RA, Echo request), others will be dropped. If an application registers here, it will be polled with a process_post_synch every time an ICMPv6 packet is received.

References uip_udp_conn::appstate, uip_icmp6_conn::appstate, tcpip_uipstate::p, PROCESS_CURRENT, PROCESS_NONE, tcpip_uipstate::state, and uip_icmp6_conns.

PROCESS_NAME ( tcpip_process  )
CCIF void tcp_attach ( struct uip_conn conn,
void *  appstate 
)

Attach a TCP connection to the current process.

This function attaches the current process to a TCP connection. Each TCP connection must be attached to a process in order for the process to be able to receive and send data. Additionally, this function can add a pointer with connection state to the connection.

Parameters
connA pointer to the TCP connection.
appstateAn opaque pointer that will be passed to the process whenever an event occurs on the connection.

References uip_conn::appstate, tcpip_uipstate::p, PROCESS_CURRENT, s, and tcpip_uipstate::state.

Referenced by tcp_socket_unregister().

CCIF struct uip_conn* tcp_connect ( uip_ipaddr_t ripaddr,
uint16_t  port,
void *  appstate 
)

Open a TCP connection to the specified IP address and port.

This function opens a TCP connection to the specified port at the host specified with an IP address. Additionally, an opaque pointer can be attached to the connection. This pointer will be sent together with uIP events to the process.

Note
The port number must be provided in network byte order so a conversion with UIP_HTONS() usually is necessary.
This function will only create the connection. The connection is not opened directly. uIP will try to open the connection the next time the uIP stack is scheduled by Contiki.
Parameters
ripaddrPointer to the IP address of the remote host.
portPort number in network byte order.
appstatePointer to application defined data.
Returns
A pointer to the newly created connection, or NULL if memory could not be allocated for the connection.

References uip_conn::appstate, c, NULL, tcpip_uipstate::p, PROCESS_CURRENT, tcpip_uipstate::state, tcpip_poll_tcp(), and uip_connect().

Referenced by tcp_socket_connect().

CCIF void tcp_listen ( uint16_t  port)

Open a TCP port.

This function opens a TCP port for listening. When a TCP connection request occurs for the port, the process will be sent a tcpip_event with the new connection request.

Note
Port numbers must always be given in network byte order. The functions UIP_HTONS() and uip_htons() can be used to convert port numbers from host byte order to network byte order.
Parameters
portThe port number in network byte order.

References i, internal_state::listenports, listenport::p, listenport::port, PROCESS_CURRENT, s, uip_listen(), and UIP_LISTENPORTS.

Referenced by tcp_socket_listen().

CCIF void tcp_unlisten ( uint16_t  port)

Close a listening TCP port.

This function closes a listening TCP port.

Note
Port numbers must always be given in network byte order. The functions UIP_HTONS() and uip_htons() can be used to convert port numbers from host byte order to network byte order.
Parameters
portThe port number in network byte order.

References i, internal_state::listenports, listenport::p, listenport::port, PROCESS_CURRENT, s, UIP_LISTENPORTS, and uip_unlisten().

Referenced by tcp_socket_unlisten().

void tcpip_icmp6_call ( uint8_t  type)

This function is called at reception of an ICMPv6 packet If an application registered as an ICMPv6 listener (with icmp6_new), it will be called through a process_post_synch()

References uip_icmp6_conn::appstate, tcpip_uipstate::p, PROCESS_NONE, process_post_synch(), tcpip_icmp6_event, and uip_icmp6_conns.

CCIF void tcpip_input ( void  )

Deliver an incoming packet to the TCP/IP stack.

This function is called by network device drivers to deliver an incoming packet to the TCP/IP stack. The incoming packet must be present in the uip_buf buffer, and the length of the packet must be in the global uip_len variable.

References NULL, PACKET_INPUT, process_post_synch(), uip_ext_len, and uip_len.

Referenced by input(), PROCESS_THREAD(), and recv_data().

uint8_t tcpip_output ( const uip_lladdr_t )

Output packet to layer 2 The eventual parameter is the MAC address of the destination.

References NULL, outputfunc, and UIP_LOG.

Referenced by eventhandler(), packet_input(), tcpip_ipv6_output(), uip_split_output(), and uip_udp_packet_send().

void tcpip_poll_tcp ( struct uip_conn conn)

Cause a specified TCP connection to be polled.

This function causes uIP to poll the specified TCP connection. The function is used when the application has data that is to be sent immediately and do not wish to wait for the periodic uIP polling mechanism.

Parameters
connA pointer to the TCP connection that should be polled.

References process_post(), and TCP_POLL.

Referenced by tcp_connect().

CCIF void tcpip_poll_udp ( struct uip_udp_conn conn)

Cause a specified UDP connection to be polled.

This function causes uIP to poll the specified UDP connection. The function is used when the application has data that is to be sent immediately and do not wish to wait for the periodic uIP polling mechanism.

Parameters
connA pointer to the UDP connection that should be polled.

References process_post(), and UDP_POLL.

Referenced by PROCESS_THREAD(), and while().

void tcpip_set_outputfunc ( uint8_t(*)(const uip_lladdr_t *)  f)

References outputfunc.

Referenced by sicslowpan_init().

void udp_attach ( struct uip_udp_conn conn,
void *  appstate 
)

Attach the current process to a UDP connection.

This function attaches the current process to a UDP connection. Each UDP connection must have a process attached to it in order for the process to be able to receive and send data over the connection. Additionally, this function can add a pointer with connection state to the connection.

Parameters
connA pointer to the UDP connection.
appstateAn opaque pointer that will be passed to the process whenever an event occurs on the connection.

References uip_udp_conn::appstate, tcpip_uipstate::p, PROCESS_CURRENT, s, and tcpip_uipstate::state.

struct uip_udp_conn* udp_broadcast_new ( uint16_t  port,
void *  appstate 
)

Create a new UDP broadcast connection.

This function creates a new (link-local) broadcast UDP connection to a specified port.

Parameters
portPort number in network byte order.
appstatePointer to application defined data.
Returns
A pointer to the newly created connection, or NULL if memory could not be allocated for the connection.

References addr, NULL, udp_bind, udp_new(), uip_create_linklocal_allnodes_mcast, and uip_ipaddr.

Referenced by PROCESS_THREAD().

CCIF struct uip_udp_conn* udp_new ( const uip_ipaddr_t ripaddr,
uint16_t  port,
void *  appstate 
)

Create a new UDP connection.

This function creates a new UDP connection with the specified remote endpoint.

Note
The port number must be provided in network byte order so a conversion with UIP_HTONS() usually is necessary.
See Also
udp_bind()
Parameters
ripaddrPointer to the IP address of the remote host.
portPort number in network byte order.
appstatePointer to application defined data.
Returns
A pointer to the newly created connection, or NULL if memory could not be allocated for the connection.

References uip_udp_conn::appstate, c, NULL, tcpip_uipstate::p, PROCESS_CURRENT, s, tcpip_uipstate::state, and uip_udp_new().

Referenced by dhcpc_init(), PROCESS_THREAD(), simple_udp_register(), udp_broadcast_new(), and udp_socket_register().

unsigned char tcpip_do_forwarding

Is forwarding generally enabled?

CCIF process_event_t tcpip_event

The uIP event.

This event is posted to a process whenever a uIP event has occurred.

Referenced by dhcpc_appcall(), PROCESS_THREAD(), tcpip_uipcall(), and while().

CCIF process_event_t tcpip_icmp6_event

The ICMP6 event.

This event is posted to a process whenever a uIP ICMP event has occurred.

Referenced by PROCESS_THREAD(), and tcpip_icmp6_call().

unsigned char tcpip_is_forwarding