Functions | |
signed portBASE_TYPE | com1shell_GetChar (signed portCHAR *pcByte) |
Get a char from the COM1 port. More... | |
void | v_com1shell_mount_local_drive (void) |
Mount default local drive 'a:'. More... | |
void | v_com1shell_stopResources (void) |
Stop the com1shell module resources. More... | |
void | vcom1shell_PrintMsg (const signed portCHAR *pcString) |
Print a string to the COM1 port. More... | |
void | vcom1shell_PutChar (signed portCHAR cByte) |
Put a char to the COM1 port. More... | |
void | vStartCom1Shell (unsigned portBASE_TYPE uxPriority) |
eStatus | xCom1Shell_GetStatus (void) |
Return the status of the COM1 shell module. More... | |
signed portBASE_TYPE com1shell_GetChar | ( | signed portCHAR * | pcByte | ) |
Get a char from the COM1 port.
pcByte | Output. The char received from the COM1 port. |
References COM1SHELL_RX_BLOCK_TIME, xComPort1Hndl, and xUsartGetChar().
Referenced by prv_GetChar_From_Requester_Stream().
void v_com1shell_mount_local_drive | ( | void | ) |
Mount default local drive 'a:'.
References fsaccess_give_mutex(), fsaccess_take_mutex(), LUN_ID_AT45DBX_MEM, nav_drive_set(), nav_partition_mount(), nav_select(), and sCom1ShellNavId.
Referenced by prv_v_leave_maintenance_mode(), and vStartCom1Shell().
void v_com1shell_stopResources | ( | void | ) |
Stop the com1shell module resources.
References vSerialClose(), and xComPort1Hndl.
Referenced by e_syscmds_reboot().
void vcom1shell_PrintMsg | ( | const signed portCHAR * | pcString | ) |
Print a string to the COM1 port.
pcString | Input. The string to print. |
References usUsartPutString(), and xComPort1Hndl.
Referenced by portTASK_FUNCTION(), prv_Print_String_To_Requester_Stream(), prvGetCmdLine(), and v_shell_Print_String_To_Requester_Stream().
void vcom1shell_PutChar | ( | signed portCHAR | cByte | ) |
Put a char to the COM1 port.
cByte | Input. The char to print. |
References COM1SHELL_NO_BLOCK, xComPort1Hndl, and xUsartPutChar().
Referenced by prv_PutChar_To_Requester_Stream(), and prvGetCmdLine().
void vStartCom1Shell | ( | unsigned portBASE_TYPE | uxPriority | ) |
Start the COM1 shell module.
uxPriority | The priority base of the COM1 shell tasks. |
References COM1SHELL_STACK_SIZE, fsaccess_alloc_nav_id(), fsaccess_give_mutex(), fsaccess_take_mutex(), NULL, pdPASS, sCom1ShellNavId, SYS_STATUS_DOWN, SYS_STATUS_STARTUP, v_com1shell_mount_local_drive(), xCom1ShellHndl, xCom1ShellStatus, and xTaskCreate.
Referenced by portTASK_FUNCTION().
eStatus xCom1Shell_GetStatus | ( | void | ) |
Return the status of the COM1 shell module.
Return the status of the COM1 shell module.
References xCom1ShellStatus.