Functions | |
bool | b_pushb1_get_value (xLogDef *pxLog) |
Get a pushbutton current state. More... | |
bool | b_pushb1_init (void) |
Init the push button 1 sensor. More... | |
bool | b_pushb2_get_value (xLogDef *pxLog) |
Get a pushbutton current state. More... | |
bool | b_pushb2_init (void) |
Init the push button 2 sensor. More... | |
bool | b_pushb3_get_value (xLogDef *pxLog) |
Get a pushbutton current state. More... | |
bool | b_pushb3_init (void) |
Init the push button 3 sensor. More... | |
eExecStatus | e_pushb1_get_config (signed portCHAR **ppcStringReply) |
Get the pushbutton1 sensor config. More... | |
eExecStatus | e_pushb1_set_config (signed portCHAR **ppcStringReply, int ac, signed portCHAR *av[]) |
Set the sensor config. More... | |
eExecStatus | e_pushb2_get_config (signed portCHAR **ppcStringReply) |
Get the pushbutton2 sensor config. More... | |
eExecStatus | e_pushb2_set_config (signed portCHAR **ppcStringReply, int ac, signed portCHAR *av[]) |
Set the sensor config. More... | |
eExecStatus | e_pushb3_get_config (signed portCHAR **ppcStringReply) |
Get the pushbutton3 sensor config. More... | |
eExecStatus | e_pushb3_set_config (signed portCHAR **ppcStringReply, int ac, signed portCHAR *av[]) |
Set the sensor config. More... | |
void | v_pushb1_stop (void) |
Stop the push button 1 sensor. More... | |
void | v_pushb2_stop (void) |
Stop the push button 2 sensor. More... | |
void | v_pushb3_stop (void) |
Stop the push button 1 sensor. More... | |
Get a pushbutton current state.
pxLog | a Log structure. The id field identifies the pushbutton. |
References acpc_pushb_events, b_pushb1, NULL, LogDef::pcStringLog, and LogDef::pfFreeStringLog.
Referenced by b_sensor_get_value().
bool b_pushb1_init | ( | void | ) |
Init the push button 1 sensor.
References bAlarm1, config_file_get_value(), Disable_global_interrupt, Enable_global_interrupt, gpio_enable_pin_interrupt(), GPIO_PIN_CHANGE, INTC_register_interrupt(), PB1_POSITION, pdTRUE, SENSOR_PB1_CONFIG_FILE, vpushb_ISR(), x_supervisor_SemaphoreGive(), and x_supervisor_SemaphoreTake().
Get a pushbutton current state.
pxLog | a Log structure. The id field identifies the pushbutton. |
References acpc_pushb_events, b_pushb2, NULL, LogDef::pcStringLog, and LogDef::pfFreeStringLog.
Referenced by b_sensor_get_value().
bool b_pushb2_init | ( | void | ) |
Init the push button 2 sensor.
References bAlarm2, config_file_get_value(), Disable_global_interrupt, Enable_global_interrupt, gpio_enable_pin_interrupt(), GPIO_PIN_CHANGE, INTC_register_interrupt(), PB2_POSITION, pdTRUE, SENSOR_PB2_CONFIG_FILE, vpushb_ISR(), x_supervisor_SemaphoreGive(), and x_supervisor_SemaphoreTake().
Get a pushbutton current state.
pxLog | a Log structure. The id field identifies the pushbutton. |
References acpc_pushb_events, b_pushb3, NULL, LogDef::pcStringLog, and LogDef::pfFreeStringLog.
Referenced by b_sensor_get_value().
bool b_pushb3_init | ( | void | ) |
Init the push button 3 sensor.
References bAlarm3, config_file_get_value(), Disable_global_interrupt, Enable_global_interrupt, gpio_enable_pin_interrupt(), GPIO_PIN_CHANGE, INTC_register_interrupt(), PB3_POSITION, pdTRUE, SENSOR_PB3_CONFIG_FILE, vpushb_ISR(), x_supervisor_SemaphoreGive(), and x_supervisor_SemaphoreTake().
eExecStatus e_pushb1_get_config | ( | signed portCHAR ** | ppcStringReply | ) |
Get the pushbutton1 sensor config.
ppcStringReply | Input/Output. The response string. NEVER NULL AS INPUT. A malloc for the response string is performed here; the caller must free this string. |
References bAlarm1, and prv_e_pushb_get_config().
eExecStatus e_pushb1_set_config | ( | signed portCHAR ** | ppcStringReply, |
int | ac, | ||
signed portCHAR * | av[] | ||
) |
Set the sensor config.
ppcStringReply | Input/Output. The response string. NEVER NULL AS INPUT. |
ac | Input. Number of args |
av | Input. pointer to args |
Set the sensor config.
ac | Input. The argument counter. For this command, should be 2. |
av | Input. The argument vector. |
ppcStringReply | Input/Output. The response string. If Input is NULL, no response string will be output. Else a malloc for the response string is performed here; the caller must free this string. |
References bAlarm1, prv_e_pushb_set_config(), and SENSOR_PB1_CONFIG_FILE.
eExecStatus e_pushb2_get_config | ( | signed portCHAR ** | ppcStringReply | ) |
Get the pushbutton2 sensor config.
ppcStringReply | Input/Output. The response string. NEVER NULL AS INPUT. A malloc for the response string is performed here; the caller must free this string. |
References bAlarm2, and prv_e_pushb_get_config().
eExecStatus e_pushb2_set_config | ( | signed portCHAR ** | ppcStringReply, |
int | ac, | ||
signed portCHAR * | av[] | ||
) |
Set the sensor config.
ppcStringReply | Input/Output. The response string. NEVER NULL AS INPUT. |
ac | Input. Number of args |
av | Input. pointer to args |
Set the sensor config.
ac | Input. The argument counter. For this command, should be 2. |
av | Input. The argument vector. |
ppcStringReply | Input/Output. The response string. |
References bAlarm2, prv_e_pushb_set_config(), and SENSOR_PB2_CONFIG_FILE.
eExecStatus e_pushb3_get_config | ( | signed portCHAR ** | ppcStringReply | ) |
Get the pushbutton3 sensor config.
ppcStringReply | Input/Output. The response string. NEVER NULL AS INPUT. A malloc for the response string is performed here; the caller must free this string. |
References bAlarm3, and prv_e_pushb_get_config().
eExecStatus e_pushb3_set_config | ( | signed portCHAR ** | ppcStringReply, |
int | ac, | ||
signed portCHAR * | av[] | ||
) |
Set the sensor config.
ppcStringReply | Input/Output. The response string. NEVER NULL AS INPUT. |
ac | Input. Number of args |
av | Input. pointer to args |
Set the sensor config.
ac | Input. The argument counter. For this command, should be 2. |
av | Input. The argument vector. |
ppcStringReply | Input/Output. The response string. |
References bAlarm3, prv_e_pushb_set_config(), and SENSOR_PB3_CONFIG_FILE.
void v_pushb1_stop | ( | void | ) |
Stop the push button 1 sensor.
References gpio_disable_pin_interrupt(), and PB1_POSITION.
void v_pushb2_stop | ( | void | ) |
Stop the push button 2 sensor.
References gpio_disable_pin_interrupt(), and PB2_POSITION.
void v_pushb3_stop | ( | void | ) |
Stop the push button 1 sensor.
Stop the push button 1 sensor.
References gpio_disable_pin_interrupt(), and PB3_POSITION.