#include <string.h>
#include <stdio.h>
#include "compiler.h"
#include "s_light.h"
#include "board.h"
#include "gpio.h"
#include "adc.h"
#include "FreeRTOS.h"
Functions | |
bool | b_light_get_value (char *buf, U32 *result) |
Get the current light sensor value. More... | |
Variables | |
static volatile avr32_adc_t * | adc = (volatile avr32_adc_t *) &AVR32_ADC |
Get the current light sensor value.
buf | char buffer in which the light sensor value is stored. |
result | returns the light sensor value. |
References adc, adc_disable(), adc_enable(), adc_get_value(), ADC_MAX_VALUE, adc_start(), and sprintf().
Referenced by device_full_custom_task().
|
static |
ADC cell.