#include "btypes.h"
Typedefs | |
typedef uint8 | TAppEngineJoystick |
typedef void | TAppEnginePrintCb (TString textToDisplay) |
Enumerations | |
enum | TAppEngineJoystickEnum { AppEngine_None, AppEngine_Left = 0x3C, AppEngine_Right = 0x3E, AppEngine_Up = 0x2B, AppEngine_Down = 0x2D, AppEngine_Push = 0x3D } |
Functions | |
void | AppEngineConnectButton (void) |
Handles functionality coupled to press of the Connect button. More... | |
boolean | AppEngineInit (TAppEnginePrintCb *pCb, TString deviceName) |
Initializes the Bluetooth functionality. More... | |
void | AppEngineInquiryButton (void) |
Handles functionality coupled to press of the Inquiry button. More... | |
void | AppEngineJoystickButton (TAppEngineJoystick joystick) |
Sends a letter for each direction on the joystick. More... | |
void | AppEngineSelectDeviceButton (void) |
Handles functionality coupled to press of the Select button. More... | |
typedef uint8 TAppEngineJoystick |
typedef void TAppEnginePrintCb(TString textToDisplay) |
void AppEngineConnectButton | ( | void | ) |
Handles functionality coupled to press of the Connect button.
None |
None |
References AppEngine_Connected_State, AppEngine_Connecting_State, AppEngine_Disconnecting_State, AppEngine_Idle_State, AppEngineNotifyCallback(), myBdAddr, mySppPort, myState, NULL, status, T2BF_STATUS_OK, T2BFSppConnect(), and T2BFSppDisconnect().
Referenced by app_engine().
boolean AppEngineInit | ( | TAppEnginePrintCb * | pCb, |
TString | deviceName | ||
) |
Initializes the Bluetooth functionality.
pCb | Pointer to callback function that shall receive events from t2BF |
deviceName | Sets the user friendly name that are used when this unit is discovered by others. |
true | Initialization successful. |
false | Baud rate set point is out of range for the given input clock frequency. |
References AppEngine_Idle_State, AppEngineBtCb(), AppEngineNotifyCallback(), AppEngineSppCb(), myBdAddr, myName, mySppPort, myState, myStatus, NULL, pMyCb, T2BF_AUTO_AUTH_ALLOW, T2BF_LITE_COD, T2BF_SEC_LEVEL_2, T2BF_SEC_NORMAL, T2BF_STATUS_OK, T2BFAutoAuthentication(), T2BFDiscoverable(), T2BFInit(), T2BFSppCreatePort(), T2BFSppOpen(), T2BFStart(), T2BFWriteName(), T2BFWritePin(), UNISTR_CHARSET_ASCII, UNISTR_ENCODING_NONE, and UNISTRToUtf16().
Referenced by app_engine().
void AppEngineInquiryButton | ( | void | ) |
Handles functionality coupled to press of the Inquiry button.
None |
None |
References AppEngine_Idle_State, AppEngine_Inquiry_State, AppEngineNotifyCallback(), DEVICE_CLASS_ALL, myBytes, myIndex, myState, pMyBdAddress, pMyName, SERVICE_CLASS_ALL, status, T2BF_STATUS_OK, T2BFENG_MAX_NAME_LENGTH, T2BFENG_MAX_SEARCH_RESULT, T2BFENG_MAX_SEARCH_TIMEOUT, T2BFInquiryStart(), and T2BFInquiryStop().
Referenced by app_engine().
void AppEngineJoystickButton | ( | TAppEngineJoystick | joystick | ) |
Sends a letter for each direction on the joystick.
joystick | Identifies what direction the joystick has been pulled in. |
None. |
References AppEngine_Down, AppEngine_Left, AppEngine_Push, AppEngine_Right, AppEngine_Up, and AppEngineInternalSendData().
Referenced by app_engine().
void AppEngineSelectDeviceButton | ( | void | ) |
Handles functionality coupled to press of the Select button.
None |
None |
References AppEngine_Idle_State, AppEngineNotifyCallback(), i, myBdAddr, myIndex, myState, pMyBdAddress, pMyName, and T2BFENG_MAX_NAME_LENGTH.
Referenced by app_engine().