In this section you can find all the projects related to the TWI - Two-Wire Slave Interface.
TWIS Slave Example for uc3c_ek | |
Using the TWIS module, process read and write operations from/to a virtual memory space pre-allocated in internal RAM. To be used with two boards with the corresponding TWIM module example. |