EBI (External Bus Interface) SDRAM Controller allows to connect a SDRAM to the microcontroller.
Macros | |
#define | SDRAM ((void *)AVR32_EBI_CS1_ADDRESS) |
Pointer to SDRAM. More... | |
#define | SDRAM_BANK_BITS 2 |
The number of bank bits for this SDRAM (1 or 2). More... | |
#define | SDRAM_CAS 2 |
The minimal column address select (READ) latency for this SDRAM (1 to 3 SDRAM cycles). More... | |
#define | SDRAM_COL_BITS 9 |
The number of column bits for this SDRAM (8 to 11). More... | |
#define | SDRAM_INIT_AUTO_REFRESH_COUNT 2 |
The minimal number of AUTO REFRESH commands required during initialization for this SDRAM. More... | |
#define | SDRAM_ROW_BITS 13 |
The number of row bits for this SDRAM (11 to 13). More... | |
#define | SDRAM_SIZE |
SDRAM size. More... | |
#define | SDRAM_STABLE_CLOCK_INIT_DELAY 100 |
The minimal stable-clock initialization delay for this SDRAM. More... | |
#define | SDRAM_TMRD 2 |
The minimal mode register delay time for this SDRAM. More... | |
#define | SDRAM_TR 7812 |
The maximal refresh time for this SDRAM (0 to 4095 SDRAM cycles). More... | |
#define | SDRAM_TRAS 37 |
The minimal row address select time for this SDRAM (0 to 15 SDRAM cycles). More... | |
#define | SDRAM_TRC 60 |
The minimal row cycle time for this SDRAM (0 to 15 SDRAM cycles). More... | |
#define | SDRAM_TRCD 15 |
The minimal row to column delay time for this SDRAM (0 to 15 SDRAM cycles). More... | |
#define | SDRAM_TRFC 66 |
The minimal refresh cycle time for this SDRAM. More... | |
#define | SDRAM_TRP 15 |
The minimal row precharge time for this SDRAM (0 to 15 SDRAM cycles). More... | |
#define | SDRAM_TWR 14 |
The minimal write recovery time for this SDRAM (0 to 15 SDRAM cycles). More... | |
#define | SDRAM_TXSR 67 |
The minimal exit self refresh time for this SDRAM (0 to 15 SDRAM cycles). More... | |
Functions | |
void | sdram_enter_self_refresh (void) |
Set the SDRAM in self refresh mode. The SELF REFRESH command can be used to retain data in the SDRAM, even if the rest of the system is powered down. When in the self refresh mode, the SDRAM retains data without external clocking. More... | |
void | sdram_exit_self_refresh (void) |
Exit from the SDRAM self refresh mode, inhibits self refresh mode. More... | |
void | sdramc_init (unsigned long hsb_hz) |
Initializes the AVR32 SDRAM Controller and the connected SDRAM(s). More... | |
#define SDRAM ((void *)AVR32_EBI_CS1_ADDRESS) |
Pointer to SDRAM.
Referenced by main(), and sdramc_init().
#define SDRAM_BANK_BITS 2 |
The number of bank bits for this SDRAM (1 or 2).
#define SDRAM_CAS 2 |
The minimal column address select (READ) latency for this SDRAM (1 to 3 SDRAM cycles).
Unit: tCK (SDRAM cycle period).
#define SDRAM_COL_BITS 9 |
The number of column bits for this SDRAM (8 to 11).
#define SDRAM_INIT_AUTO_REFRESH_COUNT 2 |
The minimal number of AUTO REFRESH commands required during initialization for this SDRAM.
#define SDRAM_ROW_BITS 13 |
The number of row bits for this SDRAM (11 to 13).
#define SDRAM_SIZE |
SDRAM size.
Referenced by main().
#define SDRAM_STABLE_CLOCK_INIT_DELAY 100 |
The minimal stable-clock initialization delay for this SDRAM.
Unit: us.
#define SDRAM_TMRD 2 |
The minimal mode register delay time for this SDRAM.
LOAD MODE REGISTER command to ACTIVE or REFRESH command delay. Unit: tCK (SDRAM cycle period).
#define SDRAM_TR 7812 |
The maximal refresh time for this SDRAM (0 to 4095 SDRAM cycles).
Refresh period. Unit: ns.
#define SDRAM_TRAS 37 |
The minimal row address select time for this SDRAM (0 to 15 SDRAM cycles).
ACTIVE-to-PRECHARGE command delay. Unit: ns.
#define SDRAM_TRC 60 |
The minimal row cycle time for this SDRAM (0 to 15 SDRAM cycles).
ACTIVE-to-ACTIVE command delay. Unit: ns.
#define SDRAM_TRCD 15 |
The minimal row to column delay time for this SDRAM (0 to 15 SDRAM cycles).
ACTIVE-to-READ/WRITE command delay. Unit: ns.
#define SDRAM_TRFC 66 |
The minimal refresh cycle time for this SDRAM.
AUTO REFRESH command period. Unit: ns.
#define SDRAM_TRP 15 |
The minimal row precharge time for this SDRAM (0 to 15 SDRAM cycles).
PRECHARGE command period. Unit: ns.
#define SDRAM_TWR 14 |
The minimal write recovery time for this SDRAM (0 to 15 SDRAM cycles).
Unit: ns.
#define SDRAM_TXSR 67 |
The minimal exit self refresh time for this SDRAM (0 to 15 SDRAM cycles).
Exit SELF REFRESH to ACTIVE command delay. Unit: ns.
void sdram_enter_self_refresh | ( | void | ) |
Set the SDRAM in self refresh mode. The SELF REFRESH command can be used to retain data in the SDRAM, even if the rest of the system is powered down. When in the self refresh mode, the SDRAM retains data without external clocking.
void sdram_exit_self_refresh | ( | void | ) |
Exit from the SDRAM self refresh mode, inhibits self refresh mode.
void sdramc_init | ( | unsigned long | hsb_hz | ) |
Initializes the AVR32 SDRAM Controller and the connected SDRAM(s).
hsb_hz | HSB frequency in Hz (the HSB frequency is applied to the SDRAMC and to the SDRAM). |
References ATPASTE2, i, SDRAM, SDRAM_BANK_BITS, SDRAM_CAS, SDRAM_COL_BITS, SDRAM_INIT_AUTO_REFRESH_COUNT, SDRAM_ROW_BITS, SDRAM_STABLE_CLOCK_INIT_DELAY, SDRAM_TMRD, SDRAM_TR, SDRAM_TRAS, SDRAM_TRC, SDRAM_TRCD, SDRAM_TRFC, SDRAM_TRP, SDRAM_TWR, SDRAM_TXSR, sdramc_enable_muxed_pins(), sdramc_ns_delay, and sdramc_us_delay.
Referenced by main().