Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
MEMORY - EBI Static Memory Controller

EBI (External Bus Interface) SMC (Static Memory Controller) allows to connect a Static Memory to the microcontroller.

Macros

#define EXT_SM_SIZE   17
 SMC Peripheral Memory Size in log2(Bytes) More...
 
#define NCS_CONTROLLED_READ   false
 Whether read is controlled by NCS or by NRD. More...
 
#define NCS_CONTROLLED_WRITE   false
 Whether write is controlled by NCS or by NWE. More...
 
#define NCS_RD_HOLD   0
 Unit: ns. More...
 
#define NCS_RD_PULSE   82
 Unit: ns. More...
 
#define NCS_RD_SETUP   0
 Unit: ns. More...
 
#define NCS_WR_HOLD   82
 Unit: ns. More...
 
#define NCS_WR_PULSE   82
 Unit: ns. More...
 
#define NCS_WR_SETUP   0
 Unit: ns. More...
 
#define NRD_CYCLE   Max((NCS_RD_SETUP + NCS_RD_PULSE + NCS_RD_HOLD),(NRD_SETUP + NRD_PULSE + NRD_HOLD))
 
#define NRD_HOLD   0
 
#define NRD_PULSE   82
 Unit: ns. More...
 
#define NRD_SETUP   0
 Unit: ns. More...
 
#define NWAIT_MODE   AVR32_SMC_EXNW_MODE_DISABLED
 Whether to use the NWAIT pin. More...
 
#define NWE_CYCLE   Max((NCS_WR_SETUP + NCS_WR_PULSE + NCS_WR_HOLD),(NWE_SETUP + NWE_PULSE + NWE_HOLD))
 
#define NWE_HOLD   82
 
#define NWE_PULSE   82
 Unit: ns. More...
 
#define NWE_SETUP   0
 Unit: ns. More...
 
#define PAGE_MODE   false
 
#define PAGE_SIZE   0
 
#define SMC_8_BIT_CHIPS   false
 Whether 8-bit SM chips are connected on the SMC. More...
 
#define SMC_DBW   16
 SMC Data Bus Width. More...
 
#define TDF_CYCLES   0
 
#define TDF_OPTIM   false
 

Functions

unsigned char smc_get_cs_size (unsigned char cs)
 Return the size of the peripheral connected . More...
 
void smc_init (unsigned long hsb_hz)
 Initializes the AVR32 SMC module and the connected SRAM(s). More...
 

#define EXT_SM_SIZE   17

SMC Peripheral Memory Size in log2(Bytes)

#define NCS_CONTROLLED_READ   false

Whether read is controlled by NCS or by NRD.

#define NCS_CONTROLLED_WRITE   false

Whether write is controlled by NCS or by NWE.

#define NCS_RD_HOLD   0

Unit: ns.

#define NCS_RD_PULSE   82

Unit: ns.

#define NCS_RD_SETUP   0

Unit: ns.

#define NCS_WR_HOLD   82

Unit: ns.

#define NCS_WR_PULSE   82

Unit: ns.

#define NCS_WR_SETUP   0

Unit: ns.

#define NRD_CYCLE   Max((NCS_RD_SETUP + NCS_RD_PULSE + NCS_RD_HOLD),(NRD_SETUP + NRD_PULSE + NRD_HOLD))
#define NRD_HOLD   0
#define NRD_PULSE   82

Unit: ns.

#define NRD_SETUP   0

Unit: ns.

#define NWAIT_MODE   AVR32_SMC_EXNW_MODE_DISABLED

Whether to use the NWAIT pin.

#define NWE_CYCLE   Max((NCS_WR_SETUP + NCS_WR_PULSE + NCS_WR_HOLD),(NWE_SETUP + NWE_PULSE + NWE_HOLD))
#define NWE_HOLD   82
#define NWE_PULSE   82

Unit: ns.

#define NWE_SETUP   0

Unit: ns.

#define PAGE_MODE   false
#define PAGE_SIZE   0
#define SMC_8_BIT_CHIPS   false

Whether 8-bit SM chips are connected on the SMC.

#define SMC_DBW   16

SMC Data Bus Width.

#define TDF_CYCLES   0
#define TDF_OPTIM   false

unsigned char smc_get_cs_size ( unsigned char  cs)

Return the size of the peripheral connected .

Parameters
csThe chip select value

References smc_tab_cs_size.

void smc_init ( unsigned long  hsb_hz)

Initializes the AVR32 SMC module and the connected SRAM(s).

Parameters
hsb_hzHSB frequency in Hz (the HSB frequency is applied to the SMC).
Note
Each access to the SMC address space validates the mode of the SMC and generates an operation corresponding to this mode.

Whether to use the NCS0 pin

Whether to use the NCS1 pin

Whether to use the NCS2 pin

Whether to use the NCS3 pin

Whether to use the NCS4 pin

Whether to use the NCS5 pin

References SMC_CS_SETUP, and smc_enable_muxed_pins().

Referenced by et024006_Init().