Example of an interrupt-driven USART communication.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
#include <avr32/io.h>
#include "compiler.h"
#include "board.h"
#include "print_funcs.h"
#include "intc.h"
#include "power_clocks_lib.h"
#include "gpio.h"
#include "usart.h"
#include "conf_example.h"
Macros | |
#define | EXAMPLE_TARGET_PBACLK_FREQ_HZ FOSC0 |
#define | EXAMPLE_USART (&AVR32_USART1) |
#define | EXAMPLE_USART_BAUDRATE 115200 |
#define | EXAMPLE_USART_IRQ AVR32_USART1_IRQ |
#define | EXAMPLE_USART_RX_FUNCTION AVR32_USART1_RXD_0_FUNCTION |
#define | EXAMPLE_USART_RX_PIN AVR32_USART1_RXD_0_PIN |
#define | EXAMPLE_USART_TX_FUNCTION AVR32_USART1_TXD_0_FUNCTION |
#define | EXAMPLE_USART_TX_PIN AVR32_USART1_TXD_0_PIN |
Functions | |
int | main (void) |
The main function. More... | |
static void | usart_int_handler (void) |
The USART interrupt handler. More... | |
#define EXAMPLE_TARGET_PBACLK_FREQ_HZ FOSC0 |
Referenced by main().
#define EXAMPLE_USART (&AVR32_USART1) |
Referenced by main(), and usart_int_handler().
#define EXAMPLE_USART_BAUDRATE 115200 |
Referenced by main().
#define EXAMPLE_USART_IRQ AVR32_USART1_IRQ |
Referenced by main().
#define EXAMPLE_USART_RX_FUNCTION AVR32_USART1_RXD_0_FUNCTION |
Referenced by main().
#define EXAMPLE_USART_RX_PIN AVR32_USART1_RXD_0_PIN |
Referenced by main().
#define EXAMPLE_USART_TX_FUNCTION AVR32_USART1_TXD_0_FUNCTION |
Referenced by main().
#define EXAMPLE_USART_TX_PIN AVR32_USART1_TXD_0_PIN |
Referenced by main().
int main | ( | void | ) |
The main function.
It sets up the USART module on EXAMPLE_USART. The terminal settings are 57600 8N1. Then it sets up the interrupt handler and waits for a USART interrupt to trigger.
We have nothing left to do in the main, so we may switch to a device sleep mode: we just need to be sure that the USART module will be still be active in the chosen sleep mode. The sleep mode to use is the FROZEN sleep mode: in this mode the PB clocks are still active (so the USART module which is on the Peripheral Bus will still be
Modules communicating with external circuits should normally be disabled before entering a sleep mode that will stop the module
When the USART interrupt occurs, this will wake the CPU up which will then execute the interrupt handler code then come back to the while(1) loop below to execute the sleep instruction again.
References usart_options_t::baudrate, Disable_global_interrupt, Enable_global_interrupt, EXAMPLE_TARGET_PBACLK_FREQ_HZ, EXAMPLE_USART, EXAMPLE_USART_BAUDRATE, EXAMPLE_USART_IRQ, EXAMPLE_USART_RX_FUNCTION, EXAMPLE_USART_RX_PIN, EXAMPLE_USART_TX_FUNCTION, EXAMPLE_USART_TX_PIN, gpio_enable_module(), INTC_init_interrupts(), INTC_register_interrupt(), pcl_configure_clocks(), pcl_dfll_freq_param, PCL_OSC0, pcl_switch_to_osc(), print(), SLEEP, USART_1_STOPBIT, USART_GPIO_MAP, usart_init_rs232(), usart_int_handler(), USART_NO_PARITY, USART_NORMAL_CHMODE, and USART_OPTIONS.
|
static |
The USART interrupt handler.
References c, EXAMPLE_USART, usart_read_char(), and usart_write_char().
Referenced by main().