Copyright (C) 2006-2010, Brainspark B.V.
This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>
All rights reserved.
This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.
This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.
You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
#include "polarssl/bignum.h"
Data Structures | |
struct | rsa_context |
RSA context structure. More... | |
Functions | |
int | rsa_check_privkey (const rsa_context *ctx) |
Check a private RSA key. More... | |
int | rsa_check_pubkey (const rsa_context *ctx) |
Check a public RSA key. More... | |
void | rsa_free (rsa_context *ctx) |
Free the components of an RSA key. More... | |
int | rsa_gen_key (rsa_context *ctx, int(*f_rng)(void *), void *p_rng, int nbits, int exponent) |
Generate an RSA keypair. More... | |
void | rsa_init (rsa_context *ctx, int padding, int hash_id) |
Initialize an RSA context. More... | |
int | rsa_pkcs1_decrypt (rsa_context *ctx, int mode, int *olen, const unsigned char *input, unsigned char *output, int output_max_len) |
Do an RSA operation, then remove the message padding. More... | |
int | rsa_pkcs1_encrypt (rsa_context *ctx, int(*f_rng)(void *), void *p_rng, int mode, int ilen, const unsigned char *input, unsigned char *output) |
Add the message padding, then do an RSA operation. More... | |
int | rsa_pkcs1_sign (rsa_context *ctx, int mode, int hash_id, int hashlen, const unsigned char *hash, unsigned char *sig) |
Do a private RSA to sign a message digest. More... | |
int | rsa_pkcs1_verify (rsa_context *ctx, int mode, int hash_id, int hashlen, const unsigned char *hash, unsigned char *sig) |
Do a public RSA and check the message digest. More... | |
int | rsa_private (rsa_context *ctx, const unsigned char *input, unsigned char *output) |
Do an RSA private key operation. More... | |
int | rsa_public (rsa_context *ctx, const unsigned char *input, unsigned char *output) |
Do an RSA public key operation. More... | |
int | rsa_self_test (int verbose) |
Checkup routine. More... | |
#define ASN1_HASH_MDX |
#define ASN1_HASH_SHA1 |
#define ASN1_HASH_SHA2X |
#define ASN1_STR_CONSTRUCTED_SEQUENCE "\x30" |
#define ASN1_STR_NULL "\x05" |
#define ASN1_STR_OCTET_STRING "\x04" |
#define ASN1_STR_OID "\x06" |
#define OID_COUNTRY_US "\x86\x48" |
#define OID_DIGEST_ALG_MDX "\x2A\x86\x48\x86\xF7\x0D\x02\x00" |
#define OID_HASH_ALG_SHA1 "\x2b\x0e\x03\x02\x1a" |
#define OID_HASH_ALG_SHA2X "\x60\x86\x48\x01\x65\x03\x04\x02\x00" |
#define OID_ISO_IDENTIFIED_ORG "\x2b" |
#define OID_ISO_MEMBER_BODIES "\x2a" |
#define OID_OIW_SECSIG_SHA1 "\x0e\x03\x02\x1a" |
#define OID_RSA_DATA_SECURITY "\x86\xf7\x0d" |
#define POLARSSL_ERR_RSA_BAD_INPUT_DATA -0x0400 |
#define POLARSSL_ERR_RSA_INVALID_PADDING -0x0410 |
#define POLARSSL_ERR_RSA_KEY_CHECK_FAILED -0x0430 |
#define POLARSSL_ERR_RSA_KEY_GEN_FAILED -0x0420 |
#define POLARSSL_ERR_RSA_OUTPUT_TOO_LARGE -0x0470 |
#define POLARSSL_ERR_RSA_PRIVATE_FAILED -0x0450 |
#define POLARSSL_ERR_RSA_PUBLIC_FAILED -0x0440 |
#define POLARSSL_ERR_RSA_RNG_FAILED -0x0480 |
#define POLARSSL_ERR_RSA_VERIFY_FAILED -0x0460 |
#define RSA_CRYPT 2 |
#define RSA_PKCS_V15 0 |
#define RSA_PKCS_V21 1 |
#define RSA_PRIVATE 1 |
Referenced by RSA_private_decrypt(), and RSA_private_encrypt().
#define RSA_PUBLIC 0 |
Referenced by RSA_public_decrypt(), and RSA_public_encrypt().
#define RSA_SIGN 1 |
#define SIG_RSA_MD2 2 |
#define SIG_RSA_MD4 3 |
#define SIG_RSA_MD5 4 |
#define SIG_RSA_RAW 0 |
#define SIG_RSA_SHA1 5 |
#define SIG_RSA_SHA224 14 |
#define SIG_RSA_SHA256 11 |
#define SIG_RSA_SHA384 12 |
#define SIG_RSA_SHA512 13 |
int rsa_check_privkey | ( | const rsa_context * | ctx | ) |
Check a private RSA key.
ctx | RSA context to be checked |
int rsa_check_pubkey | ( | const rsa_context * | ctx | ) |
Check a public RSA key.
ctx | RSA context to be checked |
void rsa_free | ( | rsa_context * | ctx | ) |
Free the components of an RSA key.
ctx | RSA Context to free |
int rsa_gen_key | ( | rsa_context * | ctx, |
int(*)(void *) | f_rng, | ||
void * | p_rng, | ||
int | nbits, | ||
int | exponent | ||
) |
Generate an RSA keypair.
ctx | RSA context that will hold the key |
f_rng | RNG function |
p_rng | RNG parameter |
nbits | size of the public key in bits |
exponent | public exponent (e.g., 65537) |
void rsa_init | ( | rsa_context * | ctx, |
int | padding, | ||
int | hash_id | ||
) |
Initialize an RSA context.
ctx | RSA context to be initialized |
padding | RSA_PKCS_V15 or RSA_PKCS_V21 |
hash_id | RSA_PKCS_V21 hash identifier |
int rsa_pkcs1_decrypt | ( | rsa_context * | ctx, |
int | mode, | ||
int * | olen, | ||
const unsigned char * | input, | ||
unsigned char * | output, | ||
int | output_max_len | ||
) |
Do an RSA operation, then remove the message padding.
ctx | RSA context |
mode | RSA_PUBLIC or RSA_PRIVATE |
input | buffer holding the encrypted data |
output | buffer that will hold the plaintext |
olen | will contain the plaintext length |
output_max_len | maximum length of the output buffer |
Referenced by RSA_private_decrypt(), and RSA_public_decrypt().
int rsa_pkcs1_encrypt | ( | rsa_context * | ctx, |
int(*)(void *) | f_rng, | ||
void * | p_rng, | ||
int | mode, | ||
int | ilen, | ||
const unsigned char * | input, | ||
unsigned char * | output | ||
) |
Add the message padding, then do an RSA operation.
ctx | RSA context |
f_rng | RNG function |
p_rng | RNG parameter |
mode | RSA_PUBLIC or RSA_PRIVATE |
ilen | contains the plaintext length |
input | buffer holding the data to be encrypted |
output | buffer that will hold the ciphertext |
Referenced by RSA_private_encrypt(), and RSA_public_encrypt().
int rsa_pkcs1_sign | ( | rsa_context * | ctx, |
int | mode, | ||
int | hash_id, | ||
int | hashlen, | ||
const unsigned char * | hash, | ||
unsigned char * | sig | ||
) |
Do a private RSA to sign a message digest.
ctx | RSA context |
mode | RSA_PUBLIC or RSA_PRIVATE |
hash_id | SIG_RSA_RAW, SIG_RSA_MD{2,4,5} or SIG_RSA_SHA{1,224,256,384,512} |
hashlen | message digest length (for SIG_RSA_RAW only) |
hash | buffer holding the message digest |
sig | buffer that will hold the ciphertext |
int rsa_pkcs1_verify | ( | rsa_context * | ctx, |
int | mode, | ||
int | hash_id, | ||
int | hashlen, | ||
const unsigned char * | hash, | ||
unsigned char * | sig | ||
) |
Do a public RSA and check the message digest.
ctx | points to an RSA public key |
mode | RSA_PUBLIC or RSA_PRIVATE |
hash_id | SIG_RSA_RAW, SIG_RSA_MD{2,4,5} or SIG_RSA_SHA{1,224,256,384,512} |
hashlen | message digest length (for SIG_RSA_RAW only) |
hash | buffer holding the message digest |
sig | buffer holding the ciphertext |
int rsa_private | ( | rsa_context * | ctx, |
const unsigned char * | input, | ||
unsigned char * | output | ||
) |
Do an RSA private key operation.
ctx | RSA context |
input | input buffer |
output | output buffer |
int rsa_public | ( | rsa_context * | ctx, |
const unsigned char * | input, | ||
unsigned char * | output | ||
) |
Do an RSA public key operation.
ctx | RSA context |
input | input buffer |
output | output buffer |
int rsa_self_test | ( | int | verbose | ) |
Checkup routine.