USB Device Atmel Firmware Upgrade (DFU) interface definitions.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "conf_usb.h"
#include "usb_protocol.h"
#include "usb_protocol_dfu.h"
#include "udd.h"
#include "udc.h"
#include "udi_dfu_atmel.h"
#include "conf_isp.h"
#include "isp.h"
#include "flip_protocol.h"
#include "string.h"
Macros | |
#define | CAT_CMD(val1, val2) (((uint16_t)val1<<8)|(val2<<0)) |
Macro to simplify and to optimize command decode process. More... | |
Functions | |
void | udi_dfu_atmel_disable (void) |
bool | udi_dfu_atmel_enable (void) |
uint8_t | udi_dfu_atmel_getsetting (void) |
static void | udi_dfu_atmel_mem_check (void) |
Process a blank check on memory. More... | |
static bool | udi_dfu_atmel_mem_getaddr (uint8_t *arg) |
Gets a memory address in a Atmel DFU command. More... | |
static bool | udi_dfu_atmel_mem_protected (void) |
Change DFU status to notify that the memory is protected. More... | |
static bool | udi_dfu_atmel_mem_read (void) |
Reads memory and transfer data to USB interface. More... | |
static bool | udi_dfu_atmel_mem_send_last_add (void) |
Send address which has failed during check memory. More... | |
static bool | udi_dfu_atmel_mem_write (void) |
Writes memory with data from USB interface. More... | |
static void | udi_dfu_atmel_sel_mem (uint8_t mem_num) |
Selects the memory. More... | |
bool | udi_dfu_atmel_setup (void) |
Internal routines to manage DFU requests | |
static void | udi_dfu_atmel_reset_protocol (void) |
Resets DFU status and usb setup process callbacks. More... | |
static bool | udi_dfu_flip_msg_decode (void) |
Decodes the Atmel DFU Command Called by over_under_run callback when the first data packet from a DNLOAD DFU request is received. More... | |
Manages Atmel DFU command from protocol version 2 | |
static bool | udi_dfu_atmel_program (void) |
Decodes and prepares program memory command. More... | |
static bool | udi_dfu_atmel_read (void) |
Decodes and prepares read memory command. More... | |
static bool | udi_dfu_atmel_blankcheck (void) |
Decodes and process blank check memory command. More... | |
static bool | udi_dfu_atmel_erase_chip (void) |
Decodes and process erase chip command. More... | |
static void | udi_dfu_atmel_start (void) |
Decodes and prepares CPU reset command. More... | |
static bool | udi_dfu_atmel_select_memory (void) |
Decodes and process memory select command. More... | |
Variables | |
UDC_DESC_STORAGE udi_api_t | udi_api_dfu_atmel |
Global structure which contains standard UDI interface for UDC. More... | |
To manage memories | |
static bool | udi_dfu_atmel_mem_b_protected |
Flag to signal that memory is write protected. More... | |
static isp_addr_t | udi_dfu_atmel_mem_add |
Memory address to read, write or check blank. More... | |
static isp_addr_t | udi_dfu_atmel_mem_nb_data |
Number of data to process during read, write or check blank. More... | |
static isp_mem_t | udi_dfu_atmel_mem_sel |
Memory ID selected to read, write or check blank. More... | |
Internal variables to manage DFU requests | |
#define | DFU_ATMEL_BUF_TRANS_SIZE FLIP_V2_BUF_TRANS_SIZE |
static dfu_status_t | udi_dfu_atmel_status |
Status of DFU process. More... | |
union { | |
flip_msg_v2_t msg | |
uint8_t payload [USB_DEVICE_EP_CTRL_SIZE] | |
} | udi_dfu_flip_msg |
Structure to store the command fields. More... | |
static COMPILER_WORD_ALIGNED uint8_t | udi_dfu_atmel_buf_trans [DFU_ATMEL_BUF_TRANS_SIZE] |
Buffer to receive or send data. More... | |
static bool(* | udi_dfu_atmel_upload_callback )(void) |
Callback to use when an upload request is received. More... | |
static bool | udi_dfu_atmel_reset |
Notify a reset request to start. More... | |
static bool | udi_dfu_atmel_security |
Store the current security level. More... | |
#define CAT_CMD | ( | val1, | |
val2 | |||
) | (((uint16_t)val1<<8)|(val2<<0)) |
Macro to simplify and to optimize command decode process.
Referenced by udi_dfu_flip_msg_decode().
#define DFU_ATMEL_BUF_TRANS_SIZE FLIP_V2_BUF_TRANS_SIZE |
Referenced by udi_dfu_atmel_mem_check(), udi_dfu_atmel_mem_read(), udi_dfu_atmel_mem_write(), and udi_dfu_atmel_program().
flip_msg_v2_t msg |
Referenced by tcpip_callback_with_block(), tcpip_callbackmsg_new(), tcpip_input(), tcpip_thread(), tcpip_timeout(), and tcpip_untimeout().
uint8_t payload[USB_DEVICE_EP_CTRL_SIZE] |
Referenced by COMPILER_ALIGNED(), pbuf_header(), udd_set_setup_payload(), uhd_setup_request(), and uhi_msc_scsi().
|
static |
Buffer to receive or send data.
Referenced by udi_dfu_atmel_mem_check(), udi_dfu_atmel_mem_read(), udi_dfu_atmel_mem_send_last_add(), udi_dfu_atmel_mem_write(), and udi_dfu_atmel_program().
|
static |
Memory address to read, write or check blank.
Referenced by udi_dfu_atmel_mem_check(), udi_dfu_atmel_mem_getaddr(), udi_dfu_atmel_mem_read(), udi_dfu_atmel_mem_send_last_add(), udi_dfu_atmel_mem_write(), and udi_dfu_atmel_select_memory().
|
static |
Flag to signal that memory is write protected.
Referenced by udi_dfu_atmel_program(), udi_dfu_atmel_read(), and udi_dfu_atmel_sel_mem().
|
static |
Number of data to process during read, write or check blank.
Referenced by udi_dfu_atmel_mem_check(), udi_dfu_atmel_mem_getaddr(), udi_dfu_atmel_mem_read(), and udi_dfu_atmel_mem_write().
|
static |
Memory ID selected to read, write or check blank.
|
static |
Notify a reset request to start.
Referenced by udi_dfu_atmel_enable(), udi_dfu_atmel_setup(), and udi_dfu_atmel_start().
|
static |
Store the current security level.
Referenced by udi_dfu_atmel_enable(), udi_dfu_atmel_erase_chip(), udi_dfu_atmel_program(), and udi_dfu_atmel_read().
|
static |
Status of DFU process.
|
static |
Callback to use when an upload request is received.
Referenced by udi_dfu_atmel_mem_check(), udi_dfu_atmel_read(), udi_dfu_atmel_setup(), and udi_dfu_flip_msg_decode().
union { ... } udi_dfu_flip_msg |
Structure to store the command fields.
Referenced by udi_dfu_atmel_blankcheck(), udi_dfu_atmel_erase_chip(), udi_dfu_atmel_program(), udi_dfu_atmel_read(), udi_dfu_atmel_select_memory(), udi_dfu_atmel_setup(), udi_dfu_atmel_start(), and udi_dfu_flip_msg_decode().