Copyright (C) 2006-2010, Brainspark B.V.
This file is part of PolarSSL (http://www.polarssl.org) Lead Maintainer: Paul Bakker <polarssl_maintainer at polarssl.org>
All rights reserved.
This program is free software; you can redistribute it and/or modify it under the terms of the GNU General Public License as published by the Free Software Foundation; either version 2 of the License, or (at your option) any later version.
This program is distributed in the hope that it will be useful, but WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.
You should have received a copy of the GNU General Public License along with this program; if not, write to the Free Software Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301 USA.
#include <inttypes.h>
Data Structures | |
struct | xtea_context |
XTEA context structure. More... | |
Macros | |
#define | XTEA_DECRYPT 0 |
#define | XTEA_ENCRYPT 1 |
Functions | |
int | xtea_crypt_ecb (xtea_context *ctx, int mode, unsigned char input[8], unsigned char output[8]) |
XTEA cipher function. More... | |
int | xtea_self_test (int verbose) |
void | xtea_setup (xtea_context *ctx, unsigned char key[16]) |
XTEA key schedule. More... | |
#define XTEA_DECRYPT 0 |
#define XTEA_ENCRYPT 1 |
int xtea_crypt_ecb | ( | xtea_context * | ctx, |
int | mode, | ||
unsigned char | input[8], | ||
unsigned char | output[8] | ||
) |
XTEA cipher function.
ctx | XTEA context |
mode | XTEA_ENCRYPT or XTEA_DECRYPT |
input | 8-byte input block |
output | 8-byte output block |
int xtea_self_test | ( | int | verbose | ) |
void xtea_setup | ( | xtea_context * | ctx, |
unsigned char | key[16] | ||
) |
XTEA key schedule.
ctx | XTEA context to be initialized |
key | the secret key |