In this section you can find all the projects related to the FLASHCDW - FLASH Controller Double-Word.
FLASHCDW Example for STK600_RCUC3L0 | |
Use the FLASHCDW, read and write data to the internal flash, using a flash block as an NVRAM, located either in the flash array or in the Flash User Page. | |
FLASHCDW Example for uc3l_ek | |
Use the FLASHCDW, read and write data to the internal flash, using a flash block as an NVRAM, located either in the flash array or in the Flash User Page. |