Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
Related Pages
Here is a list of all related documentation pages:
[detail level 12]
oLicenseCopyright (c) 2017-2018 Microchip Technology Inc
oQuick start guide for Serial Interface serviceThis is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases
|\Advanced use case - Send a packet of serial dataIn this use case, the USART module is configured for:
oQuick start guide for USB device Mass Storage module (UDI MSC)This is the quick start guide for the USB device interface MSC module (UDI MSC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oMSC in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oQuick start guide for USB device mouse module (UDI mouse)This is the quick start guide for the USB device mouse module (UDI mouse) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oHID mouse in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oQuick start guide for First-In-First-Out Buffer (FIFO)This is the quick start guide for the First-In-First-Out Buffer (FIFO), with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Push and flushIn this use case, two elements will be pushed to the FIFO, and the FIFO will be flushed
oQuick Start quide for common NVM driverThis is the quick start quide for the Common NVM driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick start guide for USB device generic module (UDI generic)This is the quick start guide for the USB device generic module (UDI generic) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oHID generic in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oconf_clock.h examples with USB supportContent of XMEGA conf_clock.h:
oQuickstart guide for AT25DFx component.This is the quickstart guide for the AT25DFx SerialFlash component, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick start guide for QTouch componentThis is the quick start guide for the QTouch device driver for I2C interface, with step-by-step instructions on how to configure and use the driver for a specific use case
oQuick start guide for USB device multi-touch module (UDI Multi-touch)
oQuick Start Guide for the System Clock Management service (UC3L)This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases
oxTaskHandleTask
otaskYIELDTask
otaskENTER_CRITICALTask
otaskEXIT_CRITICALTask
otaskDISABLE_INTERRUPTSTask
otaskENABLE_INTERRUPTSTask
oxTaskGetTickCountTask
ouxTaskGetNumberOfTasksTask
ovTaskListTask
ovTaskGetRunTimeStatsTask
ovTaskStartTraceTask
ousTaskEndTraceTask
ouxQueueMessagesWaitingQueue
ovQueueDeleteQueue
oQuick start guide for USB Device Vendor module (UDI Vendor)This is the quick start guide for the USB device interface Vendor module (UDI Vendor) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oVendor in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oQuick start guide for USB device Communication Class Device module (UDI CDC)This is the quick start guide for the USB device interface CDC module (UDI CDC) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oCDC in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oQuick start guide for USB device keyboard module (UDI keyboard)This is the quick start guide for the USB device keyboard module (UDI keyboard) with step-by-step instructions on how to configure and use the modules in a selection of use cases
|oHID keyboard in a composite deviceA USB Composite Device is a USB Device which uses more than one USB class
|oChange USB speedIn this use case, the USB device is used with different USB speeds
|oUse USB stringsIn this use case, the usual USB strings is added in the USB device
|oUse USB remote wakeup featureIn this use case, the USB remote wakeup feature is enabled
|oBus power application recommendationsIn this use case, the USB device BUS power feature is enabled
|\USB dynamic serial numberIn this use case, the USB serial strings is dynamic
oQuick Start Guide for the SPI Master DriverThis is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case
|\Basic setup for SPI master on XMEGA devices
oQuick start guide for SPI master on UC3 devices
oQuick start guide for SPI driver on AVR32 devicesThis is the quick start guide for the SPI - Serial Peripheral Interface, with step-by-step instructions on how to configure and use the driver for a specific use case
oQuick start guide for the maXTouch componentThis is the quick start guide for the maXTouch component The guide will give you a step-by-step introduction on how to setup and use the component to be able to read touch responses from the maXTouch Xplained kit
oQuick Start Guide for the ILI9341 Display Controller Component DriverThis is the quick start guide for the ILI9341 Display Controller Component Driver, with step-by-step instructions on how to configure and use the component driver for specific use cases
odeath.cCreate a single persistent task which periodically dynamically creates another two tasks
oQuick start guide for the common IOPORT serviceThis is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases
|\Advanced use case doing port accessIn this case we will read out the pins from one whole port and write the read value to another port
oQuickstart guide for Common service TWIThis is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick start guide for Calendar serviceThis is the quick start guide for the Calendar service, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Calculate time between datesThe use case will let the user calculate the time between two dates, by first calculating the dates from two timestamps
oQuick start guide for reset cause serviceThis is the quick start guide for the Reset Cause service, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Use case #1In this use case, the reset cause service is used to perform a software controlled reset
oQuick Start Guide for the graphics serviceThis is the quick start guide for the Graphics (GFX) service", with step-by-step instructions on how to configure and use it for a specific use case
oTodo List
\Deprecated List