In this section you can find all the projects related to the PWMA - Pulse Width Modulation A.
PWMA Example 1 for STK600-RCUC3L3 | |
Using PWMA module, generating wavefrom to two different channels and updating the duty cycle values using Interlinked multi-value mode. Timebase overflow interrupt is enabled which gets triggered whenever overflow occurs. | |
PWMA Example 1 for STK600_RCUC3L0 | |
Using PWMA module, generating wavefrom to two different channels and updating the duty cycle values using Interlinked multi-value mode. Timebase overflow interrupt is enabled which gets triggered whenever overflow occurs. | |
PWMA Example 1 for UC3_L0_XPLAINED | |
Using PWMA module, generating wavefrom to two different channels and updating the duty cycle values using Interlinked multi-value mode. Timebase overflow interrupt is enabled which gets triggered whenever overflow occurs. | |
PWMA Example 1 for UC3L-EK | |
Using PWMA module, generating wavefrom to two different channels and updating the duty cycle values using Interlinked multi-value mode. Timebase overflow interrupt is enabled which gets triggered whenever overflow occurs. | |
PWMA Example 2 for STK600-RCUC3L3 | |
Using Analog Comparator increasing/decreasing the duty cycle of the PWMA Module by enabling the Peripheral Event System in PWMA. | |
PWMA Example 2 for STK600_RCUC3L0 | |
Using Analog Comparator increasing/decreasing the duty cycle of the PWMA Module by enabling the Peripheral Event System in PWMA. | |
PWMA Example 2 for UC3_L0_XPLAINED | |
Using Analog Comparator increasing/decreasing the duty cycle of the PWMA Module by enabling the Peripheral Event System in PWMA. | |
PWMA Example 2 for UC3L-EK | |
Using Analog Comparator increasing/decreasing the duty cycle of the PWMA Module by enabling the Peripheral Event System in PWMA. |