Introduction
This example demonstrates how to use the Serial Stdio.
Main Files
- stdio_serial_example.c: the example application.
- conf_board.h: board configuration
- conf_clock.h: clock configuration
- conf_usart_serial.h: configuration of the stdio serial used by this example
- stdio_serial.h: Part Specific Stdio Serial Implementation
- read.c : System implementation function used by standard library
- write.c : System implementation function used by standard library
utils/stdio/stdio_serial API
The stdio_serial API can be found here.
Device Support
All Atmel devices can be used. This example has been tested with the following setup:
- ATXMEGA128A1 XMEGA-A1 Xplained (USB connection to host virtual com port).
- AT32UC3L064 UC3-L0 Xplained (USB connection to host virtual com port).
- SAM4E evaluation kit.
Description of the example
- Send message on serial communication port.
- Performs echo of any received character
Compiler Support
This software was written for the GNU GCC and IAR for AVR and ARM. Other compilers may or may not work.
Contact Information
For further information, visit Microchip.