Definitions and settings for the CRC hardware module driver.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
NVM Commands | |
NVM commands for 32-bit CRC of flash memory. These are only used by CLASSB_CRC32_Flash_HW. | |
#define | CRC_FLASH_RANGE NVM_CMD_FLASH_RANGE_CRC_gc |
Compute a CRC checksum on an address range. More... | |
#define | CRC_BOOT NVM_CMD_BOOT_CRC_gc |
Compute a CRC checksum on the application section. More... | |
#define | CRC_APP NVM_CMD_APP_CRC_gc |
Compute a CRC checksum on the boot section. More... | |
Enumerations | |
enum | crc_16_32_t { CRC_16BIT, CRC_32BIT } |
Enum for indicating whether to use 16- or 32-bits CRC. More... | |
Functions | |
CRC tests | |
Invariant memory tests based on CRC that are compliant with IEC60730 Class B. | |
uint16_t | CLASSB_CRC16_EEPROM_HW (eepromptr_t dataptr, const crcbytenum_t numBytes, eeprom_uint16ptr_t pchecksum) |
Compute 16-bit CRC for EEPROM address range using hardware CRC module. More... | |
uint16_t | CLASSB_CRC16_Flash_HW (flashptr_t dataptr, const crcbytenum_t numBytes, eeprom_uint16ptr_t pchecksum) |
Compute 16-bit CRC for Flash address range using hardware CRC module. More... | |
uint32_t | CLASSB_CRC32_EEPROM_HW (eepromptr_t dataptr, const crcbytenum_t numBytes, eeprom_uint32ptr_t pchecksum) |
Compute 32-bit CRC for EEPROM address range using hardware CRC module. More... | |
uint32_t | CLASSB_CRC32_Flash_HW (NVM_CMD_t crc_type, flashptr_t dataptr, const crcbytenum_t numBytes, eeprom_uint32ptr_t pchecksum) |
Compute 32-bit CRC for Flash address range using hardware CRC module. More... | |
Internal functions | |
These are functions from the CRC module driver. | |
void | crc_set_initial_value (uint32_t value) |
Set initial CRC value for next CRC calculation. More... | |
void | crc32_append_value (uint32_t value, void *ptr) |
Get and append data to generate checksum zero with CRC32. More... | |
void | crc16_append_value (uint16_t value, void *ptr) |
Appends a CRC value to the given pointer. More... | |
uint32_t | crc_flash_checksum (NVM_CMD_t crc_type, flash_addr_t flash_addr, uint32_t len) |
Perform a CRC-32 calculation on part of or entire flash. More... | |
uint32_t | crc_io_checksum (void *data, uint16_t len, enum crc_16_32_t crc_16_32) |
Calculate the CRC checksum for data in a buffer. More... | |
void | crc_io_checksum_byte_start (enum crc_16_32_t crc_16_32) |
Reset CRC module and set source to I/O interface. More... | |
void | crc_io_checksum_byte_add (uint8_t data) |
Add one byte of data to CRC performed on I/O interface. More... | |
uint32_t | crc_io_checksum_byte_stop (void) |
Disable CRC module and return checksum. More... | |
void | nvm_issue_flash_range_crc (flash_addr_t start_addr, flash_addr_t end_addr) |
Issue flash range CRC command. More... | |