Class B Oven User Interface.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <asf.h>
Functions | |
bool | oven_ui_back_button_is_pressed (void) |
Report whether the back button has been pressed and released. More... | |
void | oven_ui_draw_axis (void) |
Draw vertical and horizontal axis. More... | |
void | oven_ui_draw_plot_step (const uint8_t y1, const uint8_t y2) |
Plot a simulation time-step of the cooking plate and pot contents. More... | |
bool | oven_ui_power_button_is_pressed (void) |
Report whether the power button has been pressed and released. More... | |
void | oven_ui_set_status_leds (enum status_led s) |
Set the status LED to specified color. More... | |
void | oven_ui_update_graphics (enum pot_t potstate, uint8_t wattage, bool power) |
Update user interface elements. More... | |
bool oven_ui_back_button_is_pressed | ( | void | ) |
Report whether the back button has been pressed and released.
References gpio_pin_is_high, gpio_pin_is_low, and GPIO_PUSH_BUTTON_0.
Referenced by main().
void oven_ui_draw_axis | ( | void | ) |
Draw vertical and horizontal axis.
References gfx_mono_generic_draw_line(), and GFX_PIXEL_SET.
Referenced by main(), and oven_ui_draw_plot_step().
void oven_ui_draw_plot_step | ( | const uint8_t | y1, |
const uint8_t | y2 | ||
) |
Plot a simulation time-step of the cooking plate and pot contents.
The input values must be between 0 and 32 to fit inside the display.
y1 | Temperature of pot |
y2 | Temperature of plate |
References gfx_mono_draw_filled_rect, gfx_mono_generic_draw_line(), GFX_PIXEL_CLR, GFX_PIXEL_SET, OVEN_DISP_MAX_Y, OVEN_PLOT_MAX_X, OVEN_PLOT_MAX_Y, OVEN_PLOT_MIN_Y, OVEN_PLOT_OFFSET_X, and oven_ui_draw_axis().
Referenced by main_execute_simulation_step().
bool oven_ui_power_button_is_pressed | ( | void | ) |
Report whether the power button has been pressed and released.
References gpio_pin_is_high, gpio_pin_is_low, and GPIO_PUSH_BUTTON_1.
Referenced by main().
void oven_ui_set_status_leds | ( | enum status_led | s | ) |
Set the status LED to specified color.
Referenced by main(), and oven_classb_run_tests().
Update user interface elements.
Draw bitmap representing state of Q-Touch button as a pot on a plate, and a vertical bar representing the selected power level and whether the plate element is being actuated.
potstate | Whether a pot is detected |
wattage | Power level |
power | Whether power is applied |
References bitmap_pot_off, bitmap_pot_on, gfx_mono_draw_filled_rect, gfx_mono_put_bitmap, GFX_PIXEL_CLR, GFX_PIXEL_SET, max, MAX_WATTAGE, min, and POT_ON.
Referenced by main().