The use case will let the user calculate the time between two dates, by first calculating the dates from two timestamps.
For the code of this use case to work, the following must be added to the project:
No setup code is needed, the service is ready for use as-is.
Add to, e.g. the main loop in the application C-file: