Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
Related Pages
Here is a list of all related documentation pages:
[detail level 12]
oLicenseCopyright (c) 2017-2018 Microchip Technology Inc
oLicenseCopyright (c) 2014-2018 Microchip Technology Inc
oQuickstart guide for Common service TWIThis is the quickstart guide for the Common service TWI, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick start guide for First-In-First-Out Buffer (FIFO)This is the quick start guide for the First-In-First-Out Buffer (FIFO), with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Push and flushIn this use case, two elements will be pushed to the FIFO, and the FIFO will be flushed
oQuick start guide for the XMEGA DMA driverThis is the quick start guide for the DMA driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|oUse case #1 - Interrupt for a completed DMA transfer.This use case shows how to set up an interrupt for when a DMA transfer is completed
|\Use case #2 - Event driven DMA transfer from a peripheral.This use case shows how to set up a burst DMA transfer between a peripheral register set and the main system memory
oQuick start guide for QTouch componentThis is the quick start guide for the QTouch device driver for I2C interface, with step-by-step instructions on how to configure and use the driver for a specific use case
oQuick start guide for Timeout serviceThis is the quick start guide for the Timeout service XMEGA, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Debounce filter on a buttonIn this use case, a simple debounce filter on a button will be set up
oQuick start guide for XMEGA TWI driverThis is the quick start guide for the TWI Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
|\XMEGA E TWI additions with Bridge and Fast Mode PlusXMEGA E TWI module provides two additionnnal features compare to regular XMEGA TWI module:
oQuick start guide for WDT driverThis is the quick start guide for the Watchdog Timer (WDT), with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Reset WDT in window modeIn this use case, the WDT is configured for:
oQuick start guide for the XMEGA AC driverThis is the quick start guide for the AC Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oQuick start guide for reset cause serviceThis is the quick start guide for the Reset Cause service, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Use case #1In this use case, the reset cause service is used to perform a software controlled reset
oQuick start guide for XMEGA DES driverThis is the quick start guide for the DES Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oQuick Start quide for common NVM driverThis is the quick start quide for the Common NVM driver, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick Start Guide for the mono graphics serviceThis is the quick start guide for the Monochrome Graphics service, with step-by-step instructions on how to configure and use it for a specific use case
oQuick start guide for PMIC driverThis is the quick start guide for the PMIC driver and the closely related global interrupt driver, with step-by-step instructions on how to configure and use the drivers in a selection of use cases
|\Use case #1In this use case, the PMIC is configured for:
oQuickstart guide for AT25DFx component.This is the quickstart guide for the AT25DFx SerialFlash component, with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick Start Guide for the XMEGA QDEC DriverThis is the quick start guide for the XMEGA Quadrature Decoder (QDEC) , with step-by-step instructions on how to configure and use the driver in a selection of use cases
oQuick start guide for CCP driverThis is the quick start guide for the Configuration Change Protection (CCP) driver, with step-by-step instructions on how to use the driver
oQuick Start Guide for the System Clock Management service (XMEGA)This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases
oAdvanced use case - Peripheral Bus Clock Management (XMEGA)
oAdvanced use case - DFLL auto-calibration (XMEGA)
oQuick start guide for XMEGA DACThis is the quick start guide for the Digital to Analog Converter (DAC), with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\DA conversions on two channelsIn this use case, the DAC module is configured for:
oQuickstart guide for AVR XMEGA PWM serviceThis is the quickstart guide for the XMEGA Pulse Width Modulation (PWM) service, with step-by-step instructions on how to configure and use the service in a selection of use cases
|\Use case #1In this use case the PWM module is configured with overflow interrupt
oQuick start guide for the common IOPORT serviceThis is the quick start guide for the Common IOPORT API, with step-by-step instructions on how to configure and use the service in a selection of use cases
|\Advanced use case doing port accessIn this case we will read out the pins from one whole port and write the read value to another port
oQuick Start Guide for the XMEGA NVM DriverThis is the quick start guide for the NVM Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oQuick start guide for the maXTouch componentThis is the quick start guide for the maXTouch component The guide will give you a step-by-step introduction on how to setup and use the component to be able to read touch responses from the maXTouch Xplained kit
oQuick start guide for XMEGA AES driverThis is the quick start guide for the AES Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oQuick Start Guide for the SPI Master DriverThis is the quick start guide for the SPI Driver, with step-by-step instructions on how to configure and use the driver for a specific use case
|\Basic setup for SPI master on XMEGA devices
oQuick start guide for USART moduleThis is the quick start guide for the USART module, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\USART receive character and echo backIn this use case, the USART module is configured for:
oQuick start guide for Calendar serviceThis is the quick start guide for the Calendar service, with step-by-step instructions on how to configure and use the driver in a selection of use cases
|\Calculate time between datesThe use case will let the user calculate the time between two dates, by first calculating the dates from two timestamps
oQuick start guide for the AT30TSThis is the quick start guide for the AT30TS Temperature Sensor Library, with step-by-step instructions on how to configure and use the driver
oQuick start guide for RTC32 driverThis is the quick start guide for the RTC32 driver, with step-by-step instructions on how to configure and use the drivers in a selection of use cases
|\Use case #1This use case shows how to set an alarm for the RTC32
oQuick Start Guide for the ILI9341 Display Controller Component DriverThis is the quick start guide for the ILI9341 Display Controller Component Driver, with step-by-step instructions on how to configure and use the component driver for specific use cases
oQuick start guide for XMEGA ADCThis is the quick start guide for the Analog to Digital Converter (ADC), with step-by-step instructions on how to configure and use the driver in a selection of use cases
|oFree-running conversions with interruptIn this use case, ADCA is configured for:
|\Event-triggered conversionsIn this use case, ADCA is configured for:
oQuick Start Guide for the XMEGA EBI DriverThis is the quick start guide for the EBI Driver, with step-by-step instructions on how to configure and use the driver for specific use cases
oQuick start guide for RTC driverThis is the quick start guide for the RTC driver, with step-by-step instructions on how to configure and use the drivers in a selection of use cases
|\Use case #1In this use case, the RTC is configured for:
oQuick Start Guide for the XMEGA Sleep DriverThis is the quick start guide for the Sleep Driver, with step-by-step instructions on how to configure and use the driver for a specific use case
oQuick Start Guide for the XMEGA TC DriverThis is the quick start guide for the Timer Counter (TC) , with step-by-step instructions on how to configure and use the driver for a specific use case
oQuick start guide for Serial Interface serviceThis is the quick start guide for the Serial Interface module, with step-by-step instructions on how to configure and use the serial in a selection of use cases
|\Advanced use case - Send a packet of serial dataIn this use case, the USART module is configured for:
oQuick Start Guide for the graphics serviceThis is the quick start guide for the Graphics (GFX) service", with step-by-step instructions on how to configure and use it for a specific use case
oTodo List
\Deprecated List