Microchip® Advanced Software Framework

 All Data Structures Namespaces Files Functions Variables Typedefs Enumerations Enumerator Friends Macros Groups Pages
Modules
Here is a list of all modules:
[detail level 123456789101112131415161718192021]
oApplications and Examples
oUnit Tests
oPerformance Analyzer ApplicationThis application Performance Analyzer is a Serial interface based application, which communicates with Wireless Analyzer to demonstrate various features and capabilities of Atmel Transceivers
oSensors Platform Board ConfigurationConfiguration constants defined for the platform are used to enable peripherals and map I/O pin interfaces between sensors and the development board they are paired with
oSensor Device StackThe sensor device service provides high-level interfaces and binary driver libraries for sensor devices on systems built around Atmel microcontrollers
oTwo Wire-interface(TWI)This is the common API for TWIs
oIEEE 802.15.4 MAC v3.1.1The IEEE standard 802.15.4 MAC Layer defines the protocol and compatible interconnection for data communication devices using low data rate, low power and low complexity, short-range radio frequency (RF) transmissions in a wireless personal area network (WPAN)
oSIO2NCP - UARTThis module performs serial input/output functionalities via UART from and to the HOST
oStandard I/O (stdio)Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices
oTransceiver Feature AccessThe Atmel transceivers provide a variety of additional hardware features features that are not reflected in the IEEE 802.15.4 standard
oFirst-In-First-Out Buffer (FIFO)See Quick start guide for First-In-First-Out Buffer (FIFO)
oDirect Memory Access controller (DMA)See Quick start guide for the XMEGA DMA driver
oImplementation of SD/MMC/SDIO Stack
oSD/MMC/SDIO common stackSD/MMC/SDIO basic APIs used by SD/MMC/SDIO memory APIs (sd_mmc_stack_mem_group)
oQTouch device driver for I2C interfaceSee Quick start guide for QTouch component
oTimeout service XMEGASee Quick start guide for Timeout service
oAtmel part identification macrosThis collection of macros identify which series and families that the various Atmel parts belong to
oTWI - Two-Wire InterfaceSee Quick start guide for XMEGA TWI driver
oAtmel FLIP Protocol definitionsTo perform firmware upgrade, Atmel has developed an application called "FLIP" This software is a flexible application which lets you program and configure Atmel's microcontroller devices in their final environment without needing any dedicated hardware
oDefinitions for Atmel FLIP Protocol version 2Note: Used by uc3 and Xmega parts
oWatchdog Timer (WDT)See Quick start guide for WDT driver
oAnalog Comparator (AC)See Quick start guide for the XMEGA AC driver
oCPU reset causeSee Quick start guide for reset cause service
oHX8347A Display Controller Low Level driverThis is the low level driver for the HX8347A display controller
oFatFS file system serviceService of FatFS file system
oData Encryption Standard (DES)See Quick start guide for XMEGA DES driver
oNVM serviceSee Quick Start quide for common NVM driver
oGeneric board supportThe generic board support module includes board-specific definitions and function prototypes, such as the board initialization function
oGlobal interrupt managementThis is a driver for global enabling and disabling of interrupts
oQTouch Library for AVR & AVR32 devicesThis is the QTouch Library for AVR and AVR32 devices that consists of one api header file(touch_api.h) and respective pre-compiled libraries
oMonochrome graphical display systemSee Quick Start Guide for the mono graphics service
oSPI - Serial Peripheral InterfaceDriver for the Serial Peripheral Interface (SPI)
oCommon WL DefinitionsAll General Definitions used by the Wireless Stack applications are defined in this module
oNVM driver example functions
oST7565R LCD Controller Low-level driverThis is a low level driver for the ST7565R LCD controller
oProgrammable Multilevel Interrupt ControllerSee Quick start guide for PMIC driver
oGeneral Purpose Input/OutputThis is the common API for GPIO
oAT25DFx SerialFlash component driver.See Quickstart guide for AT25DFx component.
oXMEGA compiler driverCompiler abstraction layer and code utilities for 8-bit AVR
oXMEGA Quadrature Decoder (QDEC)This is a driver for the AVR XMEGA Quadrature Decoder module (QDEC)
oConfiguration Change ProtectionSee Quick start guide for CCP driver
oSSD1306 OLED Controller Low-level driverThis is a low level driver for the SSD1306 OLED controller through 4-wire SPI
oClock Management
oDigital to Analog Converter (DAC)See Quick start guide for XMEGA DAC
oXMEGA Pulse Width Modulation (PWM) serviceSee Quickstart guide for AVR XMEGA PWM service
oCommon IOPORT APISee Quick start guide for the common IOPORT service
oATSHA204 Component Example - status LED'sFunctions
oSIO2HOST - UARTThis module performs serial input/output functionalities via UART
oTest Suite FrameworkThis module is the test suite framework, which provides a set of standard functions and macros for defining and running test suites
omaXTouch low-level componentSee Quick start guide for the maXTouch component
oTransceiver Abstraction LayerThe Transceiver Abstraction Layer (TAL) implements the transceiver specific functionalities and provides interfaces to the upper layers (like IEEE 802.15.4 MAC )and uses the services of PAL
oUSART in SPI (Serial Peripheral Interface) modeThis is the common API for USART in SPI mode
oAT45dbx DataFlash component driver.This is a driver for the AT45dbX series DataFlash memories
oAdvanced Encryption Standard (AES)See Quick start guide for XMEGA AES driver
oVirtual Memory in RAMThe component manages a disk on a volatile memory (internal RAM)
oSerial Peripheral Interface (SPI)This is the common API for SPI interface
oXMEGA SPI master service.This is the API for SPI master service on XMEGA
oBusy-Wait Delay RoutinesThis module provides simple loop-based delay routines for those applications requiring a brief wait during execution
oUSART module (USART)See Quick start guide for USART module
oCalendar serviceSee Quick start guide for Calendar service
oSensors Xplained Extension BoardsThis file contains definitions and services related to the features of the SENSORS_XPLAINED_XXX Xplained boards
oAT30TS Temperature Sensor LibraryThis module contains different routines that can be used for interfacing AT30TS series of Digital Temperature Sensors
o32-bit Real Time Counter (RTC32)See Quick start guide for RTC32 driver
oSerial Standard I/O (stdio) Example
oMemory Control AccessCommon abstraction layer for memory interfaces
oSerial Interface ModuleThis module is responsible for encoding and decoding the serial bytes to/from Host into corresponding MAC APIs
oMemory Bag AllocatorThe Membag allocator is a optimized, fragmentationless general purpose memory allocator utility module designed to replace the standard C library malloc() and free() functions in resource constrained environments
oILI9341 Display Controller Component DriverSee Quick Start Guide for the ILI9341 Display Controller Component Driver
oAnalog to Digital Converter (ADC)See Quick start guide for XMEGA ADC
oATSHA204 Component Example - USARTLogging functions
oData in Huge Data Memory SpaceDue to shortcomings of the GCC compiler for 8-bit AVR, custom functions are needed for access to data beyond the 64 kB boundary, i.e., addresses that are larger than 16-bit
oExternal Bus Interface (EBI)See Quick Start Guide for the XMEGA EBI Driver 
oPort of low level driver for FatFSLow level driver for FatFS
oSHA204 Service - timer functionsCode example to use the timeout timer: sha204_start_timeout_timer_ms(timeout); bool status = false; do { status = try_your_thing(); } while ((sha204_timer expired == false) && (status == false));
oReal Time Counter (RTC)See Quick start guide for RTC driver
oSleep controller driverThis is a low-level driver implementation for the AVR XMEGA sleep controller
oSHA204 Service - hardware independent communication functions
oSHA204 Service - command marshaling functions
oSHA204 Service - hardware dependent communication functions
oTimer Counter (TC)See Quick Start Guide for the XMEGA TC Driver
oSecurity toolboxThe STB (Security Toolbox) is a high level security abstraction layer providing an easy- to-use crypto API for direct application access.It is placed on top of the SAL and abstracts and implements transceiver or MCU dependent functionality that encrypts or decrypts frames usimg CCM according to 802.15.4/Zigbee
oSleep managerThe sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time
oSerial Interface (Serial)See Quick start guide for Serial Interface service
oGraphical display systemThis service provides an interface to drawing graphics on a graphical display
oGroup_tal_slotted_csma_231
oGroup_tal_pib
oGroup_tal_tx_212b
oApp_widget_group
oGroup_tal_slotted_csma_233
oGroup_tal_tx
oGroup_tal_init
oGroup_tal_rx
\Group_tal_irq