This is the quick start guide for the Configuration Change Protection (CCP) driver, with step-by-step instructions on how to use the driver.
The use case contains a code fragment, and this can be copied into, e.g., the main application function.
In this use case, the CCP is used to write to the protected XMEGA Clock Control register.