This is the quick start guide for the System Clock Management service, with step-by-step instructions on how to configure and use the service for specific use cases.
System Clock Management use cases
Basic usage of the System Clock Management service
This section will present a basic use case for the System Clock Management service. This use case will configure the main system clock to 32MHz, using an internal PLL module to multiply the frequency of a crystal attached to the microcontroller. The secondary peripheral bus clock and CPU clock are scaled down from the speed of the main system clock.
Prerequisites
Initialization code
Add to the application initialization code:
Workflow
- Configure the system clocks according to the settings in conf_clock.h:
Example code
Add or uncomment the following in your conf_clock.h header file, commenting out all other definitions of the same symbol(s):
#define CONFIG_SYSCLK_SOURCE SYSCLK_SRC_PLL
#define CONFIG_PLL0_SOURCE PLL_SRC_XOSC
#define CONFIG_PLL0_MUL (32000000UL / BOARD_XOSC_HZ)
#define CONFIG_PLL0_DIV 1
#define CONFIG_SYSCLK_PSADIV SYSCLK_PSADIV_1
#define CONFIG_SYSCLK_PSBCDIV SYSCLK_PSBCDIV_1_2
Workflow
- Configure the main system clock to use the output of the PLL module as its source:
#define CONFIG_SYSCLK_SOURCE SYSCLK_SRC_PLL
- Configure the PLL0 module to use external crystal oscillator XOSC as its source:
#define CONFIG_PLL0_SOURCE PLL_SRC_XOSC
- Configure the PLL0 module to multiply the external oscillator XOSC frequency up to 32MHz:
#define CONFIG_PLL0_MUL (32000000UL / BOARD_XOSC_HZ)
#define CONFIG_PLL0_DIV 1
- Note
- For user boards,
BOARD_XOSC_HZ
should be defined in the board conf_board.h
configuration file as the frequency of the crystal attached to XOSC.
- Configure the main CPU clock and slow peripheral bus to run at 16MHz, run the fast peripheral bus at the full 32MHz speed:
#define CONFIG_SYSCLK_PSADIV SYSCLK_PSADIV_1
#define CONFIG_SYSCLK_PSBCDIV SYSCLK_PSBCDIV_1_2
- Note
- Some dividers are powers of two, while others are integer division factors. Refer to the formulas in the conf_clock.h template commented above each division define.