This is the quick start guide for the Watchdog Timer (WDT), with step-by-step instructions on how to configure and use the driver in a selection of use cases.
The use cases contain several code fragments. The code fragments in the steps for setup can be copied into a custom initialization function, while the steps for usage can be copied into, e.g., the main application function.
In this use case, the WDT is configured for:
The use case enables the WDT, and resets it after 5 ms to prevent system reset after time out period of 8 ms.
For the setup code of this use case to work, the following must be added to the project:
Add to application initialization:
Add to, e.g., main loop in application C-file: