functions
Functions | |
void | display_status (uint8_t device_present_mask, uint8_t sha204_revision) |
This function displays information using LEDs about the SHA204 devices on the Security Xplained board. More... | |
void | led_display_number (uint8_t value) |
This function displays a byte value using the Xplained LEDs. More... | |
void display_status | ( | uint8_t | device_present_mask, |
uint8_t | sha204_revision | ||
) |
This function displays information using LEDs about the SHA204 devices on the Security Xplained board.
[in] | device_present_mask | The high nibble represents the four SHA204 devices. |
[in] | sha204_revision | revision of the SHA204 devices |
void led_display_number | ( | uint8_t | value | ) |
This function displays a byte value using the Xplained LEDs.
[in] | value | byte to display |