Microchip® Advanced Software Framework

common/services/usb/class/msc/device/example/main.c File Reference

Main functions for MSC example.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include "conf_usb.h"
#include "ui.h"

Functions

int main (void)
 Main function. Execution starts here. More...
 
void main_msc_disable (void)
 Called by MSC interface Callback running when USB Host disable MSC interface. More...
 
bool main_msc_enable (void)
 Called by MSC interface Callback running when USB Host enable MSC interface. More...
 
void main_resume_action (void)
 Called by UDD when the USB line exit of suspend state. More...
 
void main_sof_action (void)
 Called when a start of frame is received on USB line. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 

Variables

static volatile bool main_b_msc_enable = false
 

void main_msc_disable ( void  )

Called by MSC interface Callback running when USB Host disable MSC interface.

References main_b_msc_enable, and main_b_msc_enumerated.

bool main_msc_enable ( void  )

Called by MSC interface Callback running when USB Host enable MSC interface.

Return values
trueif MSC startup is ok

References main_b_msc_enable, and main_b_msc_enumerated.

void main_resume_action ( void  )

Called by UDD when the USB line exit of suspend state.

Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.

Called by UDD when the USB line exit of suspend state.

Called by USB stack when the bus resumes from suspend.

References ui_wakeup().

void main_sof_action ( void  )

Called when a start of frame is received on USB line.

Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.

Called when a start of frame is received on USB line.

Called by USB stack when a start of frame is received, i.e., every millisecond during normal operation. This function triggers processing of the user interface if the HID interface has been enabled.

References main_b_msc_enable, udd_get_frame_number(), and ui_process().

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

Called by USB stack when host suspends the bus.

References ui_powerdown().

volatile bool main_b_msc_enable = false
static