Microchip® Advanced Software Framework

zid.h File Reference

API for ZID profile.

Author
Microchip Technology Inc: http://www.microchip.com
Support: https://www.microchip.com/support/
#include "rf4ce.h"
#include "nwk_internal.h"
#include "zid_build_config.h"
#include "gdp.h"
#include "nwk_config.h"

Data Structures

struct  contact_data_report_tag
 
struct  hid_adaptor_attr_tag
 
struct  hid_attr_tag
 
struct  keyboard_input_desc_tag
 
struct  keyboard_output_desc_tag
 
struct  mouse_desc_tag
 
struct  null_report_tag
 
struct  pair_table_tag
 
struct  pinch_gesture_report_tag
 
struct  rotation_gesture_report_tag
 
struct  scroll_gesture_report_tag
 
struct  sync_report_tag
 
struct  tap_gesture_report_tag
 
struct  tap_support_properties_tag
 
struct  touch_sensor_properties_tag
 
struct  zid_ib_tag
 ZID information base. More...
 
struct  zid_indication_callback_tag
 struct for zrc indication callback. More...
 
struct  zid_report_data_record_tag
 ZID profile constants. More...
 

Macros

#define aplcIdleRateGuardTime   1500 /* 1500 ms */
 ZID profile constants. More...
 
#define aplcIdleRateGuardTime_us   (aplcIdleRateGuardTime * 1000UL)
 
#define aplcKeyExchangeTransferCount_def   0x24 /* as per ZID spec */
 
#define aplcMaxConfigPrepTime   200 /* 200ms */
 The maximum time a HID class device shall take to construct a push attributes command frame and send it to the HID adaptor during its configuration state. More...
 
#define aplcMaxConfigPrepTime_us   (aplcMaxConfigPrepTime * 1000UL)
 
#define aplcMaxConfigWaitTime   300 /* ms */
 The maximum time the HID adaptor shall wait to receive a push attributes command frame from a HID class device during its configuration state. More...
 
#define aplcMaxConfigWaitTime_us   (aplcMaxConfigWaitTime * 1000UL)
 
#define aplcMaxHIDRxOnWaitTime   100 /* ms */
 The maximum time a HID class device originator shall wait for a response to a heartbeat command frame or a request to stay awake via the data pending subfield of the frame control field of an incoming frame. More...
 
#define aplcMaxHIDRxOnWaitTime_us   (aplcMaxHIDRxOnWaitTime * 1000UL)
 
#define aplcMaxNonStdDescCompSize   256 /* bytes */
 The maximum size of a single non standard descriptor component. More...
 
#define aplcMaxNonStdDescCompsPerHID   4
 The maximum number of non standard descriptors that can be supported on a HID class device. More...
 
#define aplcMaxNonStdDescFragmentSize   80 /* bytes */
 The maximum size of a non standard descriptor fragment that will fit in an over-the-air frame. More...
 
#define aplcMaxNullReportSize   16 /* bytes */
 The maximum size of a NULL report. More...
 
#define aplcMaxPairIndicationWaitTime   1 /* second */
 The maximum amount of time a device waits after receiving a successful NLME-AUTO-DISCOVERY.confirm primitive for a pair indication to arrive from the pairing initiator. More...
 
#define aplcMaxPairIndicationWaitTime_us
 
#define aplcMaxReportRepeatInterval   100 /* ms */
 The maximum time between consecutive report data transmissions. More...
 
#define aplcMaxReportRepeatInterval_us   (aplcMaxReportRepeatInterval * 1000UL)
 
#define aplcMaxResponseWaitTime   200 /* ms */
 The maximum time a device shall wait for a response command frame following a request command frame. More...
 
#define aplcMaxResponseWaitTime_us   (aplcMaxResponseWaitTime * 1000UL)
 
#define aplcMaxStdDescCompsPerHID   12
 The maximum number of standard descriptors that can be supported on a HID class device. More...
 
#define aplcMinIntPipeUnsafeTxWindowTime   50 /* ms */
 Minimum window time permitted when using the interrupt pipe before a safe transmission is required. More...
 
#define aplcMinIntPipeUnsafeTxWindowTime_us
 
#define aplcMinKeyExchangeTransferCount   3
 The minimum value of the KeyExTransferCount parameter passed to the pair request primitive during the push button pairing procedure. More...
 
#define aplZIDProfileVersion_def   0x0001
 
#define AUTO_DISC_DURATION_SYM   0x1C9C38
 The automatic discovery response mode duration shall be set to 0x1c9c38 (30s). More...
 
#define DISCOVERY_DURATION   0x00186A
 ZID profile initial NIB attributes. More...
 
#define DISCOVERY_REPETITION_INTERVAL   0x00F424
 Default value for the discovery repetition interval. More...
 
#define HID_COUNTRY_CODE   0x00
 
#define HID_DEVICE_RELEASE_NUMBER   0x0000
 
#define HID_DEVICE_SUB_CLASS   ZID_NO_SUBCLASS
 
#define HID_NUM_DESCRIPTORS   0
 
#define HID_NUM_NULL_REPORTS   0
 
#define HID_NUM_STD_DESCRIPTORS   2
 
#define HID_NUMBER_ENDPOINTS   0x02
 
#define HID_PARSER_VERSION   0x0111
 ZID profile constants. More...
 
#define HID_POLL_INTERVAL   1
 
#define HID_PRODUCT_ID   0x0000
 
#define HID_PROTOCOL_CODE   PROTOCOL_CODE_NONE
 
#define HID_STD_DESCRIPTOR_LIST_0   MOUSE
 
#define HID_STD_DESCRIPTOR_LIST_1   KEYBOARD
 
#define HID_STD_DESCRIPTOR_LIST_2   0
 
#define HID_STD_DESCRIPTOR_LIST_3   0
 
#define HID_VENDOR_ID   0x1014
 
#define MAX_DISCOVERY_REPETITIONS   0x1E
 Default value for maximum number of times the discovery request command is sent. More...
 
#define MAX_REPORTED_NODE_DESCRIPTORS   1
 Default value for Number of reported node descriptor received during discovery process. More...
 
#define TXO_CTRL_PIPE   0x80
 Constant defines used for TxOption field for report data transmission mode. More...
 
#define TXO_INTER_PIPE   0x00
 

Typedefs

typedef struct
contact_data_report_tag 
contact_data_report_t
 
typedef struct hid_adaptor_attr_tag hid_adaptor_attr_t
 
typedef struct hid_attr_tag hid_attr_t
 
typedef struct
keyboard_input_desc_tag 
keyboard_input_desc_t
 
typedef struct
keyboard_output_desc_tag 
keyboard_output_desc_t
 
typedef struct mouse_desc_tag mouse_desc_t
 
typedef struct null_report_tag null_report_t
 
typedef struct pair_table_tag pair_table_t
 
typedef struct
pinch_gesture_report_tag 
pinch_gesture_report_t
 
typedef struct
rotation_gesture_report_tag 
rotation_gesture_report_t
 
typedef struct
scroll_gesture_report_tag 
scroll_gesture_report_t
 
typedef struct sync_report_tag sync_report_t
 
typedef struct
tap_gesture_report_tag 
tap_gesture_report_t
 
typedef struct
tap_support_properties_tag 
tap_support_properties_t
 
typedef struct
touch_sensor_properties_tag 
touch_sensor_properties_t
 
typedef void(* vendor_data_ind_cb_t )(uint8_t PairingRef, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags)
 
typedef enum
zid_attribute_status_tag 
zid_attribute_status_t
 Attribute status. More...
 
typedef enum zid_attribute_tag zid_attribute_t
 ZID attribute Ids. More...
 
typedef enum zid_cmd_code_tag zid_cmd_code_t
 ZID command codes. More...
 
typedef void(* zid_connect_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef)
 
typedef void(* zid_data_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef)
 
typedef enum
zid_device_subclass_tag 
zid_device_subclass_t
 ZID device subclass. More...
 
typedef void(* zid_get_attribute_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex, uint8_t AttributeSize, uint8_t *ZIDAttributeValue)
 
typedef void(* zid_get_report_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef)
 
typedef void(* zid_get_report_indication_cb_t )(uint8_t PairingRef, zid_report_types_t zid_report_type, zid_report_desc_t zid_report_desc, uint8_t RxLinkQuality, uint8_t RxFlags)
 
typedef void(* zid_heartbeat_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef)
 
typedef void(* zid_heartbeat_indication_cb_t )(uint8_t PairingRef)
 
typedef struct zid_ib_tag zid_ib_t
 ZID information base. More...
 
typedef struct
zid_indication_callback_tag 
zid_indication_callback_t
 struct for zrc indication callback. More...
 
typedef enum zid_protocol_code_tag zid_protocol_code_t
 ZID protocol code. More...
 
typedef enum zid_protocol_tag zid_protocol_t
 ZID protocol. More...
 
typedef void(* zid_report_data_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef)
 
typedef void(* zid_report_data_indication_cb_t )(uint8_t PairingRef, uint8_t num_report_records, zid_report_data_record_t *zid_report_data_record_ptr, uint8_t RxLinkQuality, uint8_t RxFlags)
 
typedef struct
zid_report_data_record_tag 
zid_report_data_record_t
 ZID profile constants. More...
 
typedef enum zid_report_desc_tag zid_report_desc_t
 
typedef enum zid_report_types_tag zid_report_types_t
 ZID report type field values. More...
 
typedef void(* zid_set_attribute_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex)
 
typedef void(* zid_set_report_confirm_cb_t )(nwk_enum_t Status, uint8_t PairingRef)
 
typedef void(* zid_standby_confirm_cb_t )(nwk_enum_t Status, bool StdbyEnabled)
 
typedef void(* zid_standby_leave_indication_cb_t )(void)
 
typedef enum zid_standby_tag zid_standby_t
 

Enumerations

enum  zid_attribute_status_tag {
  ATTRIBUTE_SUCCESS = 0x00,
  ATTRIBUTE_UNSUPPORTED,
  ATTRIBUTE_ILLEGAL
}
 Attribute status. More...
 
enum  zid_attribute_tag {
  aplKeyExchangeTransferCount = 0x82,
  aplZIDProfileVersion = 0xA0,
  aplIntPipeUnsafeTxWindowTime = 0xA1,
  aplReportRepeatInterval = 0xA2,
  privatePendingData = 0xA5,
  aplHIDParserVersion = 0xe0,
  aplHIDDeviceSubclass,
  aplHIDProtocolCode,
  aplHIDCountryCode,
  aplHIDDeviceReleaseNumber,
  aplHIDVendorId,
  aplHIDProductId,
  aplHIDNumEndpoints,
  aplHIDPollInterval,
  aplHIDNumStdDescComps,
  aplHIDStdDescCompsList,
  aplHIDNumNullReports,
  aplHIDNumNonStdDescComps = 0xf0,
  aplHIDNonStdDescCompSpec
}
 ZID attribute Ids. More...
 
enum  zid_cmd_code_tag {
  GET_REPORT = 0x01,
  REPORT_DATA,
  SET_REPORT
}
 ZID command codes. More...
 
enum  zid_device_subclass_tag {
  ZID_NO_SUBCLASS = 0x00,
  ZID_BOOT_INTERFACE_SUBCLASS
}
 ZID device subclass. More...
 
enum  zid_protocol_code_tag {
  PROTOCOL_CODE_NONE = 0x00,
  PROTOCOL_CODE_KEYBOARD,
  PROTOCOL_CODE_MOUSE
}
 ZID protocol code. More...
 
enum  zid_protocol_tag {
  PROTOCOL_BOOT = 0x00,
  PROTOCOL_REPORT
}
 ZID protocol. More...
 
enum  zid_report_desc_tag {
  MOUSE = 0x01,
  KEYBOARD,
  CONTACT_DATA,
  TAP_GESTURE,
  SCROLL_GESTURE,
  PINCH_GESTURE,
  ROTATE_GESTURE,
  SYNC,
  TOUCH_SENSOR_PROPERTIES,
  TAP_SUPPORT_PROPERTIES
}
 
enum  zid_report_types_tag {
  INPUT = 0x01,
  OUTPUT,
  FEATURE
}
 ZID report type field values. More...
 
enum  zid_standby_tag {
  STDBY_ACTIVE,
  STDBY_DISABLED,
  STDBY_ACTIVE_REQ,
  STDBY_DISABLE_REQ,
  STDBY_DISABLE_INTERN_REQ
}
 

Functions

bool check_zid_adaptor_compatibility (uint8_t PairingRef, uint8_t payload_length, uint8_t *payload)
 This function checks the Adaptor compatibility while pairing decides whether push button pairing request should be allowed. More...
 
bool get_attribute_properties (uint8_t PairingRef, zid_attribute_t attribute_id, uint8_t index, uint8_t *length, uint8_t *value)
 
void register_zid_indication_callback (zid_indication_callback_t *zid_ind_callback)
 Registering zrc indication callback. More...
 
bool send_generic_response (uint8_t PairingRef, gdp_response_code_t code)
 
bool zid_get_attribute_request (bool OTA, uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex, FUNC_PTR zid_get_attribute_confirm)
 
bool zid_get_report_data_request (uint8_t PairingRef, zid_report_types_t zid_report_type, zid_report_desc_t zid_report_desc, uint8_t TxOptions, FUNC_PTR zid_get_report_confirm)
 
bool zid_heartbeat_request (uint8_t PairingRef, FUNC_PTR zid_heartbeat_confirm)
 
bool zid_org_connect_request (uint8_t OrgAppCapabilities, dev_type_t OrgDevTypeList[DEVICE_TYPE_LIST_SIZE], profile_id_t OrgProfileIdList[PROFILE_ID_LIST_SIZE], dev_type_t SearchDevType, uint8_t DiscProfileIdListSize, profile_id_t DiscProfileIdList[PROFILE_ID_LIST_SIZE], FUNC_PTR zid_connect_confirm)
 
bool zid_rec_connect_request (uint8_t RecAppCapabilities, dev_type_t RecDevTypeList[3], profile_id_t RecProfileIdList[7], FUNC_PTR zid_connect_confirm)
 
bool zid_report_data_request (uint8_t PairingRef, uint8_t numReportRecords, zid_report_data_record_t *reportRecord, uint8_t TxOptions, FUNC_PTR zid_report_data_confirm)
 
void zid_reset (bool SetDefault)
 
void zid_reset_attributes (void)
 
bool zid_set_attribute_request (uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex, uint8_t *ZIDAttributeValue, FUNC_PTR zid_set_attribute_confirm)
 
bool zid_set_null_report (uint8_t report_index, null_report_t *null_report_ptr)
 
bool zid_set_report_request (uint8_t PairingRef, uint8_t payloadlength, uint8_t *payload, uint8_t TxOptions, FUNC_PTR confirm_cb)
 
bool zid_standby_request (bool standby_request, FUNC_PTR zid_standby_confirm)
 

#define aplcIdleRateGuardTime   1500 /* 1500 ms */

ZID profile constants.

The length of time the HID adaptor will repeat a report from a remote HID class device when its idle rate is non-zero, before a direct report command frame must be received from the remote HID class device.

#define aplcIdleRateGuardTime_us   (aplcIdleRateGuardTime * 1000UL)
#define aplcKeyExchangeTransferCount_def   0x24 /* as per ZID spec */
#define aplcMaxConfigPrepTime   200 /* 200ms */

The maximum time a HID class device shall take to construct a push attributes command frame and send it to the HID adaptor during its configuration state.

#define aplcMaxConfigPrepTime_us   (aplcMaxConfigPrepTime * 1000UL)
#define aplcMaxConfigWaitTime   300 /* ms */

The maximum time the HID adaptor shall wait to receive a push attributes command frame from a HID class device during its configuration state.

#define aplcMaxConfigWaitTime_us   (aplcMaxConfigWaitTime * 1000UL)
#define aplcMaxHIDRxOnWaitTime   100 /* ms */

The maximum time a HID class device originator shall wait for a response to a heartbeat command frame or a request to stay awake via the data pending subfield of the frame control field of an incoming frame.

#define aplcMaxHIDRxOnWaitTime_us   (aplcMaxHIDRxOnWaitTime * 1000UL)
#define aplcMaxNonStdDescCompSize   256 /* bytes */

The maximum size of a single non standard descriptor component.

The HID adaptor shall be able to store descriptor components of this size for each component stored on a device.

#define aplcMaxNonStdDescCompsPerHID   4

The maximum number of non standard descriptors that can be supported on a HID class device.

The HID adaptor shall be able to store this many non standard descriptors for each paired HID class device.

#define aplcMaxNonStdDescFragmentSize   80 /* bytes */

The maximum size of a non standard descriptor fragment that will fit in an over-the-air frame.

#define aplcMaxNullReportSize   16 /* bytes */

The maximum size of a NULL report.

The HID adaptor shall be able to store NULL reports of this size for each component stored on a device.

#define aplcMaxPairIndicationWaitTime   1 /* second */

The maximum amount of time a device waits after receiving a successful NLME-AUTO-DISCOVERY.confirm primitive for a pair indication to arrive from the pairing initiator.

#define aplcMaxPairIndicationWaitTime_us
Value:
1200000UL /*(aplcMaxPairIndicationWaitTime
** 1000000UL)*/
#define aplcMaxReportRepeatInterval   100 /* ms */

The maximum time between consecutive report data transmissions.

#define aplcMaxReportRepeatInterval_us   (aplcMaxReportRepeatInterval * 1000UL)
#define aplcMaxResponseWaitTime   200 /* ms */

The maximum time a device shall wait for a response command frame following a request command frame.

#define aplcMaxResponseWaitTime_us   (aplcMaxResponseWaitTime * 1000UL)
#define aplcMaxStdDescCompsPerHID   12

The maximum number of standard descriptors that can be supported on a HID class device.

The HID adaptor shall be able to store this many standard descriptors for each paired HID class device.

#define aplcMinIntPipeUnsafeTxWindowTime   50 /* ms */

Minimum window time permitted when using the interrupt pipe before a safe transmission is required.

#define aplcMinIntPipeUnsafeTxWindowTime_us
Value:
1000UL)
#define aplcMinIntPipeUnsafeTxWindowTime
Minimum window time permitted when using the interrupt pipe before a safe transmission is required...
Definition: zid.h:131
#define aplcMinKeyExchangeTransferCount   3

The minimum value of the KeyExTransferCount parameter passed to the pair request primitive during the push button pairing procedure.

#define aplZIDProfileVersion_def   0x0001
#define AUTO_DISC_DURATION_SYM   0x1C9C38

The automatic discovery response mode duration shall be set to 0x1c9c38 (30s).

#define DISCOVERY_DURATION   0x00186A

ZID profile initial NIB attributes.

Controller discovery duration

#define DISCOVERY_REPETITION_INTERVAL   0x00F424

Default value for the discovery repetition interval.

#define HID_COUNTRY_CODE   0x00
#define HID_DEVICE_RELEASE_NUMBER   0x0000
#define HID_DEVICE_SUB_CLASS   ZID_NO_SUBCLASS
#define HID_NUM_DESCRIPTORS   0
#define HID_NUM_NULL_REPORTS   0
#define HID_NUM_STD_DESCRIPTORS   2
#define HID_NUMBER_ENDPOINTS   0x02
#define HID_PARSER_VERSION   0x0111

ZID profile constants.

#define HID_POLL_INTERVAL   1
#define HID_PRODUCT_ID   0x0000
#define HID_PROTOCOL_CODE   PROTOCOL_CODE_NONE
#define HID_STD_DESCRIPTOR_LIST_0   MOUSE
#define HID_STD_DESCRIPTOR_LIST_1   KEYBOARD
#define HID_STD_DESCRIPTOR_LIST_2   0
#define HID_STD_DESCRIPTOR_LIST_3   0
#define HID_VENDOR_ID   0x1014
#define MAX_DISCOVERY_REPETITIONS   0x1E

Default value for maximum number of times the discovery request command is sent.

#define MAX_REPORTED_NODE_DESCRIPTORS   1

Default value for Number of reported node descriptor received during discovery process.

#define TXO_CTRL_PIPE   0x80

Constant defines used for TxOption field for report data transmission mode.

#define TXO_INTER_PIPE   0x00

typedef struct hid_attr_tag hid_attr_t
typedef struct mouse_desc_tag mouse_desc_t
typedef struct pair_table_tag pair_table_t
typedef void(* vendor_data_ind_cb_t)(uint8_t PairingRef, uint16_t VendorId, uint8_t nsduLength, uint8_t *nsdu, uint8_t RxLinkQuality, uint8_t RxFlags)

Attribute status.

ZID attribute Ids.

ZID command codes.

typedef void(* zid_connect_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef)
typedef void(* zid_data_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef)

ZID device subclass.

typedef void(* zid_get_attribute_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex, uint8_t AttributeSize, uint8_t *ZIDAttributeValue)
typedef void(* zid_get_report_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef)
typedef void(* zid_get_report_indication_cb_t)(uint8_t PairingRef, zid_report_types_t zid_report_type, zid_report_desc_t zid_report_desc, uint8_t RxLinkQuality, uint8_t RxFlags)
typedef void(* zid_heartbeat_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef)
typedef void(* zid_heartbeat_indication_cb_t)(uint8_t PairingRef)
typedef struct zid_ib_tag zid_ib_t

ZID information base.

struct for zrc indication callback.

App should use this struct to register indication callback functions

ZID protocol code.

ZID protocol.

typedef void(* zid_report_data_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef)
typedef void(* zid_report_data_indication_cb_t)(uint8_t PairingRef, uint8_t num_report_records, zid_report_data_record_t *zid_report_data_record_ptr, uint8_t RxLinkQuality, uint8_t RxFlags)

ZID profile constants.

ZID report type field values.

typedef void(* zid_set_attribute_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef, zid_attribute_t ZIDAttribute, uint8_t ZIDAttributeIndex)
typedef void(* zid_set_report_confirm_cb_t)(nwk_enum_t Status, uint8_t PairingRef)
typedef void(* zid_standby_confirm_cb_t)(nwk_enum_t Status, bool StdbyEnabled)
typedef void(* zid_standby_leave_indication_cb_t)(void)

Attribute status.

Enumerator
ATTRIBUTE_SUCCESS 
ATTRIBUTE_UNSUPPORTED 
ATTRIBUTE_ILLEGAL 

ZID attribute Ids.

Enumerator
aplKeyExchangeTransferCount 

The minimum value of the KeyExTransferCount parameter passed to the pair request primitive during the push button pairing procedure.

aplZIDProfileVersion 

The aplZIDProfileVersion attribute specifies the version of the ZID profile specification to which the device was designed.

aplIntPipeUnsafeTxWindowTime 

The aplIntPipeSUnsafeTxWindowTime attribute specifies the maximum time, during which transmissions use the unacknowledged, single channel service, permitted before an acknowledged, multiple channel transmission is required.

aplReportRepeatInterval 
privatePendingData 

Private attribute used to set the pending data bit.

aplHIDParserVersion 

The aplHIDParserVersion attribute specifies the version of the core HID specification.

aplHIDDeviceSubclass 

The aplHIDDeviceSubclass attribute specifies the HID subclass code of the HID class device.

aplHIDProtocolCode 

The aplHIDProtocolCode attribute specifies the HID protocol code of the HID class device supporting the boot protocol.

aplHIDCountryCode 

The aplHIDCountryCode attribute specifies the country for which the hardware is localized.

aplHIDDeviceReleaseNumber 

The aplHIDDeviceReleaseNumber attribute specifies the release number of the device itself.

aplHIDVendorId 

The aplHIDVendorId attribute specifies the USB-IF assigned identifier corresponding to the vendor of the device.

aplHIDProductId 

The aplHIDProductId attribute specifies a manufacturer assigned product identifier for the device.

aplHIDNumEndpoints 
aplHIDPollInterval 

The aplHIDPollInterval attribute specifies the polling interval for all endpoint data transfers.

aplHIDNumStdDescComps 

The aplHIDNumStdDescComps attribute specifies the number of RF4CE ZID profile defined standard descriptors supported by the device.

aplHIDStdDescCompsList 

The aplHIDStdDescriptorList attribute is of length equal to the value of the aplHIDNumStdDescComps attribute and shall specify the list of standard RF4CE ZID profile defined descriptors supported by the device.

aplHIDNumNullReports 
aplHIDNumNonStdDescComps 

The aplHIDNumDescriptors attribute specifies the number of non standard HID descriptors stored on the device.

aplHIDNonStdDescCompSpec 

The aplHIDDescriptorSpec-i attributes specifies the actual HID descriptors supported on the device.

ZID command codes.

Enumerator
GET_REPORT 
REPORT_DATA 
SET_REPORT 

ZID device subclass.

Enumerator
ZID_NO_SUBCLASS 
ZID_BOOT_INTERFACE_SUBCLASS 

ZID protocol code.

Enumerator
PROTOCOL_CODE_NONE 
PROTOCOL_CODE_KEYBOARD 
PROTOCOL_CODE_MOUSE 

ZID protocol.

Enumerator
PROTOCOL_BOOT 
PROTOCOL_REPORT 
Enumerator
MOUSE 
KEYBOARD 
CONTACT_DATA 
TAP_GESTURE 
SCROLL_GESTURE 
PINCH_GESTURE 
ROTATE_GESTURE 
SYNC 
TOUCH_SENSOR_PROPERTIES 
TAP_SUPPORT_PROPERTIES 

ZID report type field values.

Enumerator
INPUT 
OUTPUT 
FEATURE 
Enumerator
STDBY_ACTIVE 
STDBY_DISABLED 
STDBY_ACTIVE_REQ 
STDBY_DISABLE_REQ 
STDBY_DISABLE_INTERN_REQ 

bool check_zid_adaptor_compatibility ( uint8_t  PairingRef,
uint8_t  payload_length,
uint8_t *  payload 
)

This function checks the Adaptor compatibility while pairing decides whether push button pairing request should be allowed.

Decision could be based on one of the parameter.

Parameters
PairingRefPairing reference.
payload_lengthLength of the Payload
*payloadPointer to the Payload Adaptor attributes can be extracted from the payload.
Returns
true if pairing is granted; else false

References payload.

bool get_attribute_properties ( uint8_t  PairingRef,
zid_attribute_t  attribute_id,
uint8_t  index,
uint8_t *  length,
uint8_t *  value 
)
void register_zid_indication_callback ( zid_indication_callback_t zid_ind_callback)

Registering zrc indication callback.

The application needs to register the zrc indication call back functions so that the corresponding indication function will get called by the profile on receiving the indication from the network layer.

Parameters
zrc_indication_callback_tindication callback struct
See Also
zrc_indication_callback_t

Referenced by main(), and zid_indication_callback_init().

bool send_generic_response ( uint8_t  PairingRef,
gdp_response_code_t  code 
)
bool zid_get_attribute_request ( bool  OTA,
uint8_t  PairingRef,
zid_attribute_t  ZIDAttribute,
uint8_t  ZIDAttributeIndex,
FUNC_PTR  zid_get_attribute_confirm 
)

Referenced by handle_incoming_msg().

bool zid_get_report_data_request ( uint8_t  PairingRef,
zid_report_types_t  zid_report_type,
zid_report_desc_t  zid_report_desc,
uint8_t  TxOptions,
FUNC_PTR  zid_get_report_confirm 
)

Referenced by handle_incoming_msg().

bool zid_heartbeat_request ( uint8_t  PairingRef,
FUNC_PTR  zid_heartbeat_confirm 
)

Referenced by handle_incoming_msg().

bool zid_org_connect_request ( uint8_t  OrgAppCapabilities,
dev_type_t  OrgDevTypeList[DEVICE_TYPE_LIST_SIZE],
profile_id_t  OrgProfileIdList[PROFILE_ID_LIST_SIZE],
dev_type_t  SearchDevType,
uint8_t  DiscProfileIdListSize,
profile_id_t  DiscProfileIdList[PROFILE_ID_LIST_SIZE],
FUNC_PTR  zid_connect_confirm 
)
bool zid_rec_connect_request ( uint8_t  RecAppCapabilities,
dev_type_t  RecDevTypeList[3],
profile_id_t  RecProfileIdList[7],
FUNC_PTR  zid_connect_confirm 
)
bool zid_report_data_request ( uint8_t  PairingRef,
uint8_t  numReportRecords,
zid_report_data_record_t reportRecord,
uint8_t  TxOptions,
FUNC_PTR  zid_report_data_confirm 
)
void zid_reset ( bool  SetDefault)
void zid_reset_attributes ( void  )
bool zid_set_attribute_request ( uint8_t  PairingRef,
zid_attribute_t  ZIDAttribute,
uint8_t  ZIDAttributeIndex,
uint8_t *  ZIDAttributeValue,
FUNC_PTR  zid_set_attribute_confirm 
)
bool zid_set_null_report ( uint8_t  report_index,
null_report_t null_report_ptr 
)

Referenced by handle_incoming_msg().

bool zid_set_report_request ( uint8_t  PairingRef,
uint8_t  payloadlength,
uint8_t *  payload,
uint8_t  TxOptions,
FUNC_PTR  confirm_cb 
)

Referenced by handle_incoming_msg().

bool zid_standby_request ( bool  standby_request,
FUNC_PTR  zid_standby_confirm 
)

Referenced by handle_incoming_msg().