#include "conf_explorer.h"
#include "fs_com.h"
#include "fat.h"
#include <string.h>
#include "ctrl_access.h"
Macros | |
#define | _fat_c_ |
Functions | |
void | fat_cache_clear (void) |
This function clears the sector cache. More... | |
bool | fat_cache_flush (void) |
This function flushes the sector cache on the memory if necessary. More... | |
void | fat_cache_mark_sector_as_dirty (void) |
This function sets a flag to signal that sector cache is modified. More... | |
bool | fat_cache_read_sector (bool b_load) |
This function loads a memory sector in internal cache sector. More... | |
void | fat_cache_reset (void) |
This function resets the sector cache. More... | |
bool | fat_check_device (void) |
This function checks device state. More... | |
bool | fat_check_eof_name (uint16_t character) |
Check end of name. More... | |
bool | fat_check_is_file (void) |
This function checks if the selected file entry is a file and not a directory. More... | |
bool | fat_check_mount (void) |
This function checks if the partition is mounted. More... | |
bool | fat_check_mount_noopen (void) |
This function checks if the partition is mounted and no file is opened. More... | |
bool | fat_check_mount_select (void) |
This function checks if the partition is mounted and if a file is selected. More... | |
bool | fat_check_mount_select_noopen (void) |
This function checks if the partition is mounted and if no file is opened and a file is selected. More... | |
bool | fat_check_mount_select_open (void) |
This function checks if the partition is mounted and if a file is opened. More... | |
bool | fat_check_nav_access_disk (void) |
This function checks write access. More... | |
bool | fat_check_nav_access_file (bool mode) |
This function checks all access at current file. More... | |
bool | fat_check_noopen (void) |
This function checks if a file is not opened on current navigator. More... | |
bool | fat_check_open (void) |
This function checks if a file is opened on current navigator. More... | |
bool | fat_check_select (void) |
This function checks if a file is selected on current navigator. More... | |
void | fat_clear_entry_info_and_ptr (void) |
This function resets the selection pointers. More... | |
bool | fat_cluster_list (uint8_t opt_action, bool b_for_file) |
This function gets or clears a cluster list. More... | |
void | fat_copy_nav (uint8_t u8_idnav) |
This function copies the main navigator to another navigator. More... | |
bool | fat_entry_check (bool b_type) |
This function checks the entry. More... | |
bool | fat_entry_checkext (FS_STRING sz_filter) |
This function checks the file extension. More... | |
bool | fat_entry_is_dir (void) |
This function checks if the entry file is a directory. More... | |
bool | fat_entry_longname (FS_STRING sz_name, uint8_t u8_size_max, bool b_mode, bool b_match_case) |
This function returns or compares the long name entry. More... | |
bool | fat_entry_shortname (FS_STRING sz_name, uint8_t u8_size_max, bool b_mode) |
This function returns or compares the short name entry. More... | |
void | fat_get_entry_info (void) |
This function reads information about selected file. More... | |
PTR_CACHE | fat_get_ptr_entry (void) |
This function returns a cache pointer on the current entry. More... | |
void | fat_invert_nav (uint8_t u8_idnav) |
This function inverts the current navigation with another. More... | |
bool | fat_read_dir (void) |
This function fill the internal cache with a sector from current directory. More... | |
bool | fat_read_file (uint8_t mode) |
This function gets or clears a cluster list at the current position in the selected file. More... | |
void | fat_write_entry_file (void) |
This function writes the information about selected file. More... | |
bool | fat_write_file (uint8_t mode, uint32_t u32_nb_sector_write) |
This function gets and eventually allocs a cluster list at the current position in the selected file. More... | |
Internal functions to manage cluster list caches | |
void | fat_cache_clusterlist_update_start (bool b_for_file) |
This function initializes a cache in cluster list caches. More... | |
void | fat_cache_clusterlist_update_finish (void) |
This function updates a cache of cluster list caches. More... | |
bool | fat_cache_clusterlist_update_read (bool b_for_file) |
This function searches a cluster list in cluster list caches. More... | |
void | fat_cache_clusterlist_update_select (void) |
This function signals that a cache is used. More... | |
void | fat_cache_clusterlist_reset (void) |
This function resets the cluster list caches. More... | |
Variables | |
Store navigator data no selected | |
_MEM_TYPE_SLOW_ Fs_management | fs_g_navext [FS_NB_NAVIGATOR-1] |
_MEM_TYPE_SLOW_ Fs_management_fast | fs_g_navext_fast [FS_NB_NAVIGATOR-1] |
_MEM_TYPE_SLOW_ Fs_management_entry | fs_g_navext_entry [FS_NB_NAVIGATOR-1] |
Variables to manage cluster list caches | |
_MEM_TYPE_SLOW_ Fs_clusterlist_cache | fs_g_cache_clusterlist [FS_NB_CACHE_CLUSLIST *2] |
_MEM_TYPE_SLOW_ uint8_t | fs_g_u8_current_cache |
Position of the current cluster in the FAT <br> | |
Global variable used to take time with routines fat_cluster_readnext() and fat_cluster_val() | |
_MEM_TYPE_FAST_ uint16_t | fs_g_u16_pos_fat |
bool | fat_cluster_val (bool b_mode) |
This function returns or modifies a cluster value in FAT. More... | |
bool | fat_cluster_readnext (void) |
This function is optimized to read a continue cluster list on FAT16 and FAT32. More... | |
uint8_t | fat_checkcluster (void) |
This function checks the cluster value. More... | |
#define _fat_c_ |
This function updates a cache of cluster list caches.
References fat_cache_clusterlist_update_select(), fs_g_cache_clusterlist, fs_g_nav, fs_g_seg, fs_g_u8_current_cache, Fs_segment::u32_addr, Fs_clusterlist_cache::u32_addr, Fs_clusterlist_cache::u32_size, Fs_segment::u32_size_or_pos, Fs_clusterlist_cache::u32_start, Fs_management::u8_BPB_SecPerClus, Fs_management::u8_lun, and Fs_clusterlist_cache::u8_lun.
Referenced by fat_cluster_list().
This function searches a cluster list in cluster list caches.
b_for_file | If true then it is a file cluster list else a directory cluster list |
References fat_cache_clusterlist_update_select(), fat_cache_clusterlist_update_start(), fs_g_cache_clusterlist, fs_g_cluster, fs_g_nav, fs_g_seg, fs_g_u8_current_cache, FS_NB_CACHE_CLUSLIST, Fs_segment::u32_addr, Fs_clusterlist_cache::u32_addr, Fs_management::u32_offset_data, st_fs_cluster::u32_pos, Fs_management::u32_ptr_fat, Fs_clusterlist_cache::u32_size, Fs_segment::u32_size_or_pos, Fs_clusterlist_cache::u32_start, Fs_management::u8_BPB_SecPerClus, Fs_management::u8_lun, and Fs_clusterlist_cache::u8_lun.
Referenced by fat_cluster_list().
This function signals that a cache is used.
References Fs_clusterlist_cache::b_cache_file, fs_g_cache_clusterlist, fs_g_u8_current_cache, FS_NB_CACHE_CLUSLIST, and Fs_clusterlist_cache::u8_level_use.
Referenced by fat_cache_clusterlist_update_finish(), and fat_cache_clusterlist_update_read().
This function initializes a cache in cluster list caches.
b_for_file | If true then it is a file cluster list else a directory cluster list |
References Fs_clusterlist_cache::b_cache_file, fs_g_cache_clusterlist, fs_g_cluster, fs_g_seg, fs_g_u8_current_cache, FS_NB_CACHE_CLUSLIST, Fs_clusterlist_cache::u32_cluster, st_fs_cluster::u32_pos, Fs_segment::u32_size_or_pos, Fs_clusterlist_cache::u32_start, Fs_clusterlist_cache::u8_level_use, and Fs_clusterlist_cache::u8_lun.
Referenced by fat_cache_clusterlist_update_read().
_MEM_TYPE_SLOW_ Fs_clusterlist_cache fs_g_cache_clusterlist[FS_NB_CACHE_CLUSLIST *2] |
_MEM_TYPE_SLOW_ Fs_management fs_g_navext[FS_NB_NAVIGATOR-1] |
Referenced by fat_check_device(), fat_check_nav_access_file(), fat_copy_nav(), and fat_invert_nav().
_MEM_TYPE_SLOW_ Fs_management_entry fs_g_navext_entry[FS_NB_NAVIGATOR-1] |
Referenced by fat_check_device(), fat_check_nav_access_file(), fat_copy_nav(), and fat_invert_nav().
_MEM_TYPE_SLOW_ Fs_management_fast fs_g_navext_fast[FS_NB_NAVIGATOR-1] |
Referenced by fat_check_device(), fat_check_nav_access_file(), fat_copy_nav(), and fat_invert_nav().
_MEM_TYPE_FAST_ uint16_t fs_g_u16_pos_fat |
Referenced by fat_cluster_val().
_MEM_TYPE_SLOW_ uint8_t fs_g_u8_current_cache |