Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
FAT file system

FAT file system driver that provides an interface for accessing a FAT file system located on a memory device.

Supports FAT12, FAT16 and FAT32.

Data Structures

struct  Fs_clusterlist_cache
 Structure to store the cluster list cache. More...
 
struct  Fs_management
 Structure to save the variables frequently used by file system mounted. More...
 
struct  Fs_management_entry
 Structure to save the frequently variables of file system mounted. More...
 
struct  Fs_management_fast
 Structure to save the variables very frequently used by file system mounted. More...
 
union  Fs_rootdir
 Union to define a root directory. More...
 
struct  Fs_sector_cache
 Structure to store the information about sector cache (=last sector read or write on disk) More...
 
struct  Fs_segment
 Structure to define a segment. More...
 
struct  st_fs_cluster
 Structure to store cluster information. More...
 

Macros

#define _GLOBEXT_   extern
 
#define FS_BUF_SECTOR_EMPTY   0xFF
 Signal that sector cache is not valid. More...
 
#define FS_MBR_OFFSET_PART_ENTRY(num)   ((uint16_t)((uint16_t)(0x1BE)+(0x10 * num)))
 Position (unit byte) in the MBR of a partition entry. More...
 
#define Is_fat12   (FS_TYPE_FAT_12 == fs_g_nav_fast.u8_type_fat)
 
#define Is_fat16   (FS_TYPE_FAT_16 == fs_g_nav_fast.u8_type_fat)
 
#define Is_fat32   (FS_TYPE_FAT_32 == fs_g_nav_fast.u8_type_fat)
 
#define Is_unicode   (0)
 

Functions

bool fat_format (uint8_t u8_fat_type)
 This function formats the drive. More...
 
uint8_t fat_get_nbpartition (void)
 This function returns the number of partition present on selected drive. More...
 
bool fat_mount (void)
 This function mounts a partition. More...
 
bool fat_serialnumber (bool b_action, uint8_t _MEM_TYPE_SLOW_ *a_u8_sn)
 This function reads or writes a serial number. More...
 

Variables

_GLOBEXT_ _MEM_TYPE_FAST_
Fs_cluster 
fs_g_cluster
 To take time in functions: fat_getfreespace, fat_cluster_list, fat_cluster_val, fat_checkcluster. More...
 
_GLOBEXT_ _MEM_TYPE_FAST_
Fs_segment 
fs_g_seg
 Variable frequently used by many function (optimization, no parameter in function) More...
 
_GLOBEXT_ bool g_b_no_check_disk
 Variables to enable/disable the disk check before each action on disk. More...
 
_GLOBEXT_ bool g_b_string_length
 Variables to select LENGTH string mode (initialised in nav_reset()) More...
 
_GLOBEXT_ bool g_b_unicode
 Variables to select string format (initialised in nav_reset()) More...
 

Macro to access at fields in BPB sector (only used in fat_mount() function)

The name prefixed by "BPB_" are defined in "Hardware White Paper FAT"

#define LOW_16_BPB_BytsPerSec   fs_g_sector[11]
 
#define HIGH_16_BPB_BytsPerSec   fs_g_sector[12]
 
#define U8_BPB_SecPerClus   fs_g_sector[13]
 
#define LOW_16_BPB_RootEntCnt   fs_g_sector[17]
 
#define HIGH_16_BPB_RootEntCnt   fs_g_sector[18]
 
#define LOW_16_BPB_FATSz16   fs_g_sector[22]
 
#define HIGH_16_BPB_FATSz16   fs_g_sector[23]
 
#define LOW0_32_BPB_FATSz32   fs_g_sector[36]
 
#define LOW1_32_BPB_FATSz32   fs_g_sector[37]
 
#define LOW2_32_BPB_FATSz32   fs_g_sector[38]
 
#define LOW3_32_BPB_FATSz32   fs_g_sector[39]
 
#define LOW_16_BPB_TotSec16   fs_g_sector[19]
 
#define HIGH_16_BPB_TotSec16   fs_g_sector[20]
 
#define LOW0_32_BPB_TotSec32   fs_g_sector[32]
 
#define LOW1_32_BPB_TotSec32   fs_g_sector[33]
 
#define LOW2_32_BPB_TotSec32   fs_g_sector[34]
 
#define LOW3_32_BPB_TotSec32   fs_g_sector[35]
 
#define LOW_16_BPB_ResvSecCnt   fs_g_sector[14]
 
#define HIGH_16_BPB_ResvSecCnt   fs_g_sector[15]
 
#define U8_BPB_NumFATs   fs_g_sector[16]
 
#define LOW0_32_BPB_RootClus   fs_g_sector[44]
 
#define LOW1_32_BPB_RootClus   fs_g_sector[45]
 
#define LOW2_32_BPB_RootClus   fs_g_sector[46]
 
#define LOW3_32_BPB_RootClus   fs_g_sector[47]
 
#define LOW_16_BPB_FSInfo   fs_g_sector[48]
 
#define HIGH_16_BPB_FSInfo   fs_g_sector[49]
 

Constants used to sign a MBR or PBR sectors

#define FS_BR_SIGNATURE_LOW   0x55
 
#define FS_BR_SIGNATURE_HIGH   0xAA
 

Constants used in MBR sector

#define FS_PART_BOOTABLE   0x80
 
#define FS_PART_NO_BOOTABLE   0x00
 
#define FS_PART_TYPE_FAT12   0x01
 
#define FS_PART_TYPE_FAT16_INF32M   0x04
 
#define FS_PART_TYPE_FAT16_SUP32M   0x06
 
#define FS_PART_TYPE_FAT16_SUP32M_BIS   0x0E
 
#define FS_PART_TYPE_FAT32   0x0B
 
#define FS_PART_TYPE_FAT32_BIS   0x0C
 
#define FS_PART_REMOVE_MEDIA   0xF0
 
#define FS_PART_NO_REMOVE_MEDIA   0xF8
 
#define FS_PART_HARD_DISK   0x81
 
#define FS_BOOT_SIGN   0x29
 

Maximum of FAT cluster

#define FS_FAT12_MAX_CLUSTERS   4085
 
#define FS_FAT16_MAX_CLUSTERS   65525
 

Constants used in the first byte of file entry

#define FS_ENTRY_END   0x00
 
#define FS_ENTRY_DEL   0xE5
 
#define FS_ENTRY_LFN_LAST   0x40
 

Constantes used to manage the file entry

#define FS_SIZE_FILE_ENTRY   32
 
#define FS_SHIFT_B_TO_FILE_ENTRY   5
 
#define FS_SIZE_LFN_ENTRY   13
 
#define FS_SIZE_SFNAME   11
 
#define FS_SIZE_SFNAME_WITHOUT_EXT   8
 
#define FS_SIZE_SFNAME_EXT_ONLY   3
 

LIMITATIONS OF FILE SYSTEM

#define FS_NB_FAT   2
 

The unit sector of 512B is many used in file System stack

#define FS_512B   512
 
#define FS_512B_MASK   (512-1)
 
#define FS_512B_SHIFT_BIT   9
 
#define FS_SIZE_OF_SECTOR   FS_512B
 
#define FS_MASK_SIZE_OF_SECTOR   FS_512B_MASK
 
#define FS_SHIFT_B_TO_SECTOR   FS_512B_SHIFT_BIT
 
#define FS_CACHE_SIZE   512
 

Status of the fat_checkcluster() function

#define FS_CLUS_OK   0
 
#define FS_CLUS_BAD   1
 
#define FS_CLUS_END   2
 

Options of the fat_cluster_list() function

#define FS_CLUST_ACT_SEG   0x01
 
#define FS_CLUST_ACT_ONE   0x02
 
#define FS_CLUST_ACT_CLR   0x03
 

Options of the fat_cluster_val() function

#define FS_CLUST_VAL_READ   false
 
#define FS_CLUST_VAL_WRITE   true
 
#define FS_CLUST_VAL_EOL   0x0FFFFFFF
 

Main structures

typedef struct st_fs_cluster Fs_cluster
 Structure to store cluster information. More...
 

FAT type ID, used in "Fs_management_fast.u8_type_fat"

#define FS_TYPE_FAT_UNM   0
 Partition not mounted. More...
 
#define FS_TYPE_FAT_12   1
 
#define FS_TYPE_FAT_16   2
 
#define FS_TYPE_FAT_32   3
 

Value used in "Fs_management_fast.u16_entry_pos_sel_file"

#define FS_NO_SEL   0xFFFF
 Signal that a file entry isn't selected. More...
 
#define FS_END_FIND   0xFFFE
 Signal that a file entry is the last file entry accessible by system. More...
 

Macro to check the file open mode

#define Fat_file_is_open()   (fs_g_nav_entry.u8_open_mode !=0 )
 
#define Fat_file_isnot_open()   (fs_g_nav_entry.u8_open_mode ==0 )
 
#define Fat_file_close()   (fs_g_nav_entry.u8_open_mode =0 )
 

Variables initialized in drive_mount()

_GLOBEXT_ _MEM_TYPE_SLOW_
Fs_management 
fs_g_nav
 
_GLOBEXT_ _MEM_TYPE_FAST_
Fs_management_fast 
fs_g_nav_fast
 
_GLOBEXT_ _MEM_TYPE_SLOW_
Fs_management_entry 
fs_g_nav_entry
 

Variables used to update the second FAT zone

_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t fs_g_u32_first_mod_fat
 Offset (unit 512B) in fat of the first sector (unit 512B) More...
 
_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t fs_g_u32_last_mod_fat
 Offset (unit 512B) in fat of the last sector (unit 512B) More...
 

Variables used to manage the sector cache

typedef uint8_t _MEM_TYPE_SLOW_PTR_CACHE
 
_GLOBEXT_ _MEM_TYPE_SLOW_ uint8_t fs_g_sector [FS_CACHE_SIZE]
 Use "FAT sector cache" to store a sector from a file (see file_putc(), file_getc(), file_read_buf(), file_write_buf()) More...
 
_GLOBEXT_ _MEM_TYPE_SLOW_
Fs_sector_cache 
fs_g_sectorcache
 
_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t fs_gu32_addrsector
 Store the address of future cache (unit 512B) More...
 

Functions to verify navigator state

}@

bool fat_check_device (void)
 This function checks device state. More...
 
bool fat_check_mount (void)
 This function checks if the partition is mounted. More...
 
bool fat_check_noopen (void)
 This function checks if a file is not opened on current navigator. More...
 
bool fat_check_open (void)
 This function checks if a file is opened on current navigator. More...
 
bool fat_check_select (void)
 This function checks if a file is selected on current navigator. More...
 
bool fat_check_mount_noopen (void)
 This function checks if the partition is mounted and no file is opened. More...
 
bool fat_check_mount_select_noopen (void)
 This function checks if the partition is mounted and if no file is opened and a file is selected. More...
 
bool fat_check_mount_select_open (void)
 This function checks if the partition is mounted and if a file is opened. More...
 
bool fat_check_mount_select (void)
 This function checks if the partition is mounted and if a file is selected. More...
 
bool fat_check_is_file (void)
 This function checks if the selected file entry is a file and not a directory. More...
 

Functions to compute free space on a partition

uint32_t fat_getfreespace (void)
 This function returns the space free in the partition. More...
 
uint8_t fat_getfreespace_percent (void)
 This function returns the space free in percent. More...
 
bool fat_write_fat32_FSInfo (uint32_t u32_nb_free_cluster)
 This function writes the space free number in selected FAT32 partition. More...
 
uint32_t fat_read_fat32_FSInfo (void)
 This function returns the space free in the selected FAT32 partition. More...
 

Functions to manage the cluster list

bool fat_cluster_list (uint8_t opt_action, bool b_for_file)
 This function gets or clears a cluster list. More...
 
void fat_cache_clusterlist_reset (void)
 This function resets the cluster list caches. More...
 
bool fat_cluster_val (bool b_mode)
 This function returns or modifies a cluster value in FAT. More...
 
bool fat_cluster_readnext (void)
 This function is optimized to read a continue cluster list on FAT16 and FAT32. More...
 
uint8_t fat_checkcluster (void)
 This function checks the cluster value. More...
 
bool fat_allocfreespace (void)
 This function allocs a cluster list. More...
 
void fat_clear_info_fat_mod (void)
 This function clears the cache information about FAT modifications. More...
 
bool fat_clear_cluster (void)
 This function clears one cluster. More...
 
bool fat_update_fat2 (void)
 This function copies the modifications of the first FAT to the second FAT. More...
 

Functions to read or to write a file or a directory

bool fat_read_file (uint8_t mode)
 This function gets or clears a cluster list at the current position in the selected file. More...
 
bool fat_write_file (uint8_t mode, uint32_t u32_nb_sector_write)
 This function gets and eventually allocs a cluster list at the current position in the selected file. More...
 
bool fat_read_dir (void)
 This function fill the internal cache with a sector from current directory. More...
 
bool fat_initialize_dir (void)
 This function writes the directory information. More...
 

Functions to manage the entry field (fat.c)

bool fat_entry_check (bool b_type)
 This function checks the entry. More...
 
bool fat_entry_checkext (FS_STRING sz_filter)
 This function checks the file extension. More...
 
void fat_get_entry_info (void)
 This function reads information about selected file. More...
 
bool fat_entry_is_dir (void)
 This function checks if the entry file is a directory. More...
 
void fat_clear_entry_info_and_ptr (void)
 This function resets the selection pointers. More...
 
void fat_write_entry_file (void)
 This function writes the information about selected file. More...
 
bool fat_entry_shortname (FS_STRING sz_name, uint8_t u8_size_max, bool b_mode)
 This function returns or compares the short name entry. More...
 
bool fat_entry_longname (FS_STRING sz_name, uint8_t u8_size_max, bool b_mode, bool b_match_case)
 This function returns or compares the long name entry. More...
 
bool fat_check_eof_name (uint16_t character)
 Check end of name. More...
 
PTR_CACHE fat_get_ptr_entry (void)
 This function returns a cache pointer on the current entry. More...
 

Functions to manage the entry field (fat_unusual.c)

bool fat_create_entry_file_name (FS_STRING sz_name)
 This function creates the short and the long name of a new entry. More...
 
void fat_get_date (FS_STRING sz_date, bool type_date)
 This function reads the information about a date. More...
 
void fat_set_date (const FS_STRING sz_date, bool type_date)
 This function changes the date information. More...
 
bool fat_delete_file (bool b_cluster_list)
 This function deletes the file entries and cluster list. More...
 
bool fat_entry_label (bool b_action, FS_STRING sz_label)
 This function reads or writes a label in the partition. More...
 

Functions to manage the cache

bool fat_cache_read_sector (bool b_load)
 This function loads a memory sector in internal cache sector. More...
 
void fat_cache_reset (void)
 This function resets the sector cache. More...
 
void fat_cache_clear (void)
 This function clears the sector cache. More...
 
void fat_cache_mark_sector_as_dirty (void)
 This function sets a flag to signal that sector cache is modified. More...
 
bool fat_cache_flush (void)
 This function flushes the sector cache on the memory if necessary. More...
 

Functions to control access disk

bool fat_check_nav_access_disk (void)
 This function checks write access. More...
 
bool fat_check_nav_access_file (bool mode)
 This function checks all access at current file. More...
 

Functions to manage navigator switch

void fat_invert_nav (uint8_t u8_idnav)
 This function inverts the current navigation with another. More...
 
void fat_copy_nav (uint8_t u8_idnav)
 This function copies the main navigator to another navigator. More...
 

#define _GLOBEXT_   extern
//! - File system vocabulary :
//! MBR : Master Boot Record (constains four PE)
//! PE  : Partition Entry (constains a location informations about PBR)
//! PBR : Partition Boot Record
//! BPB : BIOS Parameter Block (see Hardware White Paper FAT)
//! PBR = BPB
//! FAT : File Allocation Table
//! 
#define Fat_file_close ( )    (fs_g_nav_entry.u8_open_mode =0 )
#define Fat_file_is_open ( )    (fs_g_nav_entry.u8_open_mode !=0 )

Referenced by fat_check_noopen().

#define Fat_file_isnot_open ( )    (fs_g_nav_entry.u8_open_mode ==0 )

Referenced by fat_check_open().

#define FS_512B_MASK   (512-1)
#define FS_512B_SHIFT_BIT   9
#define FS_BOOT_SIGN   0x29
#define FS_BR_SIGNATURE_HIGH   0xAA
#define FS_BR_SIGNATURE_LOW   0x55
#define FS_BUF_SECTOR_EMPTY   0xFF

Signal that sector cache is not valid.

Referenced by fat_cache_reset().

#define FS_CACHE_SIZE   512
#define FS_CLUS_BAD   1
#define FS_CLUS_END   2
#define FS_CLUS_OK   0

Referenced by fat_checkcluster().

#define FS_CLUST_ACT_CLR   0x03
#define FS_CLUST_ACT_ONE   0x02
#define FS_CLUST_ACT_SEG   0x01
#define FS_CLUST_VAL_EOL   0x0FFFFFFF

Referenced by fat_cluster_list().

#define FS_CLUST_VAL_READ   false
#define FS_CLUST_VAL_WRITE   true

Referenced by fat_cluster_list().

#define FS_END_FIND   0xFFFE

Signal that a file entry is the last file entry accessible by system.

Referenced by nav_filelist_set().

#define FS_ENTRY_LFN_LAST   0x40
#define FS_FAT12_MAX_CLUSTERS   4085

Referenced by fat_mount().

#define FS_FAT16_MAX_CLUSTERS   65525

Referenced by fat_mount().

#define FS_MASK_SIZE_OF_SECTOR   FS_512B_MASK
#define FS_MBR_OFFSET_PART_ENTRY (   num)    ((uint16_t)((uint16_t)(0x1BE)+(0x10 * num)))

Position (unit byte) in the MBR of a partition entry.

Referenced by fat_mount(), and fat_write_MBR().

#define FS_NB_FAT   2

Referenced by fat_mount().

#define FS_NO_SEL   0xFFFF
#define FS_PART_BOOTABLE   0x80

Referenced by fat_mount().

#define FS_PART_HARD_DISK   0x81
#define FS_PART_NO_BOOTABLE   0x00

Referenced by fat_mount(), and fat_write_MBR().

#define FS_PART_NO_REMOVE_MEDIA   0xF8
#define FS_PART_REMOVE_MEDIA   0xF0
#define FS_PART_TYPE_FAT12   0x01

Referenced by fat_mount(), and fat_write_MBR().

#define FS_PART_TYPE_FAT16_INF32M   0x04

Referenced by fat_mount(), and fat_write_MBR().

#define FS_PART_TYPE_FAT16_SUP32M   0x06

Referenced by fat_mount(), and fat_write_MBR().

#define FS_PART_TYPE_FAT16_SUP32M_BIS   0x0E

Referenced by fat_mount().

#define FS_PART_TYPE_FAT32   0x0B

Referenced by fat_mount(), and fat_write_MBR().

#define FS_PART_TYPE_FAT32_BIS   0x0C

Referenced by fat_mount().

#define FS_SHIFT_B_TO_FILE_ENTRY   5

Referenced by fat_read_dir().

#define FS_SHIFT_B_TO_SECTOR   FS_512B_SHIFT_BIT

Referenced by prv_df().

#define FS_SIZE_LFN_ENTRY   13

Referenced by fat_check_name(), and nav_file_name().

#define FS_SIZE_OF_SECTOR   FS_512B
#define FS_SIZE_SFNAME   11
#define FS_SIZE_SFNAME_EXT_ONLY   3
#define FS_SIZE_SFNAME_WITHOUT_EXT   8
#define FS_TYPE_FAT_12   1

Referenced by fat_mount(), and fat_select_filesystem().

#define FS_TYPE_FAT_16   2

Referenced by fat_mount(), and fat_select_filesystem().

#define FS_TYPE_FAT_32   3

Referenced by fat_mount(), and fat_select_filesystem().

#define HIGH_16_BPB_BytsPerSec   fs_g_sector[12]

Referenced by fat_mount().

#define HIGH_16_BPB_FATSz16   fs_g_sector[23]

Referenced by fat_mount(), and fat_write_PBR().

#define HIGH_16_BPB_FSInfo   fs_g_sector[49]
#define HIGH_16_BPB_ResvSecCnt   fs_g_sector[15]

Referenced by fat_mount().

#define HIGH_16_BPB_RootEntCnt   fs_g_sector[18]

Referenced by fat_mount().

#define HIGH_16_BPB_TotSec16   fs_g_sector[20]

Referenced by fat_mount().

#define LOW0_32_BPB_FATSz32   fs_g_sector[36]

Referenced by fat_mount(), and fat_write_PBR().

#define LOW0_32_BPB_RootClus   fs_g_sector[44]

Referenced by fat_mount().

#define LOW0_32_BPB_TotSec32   fs_g_sector[32]

Referenced by fat_mount().

#define LOW1_32_BPB_FATSz32   fs_g_sector[37]

Referenced by fat_mount(), and fat_write_PBR().

#define LOW1_32_BPB_RootClus   fs_g_sector[45]

Referenced by fat_mount().

#define LOW1_32_BPB_TotSec32   fs_g_sector[33]

Referenced by fat_mount().

#define LOW2_32_BPB_FATSz32   fs_g_sector[38]

Referenced by fat_mount().

#define LOW2_32_BPB_RootClus   fs_g_sector[46]

Referenced by fat_mount().

#define LOW2_32_BPB_TotSec32   fs_g_sector[34]

Referenced by fat_mount().

#define LOW3_32_BPB_FATSz32   fs_g_sector[39]

Referenced by fat_mount().

#define LOW3_32_BPB_RootClus   fs_g_sector[47]

Referenced by fat_mount().

#define LOW3_32_BPB_TotSec32   fs_g_sector[35]

Referenced by fat_mount().

#define LOW_16_BPB_BytsPerSec   fs_g_sector[11]
#define LOW_16_BPB_FATSz16   fs_g_sector[22]

Referenced by fat_mount(), and fat_write_PBR().

#define LOW_16_BPB_FSInfo   fs_g_sector[48]

Referenced by fat_mount().

#define LOW_16_BPB_ResvSecCnt   fs_g_sector[14]

Referenced by fat_mount().

#define LOW_16_BPB_RootEntCnt   fs_g_sector[17]

Referenced by fat_mount().

#define LOW_16_BPB_TotSec16   fs_g_sector[19]

Referenced by fat_mount().

#define U8_BPB_NumFATs   fs_g_sector[16]
#define U8_BPB_SecPerClus   fs_g_sector[13]

Referenced by fat_mount().

typedef struct st_fs_cluster Fs_cluster

Structure to store cluster information.

typedef uint8_t _MEM_TYPE_SLOW_* PTR_CACHE

bool fat_allocfreespace ( void  )

This function allocs a cluster list.

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variables used
//! IN :
//!   fs_g_seg.u32_addr          Last cluster value of a cluster list to link with the new cluster list
//!                              If no cluster list to link then set MSB0(fs_g_seg.u32_addr) to 0xFF
//!   fs_g_seg.u32_size_or_pos   Maximum size of cluster list to alloc (unit sector)
//! OUT:
//!   fs_g_seg.u32_addr          Return the first cluster value of the new cluster list
//!   fs_g_seg.u32_size_or_pos   The number of sector remaining (no allocated sectors, because disk fragmented or disk full)
//! 

Referenced by fat_alloc_entry_free().

void fat_cache_clear ( void  )

This function clears the sector cache.

Referenced by fat_clean_zone(), fat_write_MBR(), and fat_write_PBR().

bool fat_cache_flush ( void  )
bool fat_cache_read_sector ( bool  b_load)

This function loads a memory sector in internal cache sector.

@param     b_load   true,  load the cache with the memory sector corresponding <br>
                    false, Don't change the sector cache but change the memory address of cache <br>

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variable used
//! IN :
//!   fs_g_nav.u8_lun      drive number to read
//!   fs_gu32_addrsector   address to read (unit sector)
//! 

References CTRL_GOOD, fat_cache_flush(), fat_cache_reset(), FS_ERR_HW, fs_g_nav, fs_g_sector, fs_g_sectorcache, fs_g_status, fs_gu32_addrsector, memory_2_ram(), Fs_sector_cache::u32_addr, Fs_management::u8_lun, and Fs_sector_cache::u8_lun.

Referenced by fat_clean_zone(), fat_cluster_readnext(), fat_cluster_val(), fat_getfreespace_percent(), fat_initialize_fat(), fat_mount(), fat_read_dir(), fat_read_fat32_FSInfo(), fat_read_file(), fat_serialnumber(), fat_write_MBR(), fat_write_PBR(), and file_write_buf().

bool fat_check_eof_name ( uint16_t  character)

Check end of name.

Parameters
charactervalue of character to check
Returns
true, it is a character to signal a end of name (0,'\','/')
false, otherwise

Referenced by fat_check_name(), fat_create_short_entry_name(), and fat_entry_longname().

bool fat_check_is_file ( void  )

This function checks if the selected file entry is a file and not a directory.

Returns
true It is a file and not a directory
false otherwise

References Fat_is_not_a_file, FS_ERR_NO_FILE, and fs_g_status.

Referenced by file_ispresent(), and file_open().

bool fat_check_mount ( void  )
bool fat_check_mount_noopen ( void  )

This function checks if the partition is mounted and no file is opened.

Returns
true partition mounted and no file is opened
false otherwise

References fat_check_mount(), and fat_check_noopen().

Referenced by nav_dir_gotoparent(), nav_dir_is_root(), nav_dir_name(), nav_filelist_reset(), nav_filelist_set(), and nav_getcwd().

bool fat_check_mount_select ( void  )

This function checks if the partition is mounted and if a file is selected.

Returns
true partition mounted and a file is selected
false otherwise

References fat_check_mount(), and fat_check_select().

Referenced by file_ispresent(), nav_file_checkext(), nav_file_dateget(), nav_file_isreadonly(), and nav_file_name().

bool fat_check_mount_select_noopen ( void  )

This function checks if the partition is mounted and if no file is opened and a file is selected.

Returns
true partition mounted and no file is opened and a file is selected
false otherwise

References fat_check_mount(), fat_check_noopen(), and fat_check_select().

Referenced by file_open(), nav_dir_cd(), and nav_filelist_validpos().

bool fat_check_mount_select_open ( void  )

This function checks if the partition is mounted and if a file is opened.

Returns
true partition mounted and a file is opened
false otherwise

References fat_check_mount(), fat_check_open(), and fat_check_select().

Referenced by file_bof(), file_close(), file_eof(), file_getpos(), file_putc(), file_read(), file_read_buf(), file_seek(), file_set_eof(), and file_write_buf().

bool fat_check_nav_access_disk ( void  )

This function checks write access.

Returns
true, write access on disk possible
false, File open then write access not possible
bool fat_check_nav_access_file ( bool  mode)

This function checks all access at current file.

Parameters
modetrue, check to write access
false, check to read access
Returns
false in case of error, see global value "fs_g_status" for more detail :
mode true, File opened then write access not possibles
mode false, File opened in write mode then read access not possibles
true, access file possibles

References FOPEN_WRITE_ACCESS, FS_ERR_FILE_OPEN, FS_ERR_FILE_OPEN_WR, fs_g_nav, fs_g_nav_fast, fs_g_navext, fs_g_navext_entry, fs_g_navext_fast, fs_g_status, FS_NB_NAVIGATOR, FS_TYPE_FAT_UNM, Fs_management_fast::u16_entry_pos_sel_file, Fs_management::u32_cluster_sel_dir, and Fs_management::u8_lun.

Referenced by file_open().

bool fat_check_noopen ( void  )

This function checks if a file is not opened on current navigator.

Returns
true no file opened
false otherwise

References fat_check_device(), Fat_file_is_open, FS_ERR_TOO_FILE_OPEN, fs_g_nav_fast, fs_g_status, FS_TYPE_FAT_UNM, and Fs_management_fast::u8_type_fat.

Referenced by fat_check_mount_noopen(), fat_check_mount_select_noopen(), nav_drive_set(), nav_filelist_fileisnotopen(), nav_partition_mount(), and nav_setcwd().

bool fat_check_open ( void  )

This function checks if a file is opened on current navigator.

Returns
true a file is opened
false otherwise

References Fat_file_isnot_open, FS_ERR_FILE_NO_OPEN, and fs_g_status.

Referenced by fat_check_mount_select_open().

bool fat_check_select ( void  )

This function checks if a file is selected on current navigator.

Returns
true a file is selected
false otherwise

References FS_ERR_NO_FILE_SEL, fs_g_nav_fast, fs_g_status, FS_NO_SEL, and Fs_management_fast::u16_entry_pos_sel_file.

Referenced by fat_check_mount_select(), fat_check_mount_select_noopen(), fat_check_mount_select_open(), and nav_getcwd().

uint8_t fat_checkcluster ( void  )

This function checks the cluster value.

@return    value status <br>
           FS_CLUS_OK        Value correct <br>
           FS_CLUS_BAD       Value bad <br>
           FS_CLUS_END       It is a end of list <br>
//! Global variable used
//! IN :
//!   fs_g_cluster.u32_val       value to check
//! 

References FS_CLUS_BAD, FS_CLUS_END, FS_CLUS_OK, fs_g_cluster, Is_fat12, Is_fat16, Is_fat32, and st_fs_cluster::u32_val.

Referenced by fat_cluster_list().

bool fat_clear_cluster ( void  )

This function clears one cluster.

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variables used
//! IN :
//!   fs_g_seg.u32_addr          Cluster value to clear
//! 

Referenced by fat_alloc_entry_free().

void fat_clear_info_fat_mod ( void  )

This function clears the cache information about FAT modifications.

Referenced by fat_cluster_list().

bool fat_cluster_list ( uint8_t  opt_action,
bool  b_for_file 
)

This function gets or clears a cluster list.

@param     b_for_file        If true then it is a file cluster list else a directory cluster list  <br>
@param     opt_action        Choose action on the cluster list <br>
           FS_CLUST_ACT_SEG  Get continue memory segment corresponding at cluster list <br>
           FS_CLUST_ACT_ONE  Get only one memory sector (512B) corresponding at cluster list <br>
           FS_CLUST_ACT_CLR  Clear the cluster list <br>

@return  false in case of error, see global value "fs_g_status" for more detail
@return  true otherwise
//! Global variables used
//! IN :
//!   fs_g_seg.u32_addr          The first cluster of the cluster list
//!   fs_g_seg.u32_size_or_pos   Start position in the cluster list (unit 512B)
//! OUT:
//!   fs_g_seg.u32_addr          The memory segment address corresponding at the beginning of cluster list (only for action FS_CLUST_ACT_SEG & FS_CLUST_ACT_ONE)
//!   fs_g_seg.u32_size_or_pos   The memory segment size corresponding at cluster list read or cleared (unit 512B)
//! 

References _MEM_TYPE_FAST_, fat_cache_clusterlist_reset(), fat_cache_clusterlist_update_finish(), fat_cache_clusterlist_update_read(), fat_checkcluster(), fat_clear_info_fat_mod(), fat_cluster_readnext(), fat_cluster_val(), fat_update_fat2(), fat_write_fat32_FSInfo(), FS_CLUS_BAD, FS_CLUS_END, FS_CLUST_ACT_CLR, FS_CLUST_ACT_ONE, FS_CLUST_ACT_SEG, FS_CLUST_VAL_EOL, FS_CLUST_VAL_READ, FS_CLUST_VAL_WRITE, FS_ERR_FS, FS_ERR_OUT_LIST, fs_g_cache_clusterlist, fs_g_cluster, fs_g_nav, fs_g_seg, fs_g_status, fs_g_u8_current_cache, Is_fat12, Is_fat16, Is_fat32, LSB0, MSB0, Fs_management::rootdir, Fs_rootdir::seg, Fs_rootdir::u16_pos, Fs_rootdir::u16_size, Fs_segment::u32_addr, Fs_rootdir::u32_cluster, Fs_management::u32_offset_data, st_fs_cluster::u32_pos, Fs_management::u32_ptr_fat, Fs_segment::u32_size_or_pos, Fs_clusterlist_cache::u32_start, st_fs_cluster::u32_val, and Fs_management::u8_BPB_SecPerClus.

Referenced by fat_read_dir(), and fat_read_file().

bool fat_cluster_readnext ( void  )

This function is optimized to read a continue cluster list on FAT16 and FAT32.

Read global value "fs_g_status" in case of error :
         FS_ERR_HW            Hardware driver error
         FS_LUN_WP            Drive is read only

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variables used
//! IN :
//!   fs_g_u16_pos_fat        previous cluster position in FAT
//! OUT:
//!   fs_g_u16_pos_fat        read cluster position in FAT
//!   fs_g_cluster.u32_val    value of cluster read
//! 

References fat_cache_read_sector(), FS_CACHE_SIZE, fs_g_cluster, fs_g_sector, fs_gu32_addrsector, Is_fat32, LSB0, LSB1, LSB2, LSB3, and st_fs_cluster::u32_val.

Referenced by fat_cluster_list(), and fat_getfreespace().

bool fat_cluster_val ( bool  b_mode)

This function returns or modifies a cluster value in FAT.

@param     b_mode   false, to read a cluster value <br>
                    true,  to write a cluster value

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variables used
//! IN :
//!   fs_g_cluster.u32_pos    cluster number to read or write
//!   fs_g_cluster.u32_val    value to write
//! OUT:
//!   fs_g_cluster.u32_val    value ready
//!   fs_g_u16_pos_fat        position in FAT of the cluster to read or write
//!                           value init in case of the fat_cluster_readnext() routine is used after
//! 

References _MEM_TYPE_FAST_, fat_cache_mark_sector_as_dirty(), fat_cache_read_sector(), FS_CACHE_SIZE, FS_ERR_COMMAND, fs_g_cluster, fs_g_nav, fs_g_sector, fs_g_status, fs_g_u16_pos_fat, fs_g_u32_first_mod_fat, fs_g_u32_last_mod_fat, fs_gu32_addrsector, Is_fat12, Is_fat16, Is_fat32, LSB0, LSB1, LSB2, LSB3, MSB, st_fs_cluster::u32_pos, Fs_management::u32_ptr_fat, and st_fs_cluster::u32_val.

Referenced by fat_cluster_list(), fat_getfreespace(), and fat_getfreespace_percent().

void fat_copy_nav ( uint8_t  u8_idnav)

This function copies the main navigator to another navigator.

Parameters
u8_idnavId navigator to fill

References fs_g_nav, fs_g_nav_entry, fs_g_nav_fast, fs_g_navext, fs_g_navext_entry, fs_g_navext_fast, memcpy_ram2ram, and Fs_management_entry::u8_open_mode.

Referenced by nav_copy().

bool fat_create_entry_file_name ( FS_STRING  sz_name)

This function creates the short and the long name of a new entry.

@param     sz_name      name to create (ASCII or UNICODE)

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! IN:
//! b_unicode is a global flag to select UNICODE or ASCII
//! The name must be terminated by NULL and it can't have two dot characters.
//! 

Referenced by nav_file_create().

bool fat_delete_file ( bool  b_cluster_list)

This function deletes the file entries and cluster list.

Parameters
b_cluster_listtrue, delete file entries and cluster list false, delete only file entries
Returns
false in case of error, see global value "fs_g_status" for more detail
true otherwise

References fat_cache_mark_sector_as_dirty(), fat_get_ptr_entry(), fat_read_dir(), fat_read_file(), FS_ATTR_LFN_ENTRY, FS_CLUST_ACT_CLR, FS_ENTRY_DEL, FS_ENTRY_LFN_LAST, fs_g_nav_entry, fs_g_nav_fast, Fs_management_fast::u16_entry_pos_sel_file, and Fs_management_entry::u32_pos_in_file.

bool fat_entry_check ( bool  b_type)

This function checks the entry.

@param     b_type   entry type to compare (FS_FILE or FS_DIR)

@return    true,    the entry is a short entry and correspond to b_type
@return    false,   otherwise
//! Global variable used
//! IN :
//!   fs_g_sector       The directory sector corresponding at the current position
//!   fs_g_nav_fast.u16_entry_pos_sel_file    Position in directory of the entry file (unit entry)
//! 

References fat_get_ptr_entry(), FS_ATTR_DIRECTORY, FS_ATTR_VOLUME_ID, FS_DIR, FS_ENTRY_DEL, FS_ENTRY_END, FS_ERR_ENTRY_BAD, FS_ERR_ENTRY_EMPTY, FS_FILE, and fs_g_status.

Referenced by nav_filelist_set().

bool fat_entry_checkext ( FS_STRING  sz_filter)

This function checks the file extension.

@param     sz_filter      extension filter is a ASCII string (ex: "mp3,w*" )

@return    true, the file name have a good extension
@return    false, otherwise
//! Global variable used
//! IN :
//!   fs_g_sector       The directory sector corresponding at the current position
//!   fs_g_nav_fast.u16_entry_pos_sel_file    Position in directory of the entry file (unit entry)
//! 

References fat_get_ptr_entry().

Referenced by nav_file_checkext().

bool fat_entry_is_dir ( void  )

This function checks if the entry file is a directory.

Returns
true, this entry is a directory
false, otherwise

References FS_ATTR_DIRECTORY, FS_ERR_NO_DIR, fs_g_nav_entry, fs_g_status, and Fs_management_entry::u8_attr.

Referenced by nav_dir_cd(), nav_file_isdir(), and nav_setcwd().

bool fat_entry_label ( bool  b_action,
FS_STRING  sz_label 
)

This function reads or writes a label in the partition.

Parameters
b_actionchoose action (FS_LABEL_READ or FS_LABEL_WRITE)
sz_labelstring ASCII to store label (11B min) or to get new label (11B max)
Returns
false in case of error, see global value "fs_g_status" for more detail
true otherwise

References fat_cache_flush(), fat_cache_mark_sector_as_dirty(), fat_get_ptr_entry(), FS_ATTR_VOLUME_ID, FS_ENTRY_END, FS_ERR_ENTRY_BAD, FS_ERR_ENTRY_EMPTY, FS_ERR_NAME_INCORRECT, fs_g_status, FS_LABEL_READ, FS_LABEL_WRITE, and NULL.

Referenced by nav_partition_label().

bool fat_entry_longname ( FS_STRING  sz_name,
uint8_t  u8_size_max,
bool  b_mode,
bool  b_match_case 
)

This function returns or compares the long name entry.

@param     b_mode         action mode: <br>
                          FS_NAME_GET       to get the long name of selected file <br>
                          FS_NAME_CHECK     to compare the long name of selected file <br>
@param     sz_name        if FS_NAME_GET    then buffer to store the long name file (ASCII or UNICODE ) <br>
                          if FS_NAME_CHECK  then name to compare with long name (ASCII or UNICODE),
                                            it must be terminate by NULL or '*' value <br>

@param     b_match_case   false, ignore the case (only used in "FS_NAME_CHECK" action mode)
@param     u8_size_max    buffer size (unit ASCII or UNICODE ) (ignored in "FS_NAME_CHECK" mode)

@return    false is not the end of long name, or in case of error, see global value "fs_g_status" for more detail
@return    true, the name is correct or read is finish
//! Global variable used
//! IN :
//!   fs_g_sector       The directory sector corresponding at the current position
//!   fs_g_nav_fast.u16_entry_pos_sel_file    Position in directory of the entry file (unit entry)
//! 

References fat_check_eof_name(), fat_get_ptr_entry(), FS_ATTR_LFN_ENTRY, FS_ENTRY_DEL, FS_ENTRY_END, FS_ENTRY_LFN_LAST, FS_ERR_ENTRY_BAD, FS_ERR_NAME_INCORRECT, fs_g_status, FS_NAME_GET, FS_NO_LAST_LFN_ENTRY, FS_SIZE_FILE_ENTRY, g_b_string_length, Is_unicode, LSB, and MSB.

Referenced by nav_file_name().

bool fat_entry_shortname ( FS_STRING  sz_name,
uint8_t  u8_size_max,
bool  b_mode 
)

This function returns or compares the short name entry.

@param     b_mode         action mode: <br>
                          FS_NAME_GET       to get the short name of selected file <br>
                          FS_NAME_CHECK     to compare the short name of selected file <br>
@param     sz_name        if FS_NAME_GET    then buffer to store the short name file (ASCII or UNICODE ) <br>
                          if FS_NAME_CHECK  then name to compare with short name (ASCII or UNICODE),
                                            it must be terminate by NULL or '*' value <br>
@param     u8_size_max    buffer size (unit ASCII or UNICODE ) (ignored in "FS_NAME_CHECK" mode)

@return    false, in case of error, see global value "fs_g_status" for more detail
@return    true, the name is correct or read OK
//! Global variable used
//! IN :
//!   fs_g_sector       The directory sector corresponding at the current position
//!   fs_g_nav_fast.u16_entry_pos_sel_file    Position in directory of the entry file (unit entry)
//! 

References fat_get_ptr_entry(), FS_ERR_NAME_INCORRECT, fs_g_status, FS_NAME_GET, FS_SIZE_SFNAME, FS_SIZE_SFNAME_WITHOUT_EXT, g_b_string_length, Is_unicode, and MSB.

Referenced by nav_file_name().

bool fat_format ( uint8_t  u8_fat_type)

This function formats the drive.

This function formats the drive.

@param     u8_fat_type          Select the type of format <br>
           FS_FORMAT_DEFAULT,   The file system module choose the better FAT format for the drive space <br>
           FS_FORMAT_FAT,       The FAT12 or FAT16 is used to format the drive, if possible (disk space <2GB) <br>
           FS_FORMAT_FAT32,     The FAT32 is used to format the drive, if possible (disk space >32MB) <br>
           FS_FORMAT_NOMBR_FLAG if you don't want a MRB in disk then add this flag (e.g. FAT format on a CD support)

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variables used
//! IN :
//! fs_g_nav.u8_lun        indicate the drive to format
//!
//! This routine can't format a multi-partiton, if the disk contains a multi-partition area
//! then the multi-partition will be erased and replaced by a single partition on all disk space.
//! 

References fat_cache_flush(), fat_clean_zone(), fat_initialize_fat(), fat_select_filesystem(), fat_write_MBR(), fat_write_PBR(), FS_FORMAT_NOMBR_FLAG, fs_g_nav, fs_s_u32_size_partition, mem_read_capacity(), and Fs_management::u8_lun.

void fat_get_date ( FS_STRING  sz_date,
bool  type_date 
)

This function reads the information about a date.

Parameters
type_datechoose the date type (FS_DATE_LAST_WRITE or FS_DATE_CREATION)
sz_datetable to store the date
storage format (ASCII) = "YYYYMMDDHHMMSSMS" = year, month, day, hour, minute, second, millisecond

References fat_get_ptr_entry(), fat_translatedate_number_to_ascii(), and FS_DATE_LAST_WRITE.

Referenced by nav_file_dateget().

void fat_get_entry_info ( void  )

This function reads information about selected file.

//! Global variable used
//! IN :
//!   fs_g_sector       The directory sector corresponding at the current position
//!   fs_g_nav_fast.u16_entry_pos_sel_file    Position in directory of the entry file (unit entry)
//! OUT:
//!   fs_g_nav_entry. u32_cluster, u8_attr, u32_size
//! 

References fat_get_ptr_entry(), fs_g_nav_entry, LSB0, LSB1, LSB2, LSB3, Fs_management_entry::u32_cluster, Fs_management_entry::u32_size, and Fs_management_entry::u8_attr.

Referenced by nav_dir_gotoparent(), and nav_filelist_set().

uint8_t fat_get_nbpartition ( void  )

This function returns the number of partition present on selected drive.

uint32_t fat_getfreespace ( void  )
uint8_t fat_getfreespace_percent ( void  )

This function returns the space free in percent.

@return    percent of free space (1 to 100)
           if 0, then error or full
//! More speed than fat_getfreespace() routine but error delta 1%
//! 

References fat_cache_read_sector(), fat_cluster_val(), fat_getfreespace(), fat_read_fat32_FSInfo(), FS_CLUST_VAL_READ, fs_g_cluster, fs_g_nav, fs_g_sector, fs_gu32_addrsector, Is_fat12, Is_fat16, Is_fat32, Fs_management::u32_CountofCluster, Fs_management::u32_fat_size, st_fs_cluster::u32_pos, and Fs_management::u8_BPB_SecPerClus.

Referenced by nav_partition_freespace_percent().

bool fat_initialize_dir ( void  )

This function writes the directory information.

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variables used
//! IN :
//!   fs_g_seg.u32_addr          cluster value of a directory
//! OUT:
//!   update the sector cache with init directory data
//! 
void fat_invert_nav ( uint8_t  u8_idnav)

This function inverts the current navigation with another.

Parameters
u8_idnavId navigator to invert

References _MEM_TYPE_SLOW_, fs_g_nav, fs_g_nav_entry, fs_g_nav_fast, fs_g_navext, fs_g_navext_entry, fs_g_navext_fast, Max, and memcpy_ram2ram.

Referenced by nav_select().

bool fat_mount ( void  )

This function mounts a partition.

This function mounts a partition.

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variables used
//! IN :
//!   fs_g_nav.u8_lun            Indicate the drive to mount
//!   fs_g_nav.u8_partition      Indicate the partition to mount (if FS_MULTI_PARTITION =  true )
//! OUT:
//!   fs_g_nav                   update structure
//! If the FS_MULTI_PARTITION option is disabled
//! then the mount routine selects the first partition supported by file system. <br>
//! 

References fat_cache_read_sector(), fat_check_device(), fat_clear_entry_info_and_ptr(), FS_512B, FS_BR_SIGNATURE_HIGH, FS_BR_SIGNATURE_LOW, FS_ERR_NO_FORMAT, FS_ERR_NO_PART, FS_ERR_NO_SUPPORT_PART, FS_FAT12_MAX_CLUSTERS, FS_FAT16_MAX_CLUSTERS, fs_g_nav, fs_g_nav_fast, fs_g_sector, fs_g_status, fs_gu32_addrsector, FS_MBR_OFFSET_PART_ENTRY, FS_NB_FAT, FS_PART_BOOTABLE, FS_PART_NO_BOOTABLE, FS_PART_TYPE_FAT12, FS_PART_TYPE_FAT16_INF32M, FS_PART_TYPE_FAT16_SUP32M, FS_PART_TYPE_FAT16_SUP32M_BIS, FS_PART_TYPE_FAT32, FS_PART_TYPE_FAT32_BIS, FS_SIZE_FILE_ENTRY, FS_TYPE_FAT_12, FS_TYPE_FAT_16, FS_TYPE_FAT_32, FS_TYPE_FAT_UNM, HIGH_16_BPB_BytsPerSec, HIGH_16_BPB_FATSz16, HIGH_16_BPB_ResvSecCnt, HIGH_16_BPB_RootEntCnt, HIGH_16_BPB_TotSec16, LOW0_32_BPB_FATSz32, LOW0_32_BPB_RootClus, LOW0_32_BPB_TotSec32, LOW1_32_BPB_FATSz32, LOW1_32_BPB_RootClus, LOW1_32_BPB_TotSec32, LOW2_32_BPB_FATSz32, LOW2_32_BPB_RootClus, LOW2_32_BPB_TotSec32, LOW3_32_BPB_FATSz32, LOW3_32_BPB_RootClus, LOW3_32_BPB_TotSec32, LOW_16_BPB_FATSz16, LOW_16_BPB_FSInfo, LOW_16_BPB_ResvSecCnt, LOW_16_BPB_RootEntCnt, LOW_16_BPB_TotSec16, LSB, LSB0, LSB1, LSB2, LSB3, mem_sector_size(), MSB, Fs_management::rootdir, Fs_rootdir::seg, Fs_management::u16_offset_FSInfo, Fs_rootdir::u16_pos, Fs_rootdir::u16_size, Fs_rootdir::u32_cluster, Fs_management::u32_cluster_sel_dir, Fs_management::u32_CountofCluster, Fs_management::u32_fat_size, Fs_management::u32_offset_data, Fs_management::u32_ptr_fat, U8_BPB_SecPerClus, Fs_management::u8_BPB_SecPerClus, Fs_management::u8_lun, and Fs_management_fast::u8_type_fat.

Referenced by fat_check_mount(), and nav_partition_mount().

bool fat_read_dir ( void  )

This function fill the internal cache with a sector from current directory.

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variable used
//! IN :
//!   fs_g_nav.u32_cluster_sel_dir           First cluster of current directory
//!   fs_g_nav_fast.u16_entry_pos_sel_file   Position in directory (unit entry)
//! 

References fat_cache_read_sector(), fat_cluster_list(), FS_512B_SHIFT_BIT, FS_CLUST_ACT_ONE, fs_g_nav, fs_g_nav_fast, fs_g_sectorcache, fs_g_seg, fs_gu32_addrsector, FS_SHIFT_B_TO_FILE_ENTRY, Fs_management_fast::u16_entry_pos_sel_file, Fs_segment::u32_addr, Fs_management::u32_cluster_sel_dir, Fs_sector_cache::u32_clusterlist_pos, Fs_sector_cache::u32_clusterlist_start, Fs_segment::u32_size_or_pos, Fs_management::u8_lun, and Fs_sector_cache::u8_lun.

Referenced by fat_alloc_entry_free(), fat_delete_file(), fat_find_short_entry_name(), fat_garbage_collector_entry(), file_close(), nav_dir_gotoparent(), nav_file_checkext(), nav_file_dateget(), nav_file_name(), nav_filelist_set(), and nav_partition_label().

uint32_t fat_read_fat32_FSInfo ( void  )

This function returns the space free in the selected FAT32 partition.

Returns
the number of sector free (if 0xFFFFFFFF, then no value available in FSInfo Sector)

References const_FSI_LeadSig, const_FSI_StrucSig, fat_cache_read_sector(), FS_BR_SIGNATURE_HIGH, FS_BR_SIGNATURE_LOW, fs_g_nav, fs_g_sector, fs_gu32_addrsector, LSB0, LSB1, LSB2, LSB3, memcmp_code2ram, Fs_management::u16_offset_FSInfo, and Fs_management::u32_ptr_fat.

Referenced by fat_getfreespace(), and fat_getfreespace_percent().

bool fat_read_file ( uint8_t  mode)

This function gets or clears a cluster list at the current position in the selected file.

@param     mode              Choose action <br>
           FS_CLUST_ACT_SEG  Get memory segment corresponding at the position in selected file <br>
           FS_CLUST_ACT_ONE  Store in internal cache the sector corresponding at the position in selected file <br>
           FS_CLUST_ACT_CLR  Clear the cluster list corresponding at the position in selected file <br>

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variable used
//! IN :
//!   fs_g_nav_entry.u32_cluster       First cluster of selected file
//!   fs_g_nav_entry.u32_pos_in_file   Position in file (unit byte)
//! 

References fat_cache_read_sector(), fat_cluster_list(), FS_512B_MASK, FS_512B_SHIFT_BIT, FS_CLUST_ACT_CLR, FS_CLUST_ACT_ONE, FS_CLUST_ACT_SEG, FS_ERR_OUT_LIST, fs_g_nav, fs_g_nav_entry, fs_g_sectorcache, fs_g_seg, fs_g_status, fs_gu32_addrsector, Fs_segment::u32_addr, Fs_management_entry::u32_cluster, Fs_sector_cache::u32_clusterlist_pos, Fs_sector_cache::u32_clusterlist_start, Fs_management_entry::u32_pos_in_file, Fs_segment::u32_size_or_pos, Fs_management::u8_lun, and Fs_sector_cache::u8_lun.

Referenced by fat_delete_file(), file_getc(), file_read(), file_read_buf(), and file_set_eof().

bool fat_serialnumber ( bool  b_action,
uint8_t _MEM_TYPE_SLOW_ a_u8_sn 
)

This function reads or writes a serial number.

This function reads or writes a serial number.

Parameters
b_actionchoose action (FS_SN_READ or FS_SN_WRITE)
a_u8_snarray to store or get the serial number (uint8_t[4])
Returns
false in case of error, see global value "fs_g_status" for more detail
true otherwise

References fat_cache_flush(), fat_cache_mark_sector_as_dirty(), fat_cache_read_sector(), fs_g_nav, fs_g_sector, fs_gu32_addrsector, FS_SN_READ, Is_fat12, Is_fat16, and Fs_management::u32_ptr_fat.

Referenced by nav_partition_serialnumber().

void fat_set_date ( const FS_STRING  sz_date,
bool  type_date 
)

This function changes the date information.

@param     type_date         choose date field (FS_DATE_LAST_WRITE or FS_DATE_CREATION)
@param     sz_date           table with date information <br>
                             storage format (ASCII) = "YYYYMMDDHHMMSSMS" = year, month, day, hour, minute, second, millisecond
//! OUT, update cache sector with the new date
//! 
bool fat_update_fat2 ( void  )

This function copies the modifications of the first FAT to the second FAT.

Returns
false in case of error, see global value "fs_g_status" for more detail
true otherwise

Referenced by fat_cluster_list().

void fat_write_entry_file ( void  )

This function writes the information about selected file.

//! Global variable used
//! IN :
//!   fs_g_sector       The directory sector corresponding at the current position
//!   fs_g_nav_fast.u16_entry_pos_sel_file    Position in directory of the entry file (unit entry)
//! OUT:
//!   fs_g_sector    Updated
//! 

Write the Attribute

Write the size of file

Referenced by file_close().

bool fat_write_fat32_FSInfo ( uint32_t  u32_nb_free_cluster)

This function writes the space free number in selected FAT32 partition.

Read global value "fs_g_status" in case of error : FS_ERR_HW Hardware driver error FS_ERR_HW_NO_PRESENT Device not present FS_LUN_WP Drive is read only

Returns
false in case of error, see global value "fs_g_status" for more detail
true otherwise

Referenced by fat_cluster_list(), fat_getfreespace(), and fat_write_PBR().

bool fat_write_file ( uint8_t  mode,
uint32_t  u32_nb_sector_write 
)

This function gets and eventually allocs a cluster list at the current position in the selected file.

@param     mode                 Choose action <br>
           FS_CLUST_ACT_SEG     Get and eventually alloc a cluster list <br>
           FS_CLUST_ACT_ONE     Get and eventually alloc a cluster list for one sector, and load this sector in internal cache <br>
@param     u32_nb_sector_write  maximum number of sector to get and eventually to alloc for the selected file (ignored if mode = FS_CLUST_ACT_ONE)

@return    false in case of error, see global value "fs_g_status" for more detail
@return    true otherwise
//! Global variable used
//! IN :
//!   fs_g_nav_entry.u32_cluster       First cluster of selected file
//!   fs_g_nav_entry.u32_pos_in_file   Position in the file (unit byte)
//! 

Referenced by file_putc(), and file_write_buf().

_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t fs_g_u32_first_mod_fat

Offset (unit 512B) in fat of the first sector (unit 512B)

Referenced by fat_cluster_val().

_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t fs_g_u32_last_mod_fat

Offset (unit 512B) in fat of the last sector (unit 512B)

Referenced by fat_cluster_val().

_GLOBEXT_ bool g_b_no_check_disk

Variables to enable/disable the disk check before each action on disk.

Referenced by fat_check_device(), nav_checkdisk_disable(), nav_checkdisk_enable(), and nav_reset().

_GLOBEXT_ bool g_b_unicode

Variables to select string format (initialised in nav_reset())

Referenced by nav_reset().