User Datagram Protocol module.
#include "lwip/opt.h"
#include "lwip/udp.h"
#include "lwip/def.h"
#include "lwip/memp.h"
#include "lwip/inet_chksum.h"
#include "lwip/ip_addr.h"
#include "lwip/ip6.h"
#include "lwip/ip6_addr.h"
#include "lwip/netif.h"
#include "lwip/icmp.h"
#include "lwip/icmp6.h"
#include "lwip/stats.h"
#include "lwip/snmp.h"
#include "arch/perf.h"
#include "lwip/dhcp.h"
#include <string.h>
Macros | |
#define | UDP_ENSURE_LOCAL_PORT_RANGE(port) (((port) & ~UDP_LOCAL_PORT_RANGE_START) + UDP_LOCAL_PORT_RANGE_START) |
#define | UDP_LOCAL_PORT_RANGE_END 0xffff |
#define | UDP_LOCAL_PORT_RANGE_START 0xc000 |
Functions | |
err_t | udp_bind (struct udp_pcb *pcb, ip_addr_t *ipaddr, u16_t port) |
Bind an UDP PCB. More... | |
err_t | udp_connect (struct udp_pcb *pcb, ip_addr_t *ipaddr, u16_t port) |
Connect an UDP PCB. More... | |
void | udp_disconnect (struct udp_pcb *pcb) |
Disconnect a UDP PCB. More... | |
void | udp_init (void) |
Initialize this module. More... | |
void | udp_input (struct pbuf *p, struct netif *inp) |
Process an incoming UDP datagram. More... | |
struct udp_pcb * | udp_new (void) |
Create a UDP PCB. More... | |
struct udp_pcb * | udp_new_ip6 (void) |
Create a UDP PCB for IPv6. More... | |
static u16_t | udp_new_port (void) |
Allocate a new local UDP port. More... | |
void | udp_recv (struct udp_pcb *pcb, udp_recv_fn recv, void *recv_arg) |
Set a receive callback for a UDP PCB. More... | |
void | udp_remove (struct udp_pcb *pcb) |
Remove an UDP PCB. More... | |
err_t | udp_send (struct udp_pcb *pcb, struct pbuf *p) |
Send data using UDP. More... | |
err_t | udp_sendto (struct udp_pcb *pcb, struct pbuf *p, ip_addr_t *dst_ip, u16_t dst_port) |
Send data to a specified address using UDP. More... | |
err_t | udp_sendto_if (struct udp_pcb *pcb, struct pbuf *p, ip_addr_t *dst_ip, u16_t dst_port, struct netif *netif) |
Send data to a specified address using UDP. More... | |
err_t | udp_sendto_if_src (struct udp_pcb *pcb, struct pbuf *p, ip_addr_t *dst_ip, u16_t dst_port, struct netif *netif, ip_addr_t *src_ip) |
Same as udp_sendto_if(), but with source address. More... | |
Variables | |
struct udp_pcb * | udp_pcbs |
static u16_t | udp_port = UDP_LOCAL_PORT_RANGE_START |
#define UDP_ENSURE_LOCAL_PORT_RANGE | ( | port | ) | (((port) & ~UDP_LOCAL_PORT_RANGE_START) + UDP_LOCAL_PORT_RANGE_START) |
Referenced by udp_init().
#define UDP_LOCAL_PORT_RANGE_END 0xffff |
Referenced by udp_new_port().
#define UDP_LOCAL_PORT_RANGE_START 0xc000 |
Referenced by udp_new_port().
Bind an UDP PCB.
pcb | UDP PCB to be bound with a local address ipaddr and port. |
ipaddr | local IP address to bind with. Use IP_ADDR_ANY to bind to all local interfaces. |
port | local UDP port to bind with. Use 0 to automatically bind to a random port between UDP_LOCAL_PORT_RANGE_START and UDP_LOCAL_PORT_RANGE_END. |
ipaddr & port are expected to be in the same byte order as in the pcb.
References ERR_OK, ERR_USE, ip_2_ipX, ip_get_option, IP_PCB_IPVER_EQ, ipX_addr_cmp, ipX_addr_debug_print, ipX_addr_isany, ipX_addr_set_ipaddr, udp_pcb::local_port, LWIP_ASSERT, LWIP_DBG_STATE, LWIP_DBG_TRACE, LWIP_DEBUGF, udp_pcb::next, NULL, PCB_ISIPV6, snmp_insert_udpidx_tree, SOF_REUSEADDR, U16_F, UDP_DEBUG, udp_new_port(), and udp_pcbs.
Referenced by dhcp_inform(), dhcp_start(), dns_alloc_random_port(), dns_init(), lwip_dhcpserver_start_threadsafe(), lwip_netconn_do_bind(), and udp_connect().
Connect an UDP PCB.
This will associate the UDP PCB with the remote address.
pcb | UDP PCB to be connected with remote address ipaddr and port. |
ipaddr | remote IP address to connect with. |
port | remote UDP port to connect with. |
ipaddr & port are expected to be in the same byte order as in the pcb.
The udp pcb is bound to a random local port if not already bound.
TODO: this functionality belongs in upper layers
References ERR_OK, ERR_RTE, udp_pcb::flags, ip4_addr_get_u32, netif::ip_addr, ip_addr_isany, ip_route(), ipX_2_ip, ipX_addr_copy, ipX_addr_debug_print, ipX_addr_set_any, ipX_addr_set_ipaddr, udp_pcb::local_port, LWIP_DBG_STATE, LWIP_DBG_TRACE, LWIP_DEBUGF, udp_pcb::next, NULL, PCB_ISIPV6, udp_pcb::remote_port, U16_F, udp_bind(), UDP_DEBUG, UDP_FLAGS_CONNECTED, udp_pcbs, and UDP_STATS_INC.
Referenced by dhcp_start(), and lwip_netconn_do_connect().
Disconnect a UDP PCB.
pcb | the udp pcb to disconnect. |
References udp_pcb::flags, ipX_addr_set_any, PCB_ISIPV6, udp_pcb::remote_port, and UDP_FLAGS_CONNECTED.
Referenced by lwip_netconn_do_disconnect(), and lwip_tiny_dhcpserver_stop_threadsafe().
Initialize this module.
References LWIP_RAND, UDP_ENSURE_LOCAL_PORT_RANGE, and udp_port.
Referenced by lwip_init().
Process an incoming UDP datagram.
Given an incoming UDP datagram (as a chain of pbufs) this function finds a corresponding UDP PCB and hands over the pbuf to the pcbs recv function. If no pcb is found or the datagram is incorrect, the pbuf is freed.
p | pbuf to be demultiplexed to a UDP PCB (p->payload pointing to the UDP header) |
inp | network interface on which the datagram was received. |
References netif::dhcp, DHCP_CLIENT_PORT, DHCP_SERVER_PORT, ERR_OK, udp_pcb::flags, icmp_port_unreach, udp_pcb::ip4, ip6_addr_cmp, ip6_addr_isany, ip6_addr_ismulticast, ip6_current_dest_addr, ip6_current_src_addr, netif::ip_addr, ip_addr_cmp, ip_addr_isbroadcast, ip_addr_ismulticast, ip_addr_netcmp, ip_current_dest_addr, ip_current_header, ip_current_header_proto, ip_current_header_tot_len, ip_current_is_v6, ip_current_src_addr, ip_get_option, IP_PCB_IPVER_INPUT_MATCH, IP_PROTO_UDP, IP_PROTO_UDPLITE, ipX_2_ip, ipX_2_ip6, ipX_addr_cmp, ipX_addr_debug_print, ipX_addr_isany, ipX_chksum_pseudo, ipX_chksum_pseudo_partial, ipX_current_dest_addr, ipX_current_src_addr, pbuf::len, udp_pcb::local_port, LWIP_ASSERT, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_TRACE, LWIP_DEBUGF, LWIP_IGMP, LWIP_IPV6, netif_get_ip6_addr_match(), netif::netmask, udp_pcb::next, ntohs, NULL, pbuf::payload, pbuf_alloc(), pbuf_copy(), pbuf_free(), pbuf_header(), pbuf_header_force(), PBUF_RAM, PBUF_RAW, dhcp::pcb, PCB_ISIPV6, PERF_START, PERF_STOP, udp_pcb::recv, udp_pcb::recv_arg, udp_pcb::remote_port, snmp_inc_udpindatagrams, snmp_inc_udpinerrors, snmp_inc_udpnoports, SOF_BROADCAST, SOF_REUSEADDR, pbuf::tot_len, U16_F, UDP_DEBUG, udp_debug_print, UDP_FLAGS_CONNECTED, UDP_HLEN, udp_pcbs, and UDP_STATS_INC.
Referenced by ip6_input(), and ip_input().
Create a UDP PCB.
References memp_malloc(), and NULL.
Referenced by dhcp_inform(), dhcp_start(), dns_alloc_random_port(), dns_init(), lwip_dhcpserver_start_threadsafe(), pcb_new(), and udp_new_ip6().
Create a UDP PCB for IPv6.
Allocate a new local UDP port.
References udp_pcb::local_port, udp_pcb::next, NULL, UDP_LOCAL_PORT_RANGE_END, UDP_LOCAL_PORT_RANGE_START, udp_pcbs, and udp_port.
Referenced by udp_bind().
void udp_recv | ( | struct udp_pcb * | pcb, |
udp_recv_fn | recv, | ||
void * | recv_arg | ||
) |
Set a receive callback for a UDP PCB.
This callback will be called when receiving a datagram for the pcb.
pcb | the pcb for which to set the recv callback |
recv | function pointer of the callback function |
recv_arg | additional argument to pass to the callback function |
References udp_pcb::ip4, udp_pcb::recv, recv(), and udp_pcb::recv_arg.
Referenced by dhcp_start(), dns_alloc_random_port(), dns_init(), lwip_dhcpserver_start_threadsafe(), and pcb_new().
Remove an UDP PCB.
pcb | UDP PCB to be removed. The PCB is removed from the list of UDP PCB's and the data structure is freed from memory. |
References memp_free(), udp_pcb::next, NULL, and snmp_delete_udpidx_tree.
Referenced by dhcp_inform(), dhcp_start(), dhcp_stop(), dns_alloc_random_port(), dns_call_found(), lwip_netconn_do_delconn(), and lwip_tiny_dhcpserver_stop_threadsafe().
Send data using UDP.
pcb | UDP PCB used to send the data. |
p | chain of pbuf's to be sent. |
The datagram will be sent to the current remote_ip & remote_port stored in pcb. If the pcb is not bound to a port, it will automatically be bound to a random port.
References ipX_2_ip, udp_pcb::remote_port, and udp_sendto().
Referenced by lwip_netconn_do_send().
Send data to a specified address using UDP.
pcb | UDP PCB used to send the data. |
p | chain of pbuf's to be sent. |
dst_ip | Destination IP address. |
dst_port | Destination UDP port. |
dst_ip & dst_port are expected to be in the same byte order as in the pcb.
If the PCB already has a remote address association, it will be restored after the data is sent.
Referenced by dns_send(), lwip_dhcp_server_fn(), lwip_netconn_do_send(), and udp_send().
err_t udp_sendto_if | ( | struct udp_pcb * | pcb, |
struct pbuf * | p, | ||
ip_addr_t * | dst_ip, | ||
u16_t | dst_port, | ||
struct netif * | netif | ||
) |
Send data to a specified address using UDP.
The netif used for sending can be specified.
This function exists mainly for DHCP, to be able to send UDP packets on a netif that is still down.
pcb | UDP PCB used to send the data. |
p | chain of pbuf's to be sent. |
dst_ip | Destination IP address. |
dst_port | Destination UDP port. |
netif | the netif used for sending. |
dst_ip & dst_port are expected to be in the same byte order as in the pcb.
Referenced by dhcp_inform(), dhcp_rebind(), dhcp_reboot(), dhcp_release(), and dhcp_renew().
err_t udp_sendto_if_src | ( | struct udp_pcb * | pcb, |
struct pbuf * | p, | ||
ip_addr_t * | dst_ip, | ||
u16_t | dst_port, | ||
struct netif * | netif, | ||
ip_addr_t * | src_ip | ||
) |
Same as udp_sendto_if(), but with source address.
Referenced by dhcp_decline(), dhcp_discover(), and dhcp_select().
struct udp_pcb* udp_pcbs |
Referenced by udp_bind(), udp_connect(), udp_input(), and udp_new_port().
|
static |
Referenced by udp_init(), and udp_new_port().