User Datagram Protocol module.
#include "lwip/opt.h"
#include "lwip/udp.h"
#include "lwip/def.h"
#include "lwip/memp.h"
#include "lwip/inet_chksum.h"
#include "lwip/ip_addr.h"
#include "lwip/netif.h"
#include "lwip/icmp.h"
#include "lwip/stats.h"
#include "lwip/snmp.h"
#include "arch/perf.h"
#include "lwip/dhcp.h"
#include <string.h>
Macros | |
#define | UDP_LOCAL_PORT_RANGE_END 0xffff |
#define | UDP_LOCAL_PORT_RANGE_START 0xc000 |
Functions | |
err_t | udp_bind (struct udp_pcb *pcb, ip_addr_t *ipaddr, u16_t port) |
Bind an UDP PCB. More... | |
err_t | udp_connect (struct udp_pcb *pcb, ip_addr_t *ipaddr, u16_t port) |
Connect an UDP PCB. More... | |
void | udp_disconnect (struct udp_pcb *pcb) |
Disconnect a UDP PCB. More... | |
void | udp_input (struct pbuf *p, struct netif *inp) |
Process an incoming UDP datagram. More... | |
struct udp_pcb * | udp_new (void) |
Create a UDP PCB. More... | |
void | udp_recv (struct udp_pcb *pcb, udp_recv_fn recv, void *recv_arg) |
Set a receive callback for a UDP PCB. More... | |
void | udp_remove (struct udp_pcb *pcb) |
Remove an UDP PCB. More... | |
err_t | udp_send (struct udp_pcb *pcb, struct pbuf *p) |
Send data using UDP. More... | |
err_t | udp_sendto (struct udp_pcb *pcb, struct pbuf *p, ip_addr_t *dst_ip, u16_t dst_port) |
Send data to a specified address using UDP. More... | |
err_t | udp_sendto_if (struct udp_pcb *pcb, struct pbuf *p, ip_addr_t *dst_ip, u16_t dst_port, struct netif *netif) |
Send data to a specified address using UDP. More... | |
Variables | |
struct udp_pcb * | udp_pcbs |
#define UDP_LOCAL_PORT_RANGE_END 0xffff |
Referenced by udp_bind().
#define UDP_LOCAL_PORT_RANGE_START 0xc000 |
Referenced by udp_bind().
Bind an UDP PCB.
pcb | UDP PCB to be bound with a local address ipaddr and port. |
ipaddr | local IP address to bind with. Use IP_ADDR_ANY to bind to all local interfaces. |
port | local UDP port to bind with. Use 0 to automatically bind to a random port between UDP_LOCAL_PORT_RANGE_START and UDP_LOCAL_PORT_RANGE_END. |
ipaddr & port are expected to be in the same byte order as in the pcb.
References ERR_OK, ERR_USE, ip4_addr1_16, ip4_addr2_16, ip4_addr3_16, ip4_addr4_16, ip_addr_cmp, ip_addr_debug_print, ip_addr_isany, ip_addr_set, udp_pcb::local_port, LWIP_ASSERT, LWIP_DBG_STATE, LWIP_DBG_TRACE, LWIP_DEBUGF, udp_pcb::next, NULL, snmp_insert_udpidx_tree, SOF_REUSEADDR, UDP_DEBUG, UDP_LOCAL_PORT_RANGE_END, UDP_LOCAL_PORT_RANGE_START, and udp_pcbs.
Referenced by dhcp_inform(), dhcp_start(), do_bind(), and udp_connect().
Connect an UDP PCB.
This will associate the UDP PCB with the remote address.
pcb | UDP PCB to be connected with remote address ipaddr and port. |
ipaddr | remote IP address to connect with. |
port | remote UDP port to connect with. |
ipaddr & port are expected to be in the same byte order as in the pcb.
The udp pcb is bound to a random local port if not already bound.
TODO: this functionality belongs in upper layers
References ERR_OK, ERR_RTE, udp_pcb::flags, ip4_addr1_16, ip4_addr2_16, ip4_addr3_16, ip4_addr4_16, netif::ip_addr, ip_addr_isany, ip_addr_set, ip_route(), udp_pcb::local_port, LWIP_DBG_STATE, LWIP_DBG_TRACE, LWIP_DEBUGF, udp_pcb::next, NULL, udp_pcb::remote_port, udp_bind(), UDP_DEBUG, UDP_FLAGS_CONNECTED, udp_pcbs, and UDP_STATS_INC.
Referenced by dhcp_start(), and do_connect().
Disconnect a UDP PCB.
pcb | the udp pcb to disconnect. |
References udp_pcb::flags, ip_addr_set_any, udp_pcb::remote_port, and UDP_FLAGS_CONNECTED.
Referenced by do_disconnect().
Process an incoming UDP datagram.
Given an incoming UDP datagram (as a chain of pbufs) this function finds a corresponding UDP PCB and hands over the pbuf to the pcbs recv function. If no pcb is found or the datagram is incorrect, the pbuf is freed.
p | pbuf to be demultiplexed to a UDP PCB. |
inp | network interface on which the datagram was received. |
References current_iphdr_dest, current_iphdr_src, netif::dhcp, DHCP_CLIENT_PORT, DHCP_SERVER_PORT, ERR_OK, udp_pcb::flags, icmp_dest_unreach(), ICMP_DUR_PORT, if(), inet_chksum_pseudo(), inet_chksum_pseudo_partial(), ip4_addr1_16, ip4_addr2_16, ip4_addr3_16, ip4_addr4_16, netif::ip_addr, ip_addr_cmp, ip_addr_isany, ip_addr_isbroadcast, ip_addr_ismulticast, ip_current_dest_addr, ip_current_src_addr, IP_PROTO_UDP, IP_PROTO_UDPLITE, IP_SOF_BROADCAST_RECV, IPH_HL, IPH_PROTO, iphdr, udp_pcb::local_port, LWIP_ASSERT, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_TRACE, LWIP_DEBUGF, LWIP_IGMP, udp_pcb::next, ntohs, NULL, pbuf::payload, pbuf_alloc(), pbuf_copy(), pbuf_free(), pbuf_header(), PBUF_RAM, PBUF_RAW, dhcp::pcb, PERF_START, PERF_STOP, udp_pcb::recv, udp_pcb::recv_arg, udp_pcb::remote_port, snmp_inc_udpindatagrams, snmp_inc_udpinerrors, snmp_inc_udpnoports, SOF_BROADCAST, SOF_REUSEADDR, pbuf::tot_len, U16_F, UDP_DEBUG, udp_debug_print, UDP_FLAGS_CONNECTED, UDP_HLEN, udp_pcbs, and UDP_STATS_INC.
Referenced by ip_input().
Create a UDP PCB.
References memp_malloc(), NULL, and UDP_TTL.
Referenced by dhcp_inform(), dhcp_start(), and pcb_new().
void udp_recv | ( | struct udp_pcb * | pcb, |
udp_recv_fn | recv, | ||
void * | recv_arg | ||
) |
Set a receive callback for a UDP PCB.
This callback will be called when receiving a datagram for the pcb.
pcb | the pcb for wich to set the recv callback |
recv | function pointer of the callback function |
recv_arg | additional argument to pass to the callback function |
References udp_pcb::recv, recv, and udp_pcb::recv_arg.
Referenced by dhcp_start(), and pcb_new().
Remove an UDP PCB.
pcb | UDP PCB to be removed. The PCB is removed from the list of UDP PCB's and the data structure is freed from memory. |
References memp_free(), udp_pcb::next, NULL, and snmp_delete_udpidx_tree.
Referenced by dhcp_inform(), dhcp_start(), dhcp_stop(), and do_delconn().
Send data using UDP.
pcb | UDP PCB used to send the data. |
p | chain of pbuf's to be sent. |
The datagram will be sent to the current remote_ip & remote_port stored in pcb. If the pcb is not bound to a port, it will automatically be bound to a random port.
References udp_pcb::remote_port, and udp_sendto().
Referenced by do_send().
Send data to a specified address using UDP.
pcb | UDP PCB used to send the data. |
p | chain of pbuf's to be sent. |
dst_ip | Destination IP address. |
dst_port | Destination UDP port. |
dst_ip & dst_port are expected to be in the same byte order as in the pcb.
If the PCB already has a remote address association, it will be restored after the data is sent.
Referenced by do_send(), lwip_sendto(), and udp_send().
err_t udp_sendto_if | ( | struct udp_pcb * | pcb, |
struct pbuf * | p, | ||
ip_addr_t * | dst_ip, | ||
u16_t | dst_port, | ||
struct netif * | netif | ||
) |
Send data to a specified address using UDP.
The netif used for sending can be specified.
This function exists mainly for DHCP, to be able to send UDP packets on a netif that is still down.
pcb | UDP PCB used to send the data. |
p | chain of pbuf's to be sent. |
dst_ip | Destination IP address. |
dst_port | Destination UDP port. |
netif | the netif used for sending. |
dst_ip & dst_port are expected to be in the same byte order as in the pcb.
Referenced by dhcp_decline(), dhcp_discover(), dhcp_inform(), dhcp_rebind(), dhcp_reboot(), dhcp_release(), dhcp_renew(), and dhcp_select().
struct udp_pcb* udp_pcbs |
Referenced by udp_bind(), udp_connect(), and udp_input().