Pulse Width Modulation (PWM) Software Driver for modules below revision v4.0.0.
This driver provides an API to get access to the main features of the PWM controller.
Data Structures | |
struct | pwm_opt_t |
Input parameters when initializing a PWM channel. More... | |
Macros | |
#define | PWM_FAILURE -1 |
Value returned by function when it was unable to complete successfully for some unspecified reason. More... | |
#define | PWM_INVALID_ARGUMENT 1 |
Value returned by function when the channel number is invalid. More... | |
#define | PWM_INVALID_INPUT 1 |
Value returned by function when the input parameters are out of range. More... | |
#define | PWM_MODE_CENTER_ALIGNED 1 |
Operate PWM channel in center aligned mode. More... | |
#define | PWM_MODE_LEFT_ALIGNED 0 |
Operate PWM channel in left aligned mode. More... | |
#define | PWM_POLARITY_HIGH 1 |
PWM channel starts output high level. More... | |
#define | PWM_POLARITY_LOW 0 |
PWM channel starts output low level. More... | |
#define | PWM_SUCCESS 0 |
Value returned by function when it completed successfully. More... | |
#define | PWM_UPDATE_DUTY 0 |
PWM channel write in CUPDx updates duty cycle at the next period start event. More... | |
#define | PWM_UPDATE_PERIOD 1 |
PWM channel write in CUPDx updates period at the next period start event. More... | |
Functions | |
int | pwm_async_update_channel (unsigned int channel_id, const avr32_pwm_channel_t *pwm_channel) |
Update channel register CPRDx or CDTYx without synchronizing with the PWM period. This function uses the CUPDx register as a double buffer for the period or the duty cycle. Only the first 20 bits of cupd are significant. More... | |
int | pwm_channel_init (unsigned int channel_id, const avr32_pwm_channel_t *pwm_channel) |
Initialize a specific PWM channel. More... | |
int | pwm_init (const pwm_opt_t *opt) |
This function initialize the PWM controller (mode register) and disable the interrupt. More... | |
int | pwm_start_channels (unsigned long channels_bitmask) |
Start PWM channels. More... | |
int | pwm_stop_channels (unsigned long channels_bitmask) |
Stop PWM channels. More... | |
int | pwm_sync_update_channel (unsigned int channel_id, const avr32_pwm_channel_t *pwm_channel) |
Update channel register CPRDx or CDTYx by forcing synchronization with the PWM period. This function uses the CUPDx register as a double buffer for the period or the duty cycle. Only the first 20 bits of cupd are significant. More... | |
#define PWM_FAILURE -1 |
Value returned by function when it was unable to complete successfully for some unspecified reason.
#define PWM_INVALID_ARGUMENT 1 |
Value returned by function when the channel number is invalid.
Referenced by pwm_channel_init().
#define PWM_INVALID_INPUT 1 |
Value returned by function when the input parameters are out of range.
Referenced by pwm_async_update_channel(), pwm_channel_init(), pwm_init(), pwm_start_channels(), pwm_stop_channels(), and pwm_sync_update_channel().
#define PWM_MODE_CENTER_ALIGNED 1 |
Operate PWM channel in center aligned mode.
#define PWM_MODE_LEFT_ALIGNED 0 |
Operate PWM channel in left aligned mode.
Referenced by tft_bl_init(), and ui_pwm_led_init().
#define PWM_POLARITY_HIGH 1 |
PWM channel starts output high level.
Referenced by tft_bl_init().
#define PWM_POLARITY_LOW 0 |
PWM channel starts output low level.
Referenced by ui_pwm_led_init().
#define PWM_SUCCESS 0 |
Value returned by function when it completed successfully.
Referenced by pwm_async_update_channel(), pwm_channel_init(), pwm_init(), pwm_start_channels(), pwm_stop_channels(), and pwm_sync_update_channel().
#define PWM_UPDATE_DUTY 0 |
PWM channel write in CUPDx updates duty cycle at the next period start event.
Referenced by tft_bl_init(), ui_pwm_led_init(), and ui_pwm_update().
#define PWM_UPDATE_PERIOD 1 |
PWM channel write in CUPDx updates period at the next period start event.
int pwm_async_update_channel | ( | unsigned int | channel_id, |
const avr32_pwm_channel_t * | pwm_channel | ||
) |
Update channel register CPRDx or CDTYx without synchronizing with the PWM period. This function uses the CUPDx register as a double buffer for the period or the duty cycle. Only the first 20 bits of cupd are significant.
channel_id | The channel identifier (0 to max channel-1) |
*pwm_channel | Pointer to PWM channel struct avr32_pwm_channel_t |
References PWM_INVALID_INPUT, and PWM_SUCCESS.
int pwm_channel_init | ( | unsigned int | channel_id, |
const avr32_pwm_channel_t * | pwm_channel | ||
) |
Initialize a specific PWM channel.
channel_id | The channel identifier mask |
*pwm_channel | Pointer to PWM channel struct avr32_pwm_channel_t |
References PWM_INVALID_ARGUMENT, PWM_INVALID_INPUT, and PWM_SUCCESS.
Referenced by tft_bl_init(), and ui_pwm_led_init().
int pwm_init | ( | const pwm_opt_t * | opt | ) |
This function initialize the PWM controller (mode register) and disable the interrupt.
opt | PWM Channel structure parameter |
References Disable_global_interrupt, pwm_opt_t::diva, pwm_opt_t::divb, Enable_global_interrupt, Is_global_interrupt_enabled, pwm_opt_t::prea, pwm_opt_t::preb, PWM_INVALID_INPUT, and PWM_SUCCESS.
Referenced by ui_pwm_init().
int pwm_start_channels | ( | unsigned long | channels_bitmask | ) |
Start PWM channels.
channels_bitmask | A bit-mask with set bits indicating channels to start. |
References PWM_INVALID_INPUT, and PWM_SUCCESS.
Referenced by tft_bl_init(), and ui_pwm_led_init().
int pwm_stop_channels | ( | unsigned long | channels_bitmask | ) |
Stop PWM channels.
channels_bitmask | A bit-mask with set bits indicating channels to stop. |
References PWM_INVALID_INPUT, and PWM_SUCCESS.
int pwm_sync_update_channel | ( | unsigned int | channel_id, |
const avr32_pwm_channel_t * | pwm_channel | ||
) |
Update channel register CPRDx or CDTYx by forcing synchronization with the PWM period. This function uses the CUPDx register as a double buffer for the period or the duty cycle. Only the first 20 bits of cupd are significant.
channel_id | The channel identifier (0 to max channel-1) |
*pwm_channel | Pointer to PWM channel struct avr32_pwm_channel_t |
References PWM_INVALID_INPUT, and PWM_SUCCESS.
Referenced by ui_pwm_update().