Android Open Accessory.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include "conf_usb_host.h"
#include "usb_protocol_aoa.h"
#include "uhd.h"
#include "uhc.h"
#include "uhi_aoa.h"
#include <string.h>
Data Structures | |
struct | uhi_aoa_dev_t |
Stores relevant information about the USB connection. More... | |
Macros | |
#define | AOA_V2_SUPPORT 0 |
Stages of enabling the Android Device | |
#define | AOA_ENABLE_STAGE_PROCESSING 0 |
#define | AOA_ENABLE_STAGE_SUCCESSFUL 1 |
#define | AOA_ENABLE_STAGE_FAILED 2 |
Functions | |
Functions required by UHC | |
uhc_enum_status_t | uhi_aoa_install (uhc_device_t *dev) |
Functions required by UHC. More... | |
void | uhi_aoa_enable (uhc_device_t *dev) |
void | uhi_aoa_uninstall (uhc_device_t *dev) |
Routines to initialize the Android device | |
void | uhi_aoa_send_info_string (uint8_t, char *, uhd_callback_setup_end_t) |
Function to send Identifying Information to the Android Device. More... | |
Routines to communicate with the Android device | |
bool | uhi_aoa_read (uint8_t *payload, uint16_t payload_size, uhd_callback_trans_t callback_end) |
Main Function to receive a message from an Android device. More... | |
bool | uhi_aoa_write (uint8_t *payload, uint16_t payload_size, uhd_callback_trans_t callback_end) |
Main Function to send a message to an Android device. More... | |
bool | uhi_aoa_register_hid (uint16_t id, uint8_t *hid_rpt_desc, uint16_t hid_rpt_desc_len) |
Register a HID device. More... | |
bool | uhi_aoa_unregister_hid (uint16_t id) |
Unregister a HID device. More... | |
bool | uhi_aoa_send_hid_event (uint16_t id, void *hid_rpt, uint16_t rpt_size) |
Send HID events. More... | |
Variables | |
volatile uint8_t | uhi_aoa_enable_stage |
Stores the status of the process enabling the Accessory device. More... | |
volatile uint16_t | uhi_aoa_protocol |
Stores the "Android Open Accessory Protocol" version. More... | |
Internal Defines and Variables to store information about the Accessory | |
#define | uhi_aoa_dev_sel (&uhi_aoa_dev) |
Current USB device AOA selected by the UHI AOA. More... | |
static struct uhi_aoa_dev_t | uhi_aoa_dev |
void | uhi_aoa_mode_enable_step1 (uhc_device_t *) |
Function to enable the Accessory Mode on Android Devices. More... | |
void | uhi_aoa_mode_enable_step2 (usb_add_t, uhd_trans_status_t, uint16_t) |
Function to enable the Accessory Mode on Android Devices. More... | |
void | uhi_aoa_mode_enable_step3 (usb_add_t, uhd_trans_status_t, uint16_t) |
Function to enable the Accessory Mode on Android Devices. More... | |
void | uhi_aoa_mode_enable_complete (usb_add_t, uhd_trans_status_t, uint16_t) |
Function to enable the Accessory Mode on Android Devices. More... | |
static void | uhi_aoa_enable_success (void) |
Function to end AoA enabling success. More... | |
#define AOA_V2_SUPPORT 0 |
Referenced by uhi_aoa_install().