#include "stack_config.h"
#include "rf4ce.h"
#include "zrc.h"
Macros | |
#define | APP_CAPABILITIES (0x01 | (NUM_SUPPORTED_DEV_TYPES << 1) | (NUM_SUPPORTED_PROFILES << 4)) |
#define | APP_FIRST_TIMER_ID (0) |
This is the first timer identifier of the application. More... | |
#define | APP_LAST_TIMER_ID (LAST_STACK_TIMER_ID + NUMBER_OF_APP_TIMERS) |
Defines the largest timer identifier used by the application. More... | |
#define | APP_USER_STRING "Single Btn Ctrl" /* 15 characters ! */ |
#define | AVR477_ACTIVE_DURATION_SEC 10 /* in Seconds */ |
#define | AVR477_SLEEP_DURATION_SEC 10 /* In Seconds */ |
#define | AVR477_WARM_RESET_WAIT_TIME_SEC 10 /* in Seconds */ |
#define | EE_QDEBUG_OFFSET (EE_IEEE_ADDR + 0xC8) |
#define | FW_VERSION_MAJOR 1 |
#define | FW_VERSION_MINOR 3 |
#define | FW_VERSION_REV 0 |
#define | NUM_SUPPORTED_DEV_TYPES (1) |
#define | NUM_SUPPORTED_PROFILES (1) |
#define | NUMBER_OF_APP_TIMERS (1) |
Defines the number of timers used by the application. More... | |
#define | NWKC_NODE_CAPABILITIES |
#define | NWKC_VENDOR_IDENTIFIER (0x1014) |
#define | NWKC_VENDOR_STRING "ATMEL " /* 7 characters ! */ |
#define | QT_DELTA_LENGTH 0x2D |
#define | QT_REFERENCES_LENGTH 0x45 |
#define | QT_SIGNAL_LENGTH 0x45 |
#define | QT_START_DELTA_DATA 0x11 |
#define | QT_START_REF_DATA 0x1D |
#define | QT_STATE_LENGTH 0x0F |
#define | SUPPORTED_CEC_CMDS |
#define | TOTAL_NUMBER_OF_TIMERS (NUMBER_OF_APP_TIMERS + NUMBER_OF_TOTAL_STACK_TIMERS) |
Defines the total number of timers used by the application and the layers below. More... | |
#define | TX_OPTIONS |
#define | USED_QT_CHANNELS 0xF1F0F |
#define | USER_STRING_AVAILABLE true |
#define | WDT_TIMEOUT_PERIOD WDT_TO_8S |
Enumerations | |
enum | app_timer_t { T_LED_TIMER = (APP_FIRST_TIMER_ID), T_LED_TIMER = (APP_FIRST_TIMER_ID) } |
Timer ID's used by the Application. More... | |
#define APP_CAPABILITIES (0x01 | (NUM_SUPPORTED_DEV_TYPES << 1) | (NUM_SUPPORTED_PROFILES << 4)) |
#define APP_FIRST_TIMER_ID (0) |
This is the first timer identifier of the application.
The value of this identifier is an increment of the largest identifier value used by the MAC.
#define APP_LAST_TIMER_ID (LAST_STACK_TIMER_ID + NUMBER_OF_APP_TIMERS) |
Defines the largest timer identifier used by the application.
#define APP_USER_STRING "Single Btn Ctrl" /* 15 characters ! */ |
#define AVR477_ACTIVE_DURATION_SEC 10 /* in Seconds */ |
#define AVR477_SLEEP_DURATION_SEC 10 /* In Seconds */ |
#define AVR477_WARM_RESET_WAIT_TIME_SEC 10 /* in Seconds */ |
#define EE_QDEBUG_OFFSET (EE_IEEE_ADDR + 0xC8) |
Referenced by QDebug_SetSubscriptions(), and start_warm_reset_cb().
#define FW_VERSION_MAJOR 1 |
#define FW_VERSION_MINOR 3 |
#define FW_VERSION_REV 0 |
#define NUM_SUPPORTED_DEV_TYPES (1) |
#define NUM_SUPPORTED_PROFILES (1) |
#define NUMBER_OF_APP_TIMERS (1) |
Defines the number of timers used by the application.
#define NWKC_NODE_CAPABILITIES |
#define NWKC_VENDOR_IDENTIFIER (0x1014) |
#define NWKC_VENDOR_STRING "ATMEL " /* 7 characters ! */ |
#define QT_DELTA_LENGTH 0x2D |
#define QT_REFERENCES_LENGTH 0x45 |
#define QT_SIGNAL_LENGTH 0x45 |
#define QT_START_DELTA_DATA 0x11 |
#define QT_START_REF_DATA 0x1D |
#define QT_STATE_LENGTH 0x0F |
#define SUPPORTED_CEC_CMDS |
#define TOTAL_NUMBER_OF_TIMERS (NUMBER_OF_APP_TIMERS + NUMBER_OF_TOTAL_STACK_TIMERS) |
Defines the total number of timers used by the application and the layers below.
#define TX_OPTIONS |
#define USED_QT_CHANNELS 0xF1F0F |
#define USER_STRING_AVAILABLE true |
#define WDT_TIMEOUT_PERIOD WDT_TO_8S |
enum app_timer_t |