FreeRTOS Web/DSP Demo.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <FreeRTOS.h>
#include <StackMacros.h>
#include <croutine.h>
#include <list.h>
#include <mpu_wrappers.h>
#include <portable.h>
#include <projdefs.h>
#include <queue.h>
#include <semphr.h>
#include <task.h>
#include <timers.h>
#include <pmc.h>
#include <sysclk.h>
Macros | |
#define | SLIDER_SELECTOR_NB (9UL) |
#define | SLIDER_SELECTOR_RANGE (255UL / SLIDER_SELECTOR_NB) |
#define | WAIT_FOR_TOUCH_EVENT {while (app_hold) vTaskDelay(instructions_delay);} |
Wait for user to touch screen. More... | |
Functions | |
void | create_dsp_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority) |
Create the DSP task. More... | |
void | create_gfx_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority) |
Create the GFX task. More... | |
void | create_qtouch_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority) |
Create the QTouch task. More... | |
void | create_webserver_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority) |
Create the Webserver task. More... | |
Variables | |
uint32_t | app_hold |
Used to block the application on instruction screen. More... | |
const portTickType | instructions_delay |
Small delay to hold tasks, during instruction screen. More... | |
#define SLIDER_SELECTOR_NB (9UL) |
Referenced by demo_process_qt_status(), and dsp_sin_init().
#define SLIDER_SELECTOR_RANGE (255UL / SLIDER_SELECTOR_NB) |
Referenced by demo_process_qt_status().
#define WAIT_FOR_TOUCH_EVENT {while (app_hold) vTaskDelay(instructions_delay);} |
Wait for user to touch screen.
Referenced by dsp_task(), qtouch_task(), and webserver_task().
void create_dsp_task | ( | uint16_t | stack_depth_words, |
unsigned portBASE_TYPE | task_priority | ||
) |
Create the DSP task.
stack_depth_words | Task stack size in 32 bits word. |
task_priority | Task priority. |
References dsp_task(), NULL, vSemaphoreCreateBinary, xSemaphoreTake, and xTaskCreate.
Referenced by main().
void create_gfx_task | ( | uint16_t | stack_depth_words, |
unsigned portBASE_TYPE | task_priority | ||
) |
Create the GFX task.
stack_depth_words | Task stack size in 32 bits word. |
task_priority | Task priority. |
Initialize display.
Create the task as described above.
References gfx_init(), gfx_task(), NULL, and xTaskCreate.
Referenced by main().
void create_qtouch_task | ( | uint16_t | stack_depth_words, |
unsigned portBASE_TYPE | task_priority | ||
) |
Create the QTouch task.
stack_depth_words | Task stack size in 32 bits word. |
task_priority | Task priority. |
Initialize communication interface
Reset QT device
Check communication is ready and able to read Chip ID
Infinite loop here
Read setup block
Modify setup block parameters for specific example
Write setup block
Create the task as described above.
References demo_set_qt_param(), init_interface(), NULL, qt_get_comm_ready(), qt_hardware_reset(), qt_read_setup_block(), qt_write_setup_block(), qtouch_task(), setup_block, STATUS_OK, and xTaskCreate.
Referenced by main().
void create_webserver_task | ( | uint16_t | stack_depth_words, |
unsigned portBASE_TYPE | task_priority | ||
) |
Create the Webserver task.
stack_depth_words | Task stack size in 32 bits word. |
task_priority | Task priority. |
Create the task as described above.
References NULL, webserver_task(), and xTaskCreate.
Referenced by main().
uint32_t app_hold |
Used to block the application on instruction screen.
Used to block the application on instruction screen.
Referenced by gfx_task().
const portTickType instructions_delay |
Small delay to hold tasks, during instruction screen.