Microchip® Advanced Software Framework

task_qtouch_cpn.c File Reference

QTouch component task for the FreeRTOS Web/DSP Demo.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include "task_demo.h"
#include "arm_math.h"
#include "qt_i2c.h"
#include "conf_qt_i2c.h"

Macros

#define QT_SLIDER_MAX   ((0x01 << (8 - QT_SLIDER_RESOLUTION)) - 1)
 
#define QT_SLIDER_RESOLUTION   QT_SLIDER_RESOLUTION_8_BIT
 

Functions

void create_qtouch_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority)
 Create the QTouch task. More...
 
static void demo_process_qt_status (struct qt_status *qt_status)
 Process Qtouch status. More...
 
static void demo_set_qt_param (struct qt_setup_block *psetup_block)
 Set QTouch parameter for the demo. More...
 
static void init_interface (void)
 Initialize TWI communication interface. More...
 
static void qtouch_task (void *pvParameters)
 QTouch task core function. More...
 

Variables

uint32_t g_ip_mode
 IP mode: 0 unselected, 1 static, 2 dhcp. More...
 
const portTickType qtouch_delay = 200UL / portTICK_RATE_MS
 
struct qt_status qtstatus
 Storage for QT status. More...
 
struct qt_setup_block setup_block
 Storage for QT setup block. More...
 
uint8_t slider_pos = 0
 Slider position. More...
 

#define QT_SLIDER_MAX   ((0x01 << (8 - QT_SLIDER_RESOLUTION)) - 1)
#define QT_SLIDER_RESOLUTION   QT_SLIDER_RESOLUTION_8_BIT

Referenced by demo_set_qt_param().

void create_qtouch_task ( uint16_t  stack_depth_words,
unsigned portBASE_TYPE  task_priority 
)

Create the QTouch task.

Parameters
stack_depth_wordsTask stack size in 32 bits word.
task_priorityTask priority.

Initialize communication interface

Reset QT device

Check communication is ready and able to read Chip ID

Infinite loop here

Read setup block

Modify setup block parameters for specific example

Write setup block

Create the task as described above.

References demo_set_qt_param(), init_interface(), NULL, qt_get_comm_ready(), qt_hardware_reset(), qt_read_setup_block(), qt_write_setup_block(), qtouch_task(), setup_block, STATUS_OK, and xTaskCreate.

Referenced by main().

static void demo_process_qt_status ( struct qt_status qt_status)
static

Process Qtouch status.

Parameters
qt_statusPointer to Qtouch status struct variable.

Read setup block

Modify setup block parameters for specific example

Write setup block

Save a slider position to be used in the DSP task.

Necessary to avoid sin_buffer overflow, when position equals 0.

References demo_set_qt_param(), qt_status::general_status, QT_GENERAL_STATUS_RESET, QT_GENERAL_STATUS_SDET, qt_read_setup_block(), qt_write_setup_block(), setup_block, slider_pos, qt_status::slider_position, SLIDER_SELECTOR_NB, and SLIDER_SELECTOR_RANGE.

Referenced by qtouch_task().

static void demo_set_qt_param ( struct qt_setup_block psetup_block)
static

Set QTouch parameter for the demo.

Parameters
setup_blockPointer to setup block buffer.

References qt_setup_block::gpio_direction, qt_setup_block::gpio_gpo_drive2, QT_SLIDER_RESOLUTION, qt_setup_block::slider_num_keys, and qt_setup_block::slider_resolution.

Referenced by create_qtouch_task(), and demo_process_qt_status().

static void init_interface ( void  )
static

Initialize TWI communication interface.

TWI master initialization options.

100KHz for I2C speed

Initialize the TWI master driver.

References BOARD_QT_TWI_INSTANCE, twi_options::speed, and twi_master_setup().

Referenced by create_qtouch_task().

static void qtouch_task ( void pvParameters)
static

QTouch task core function.

Parameters
pvParametersJunk parameter.

Wait for user to read instructions.

QTouch task Loop.

Read all status bytes

Process the received data

References demo_process_qt_status(), g_ip_mode, qt_get_status(), qt_is_change_line_low(), qtouch_delay, qtstatus, UNUSED, vTaskDelay(), and WAIT_FOR_TOUCH_EVENT.

Referenced by create_qtouch_task().

uint32_t g_ip_mode

IP mode: 0 unselected, 1 static, 2 dhcp.

const portTickType qtouch_delay = 200UL / portTICK_RATE_MS

Referenced by qtouch_task().

struct qt_status qtstatus

Storage for QT status.

Referenced by qtouch_task().

struct qt_setup_block setup_block

Storage for QT setup block.

Referenced by create_qtouch_task(), and demo_process_qt_status().

uint8_t slider_pos = 0

Slider position.

Slider position, used as sin_buffer table index.

Referenced by demo_process_qt_status(), and dsp_task().