Microchip® Advanced Software Framework

cdc/device/example/main.h File Reference

Main functions.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

#include "usb_protocol_cdc.h"

Functions

void main_cdc_disable (uint8_t port)
 Closes the communication port This is called by CDC interface when USB Host disable it. More...
 
bool main_cdc_enable (uint8_t port)
 Opens the communication port This is called by CDC interface when USB Host enable it. More...
 
void main_cdc_set_dtr (uint8_t port, bool b_enable)
 Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port. More...
 
void main_resume_action (void)
 Turn on a led to notify active mode Called when the USB line is resumed from the suspend state. More...
 
void main_sof_action (void)
 Manages the leds behaviors Called when a start of frame is received on USB line each 1ms. More...
 
void main_suspend_action (void)
 Enters the application in low power mode Callback called when USB host sets USB line in suspend state. More...
 

void main_cdc_disable ( uint8_t  port)

Closes the communication port This is called by CDC interface when USB Host disable it.

References main_b_cdc_enable, and uart_close().

bool main_cdc_enable ( uint8_t  port)

Opens the communication port This is called by CDC interface when USB Host enable it.

Return values
trueif cdc startup is successfully done

Called by CDC interface Callback running when USB Host enable CDC interface.

Return values
trueif cdc startup is successfully done

References main_b_cdc_enable, and uart_open().

void main_cdc_set_dtr ( uint8_t  port,
bool  b_enable 
)

Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port.

References ui_com_close(), and ui_com_open().

void main_resume_action ( void  )

Turn on a led to notify active mode Called when the USB line is resumed from the suspend state.

Called by UDD when the USB line exit of suspend state.

void main_sof_action ( void  )

Manages the leds behaviors Called when a start of frame is received on USB line each 1ms.

Called when a start of frame is received on USB line.

void main_suspend_action ( void  )

Enters the application in low power mode Callback called when USB host sets USB line in suspend state.

Turn off all leds Callback running when USB Host set USB line in suspend state.

Called by UDD when a suspend is received Callback running when USB Host set USB line in suspend state.