_IPheader | IP Header structure |
 _slave_device_t | The slave device instance |
 A_BLOCK_LINK | |
 acc_t | |
 arp_header | ARP header structure |
 at25_cmd | SerialFlash transfers request prepared by the AT25 driver |
 block_status | |
 BLOCKING_QUEUE_PARAMETERS | |
 can_bit_timing_t | |
 can_mb_conf_t | Define the struct for CAN message mailbox |
 chipid_data | Definition for chip id register data struct |
 chipidtype | Chip ID catalog information: Type ID and its description stream |
 clock_opt_t | Clock mode structure |
 corCoRoutineControlBlock | |
 COUNT_SEM_STRUCT | |
 data_frame_opt_t | Data frame structure |
 DIR | |
 dma_transfer_descriptor_t | DMA transfer descriptor structure, otherwise known as a Linked List Item (LLI) |
 emac_dev_mem | EMAC device memory management struct |
 emac_device | EMAC driver structure |
 emac_options | Input parameters when initializing the emac module mode |
 emac_rx_descriptor | Receive buffer descriptor struct |
  emac_rx_addr | |
   emac_rx_addr_bm | |
  emac_rx_status | |
   emac_rx_status_bm | |
 emac_tx_descriptor | Transmit buffer descriptor struct |
  emac_tx_status | |
   emac_tx_status_bm | |
 eth_packet | Ethernet packet structure |
 ethernet_header | Ethernet header structure |
 ethernetif | Helper struct to hold private data used to operate your ethernet interface |
 FATFS | |
 fifo_desc | FIFO descriptor used by FIFO driver |
 FIL | |
 FILINFO | |
 font | Storage structure for font meta data |
 freertos_dma_tx_control | |
 freertos_pdc_rx_control | |
 freertos_peripheral_options | Define the behaviour of FreeRTOS ASF read and write functions for a peripheral |
 freertos_peripheral_parameters | |
 fs_file | |
 fsdata_file | |
 fsdata_file_noconst | |
 genclk_config | Hardware representation of a set of generic clock parameters |
 gfx_bitmap | Storage structure for bitmap pixel data and metadata |
 HeapRegion | |
 http_state | |
 hx8347a_opt_t | Input parameters when initializing HX8347A driver |
 icmp6_echo_hdr | This is the ICMP6 header adapted for echo req/resp |
 icmp6_hdr | This is the standard ICMP6 header |
 icmp_echo_hdr | This is the standard ICMP header only that the u32_t data is split to two u16_t like ICMP echo needs it |
 icmp_echo_header | ICMP echo header structure |
 ili9225_font | Font structure |
 ili9225_opt_t | Input parameters when initializing ili9225 driver |
 ili9325_font | Font structure |
 ili9325_opt_t | Input parameters when initializing ili9325 driver |
 ili93xx_font | Font structure |
 ili93xx_opt_t | Input parameters when initializing ili9325 driver |
 in_addr | For compatibility with BSD code |
 ip_addr | |
 ip_addr2 | |
 ip_addr_packed | |
 ip_globals | |
 ip_hdr | |
 ip_pcb | |
 main_conf_desc_t | USB HID mouse configuration descriptor struct |
 mem | The heap is made up as a list of structs of this type |
 membag | Internal structure used by membag to keep track of memory, with maximum 32 blocks per membag |
 memp | |
 mxt_conf_messageprocessor_t5 | Object message |
 mxt_device | MaXTouch device information data container struct |
 mxt_gen_commandprocessor_t6 | Commandprocessor T6 object |
 mxt_info_object | Identification header |
 mxt_object | Object table entry |
 mxt_report_id_map | Map of the report ID vs object type and instance |
 mxt_touch_event | Touch event struct |
 nand_flash_ecc | NAND Flash ECC layer is called by upper layer, it will call the raw layer to do write/read operations, and do ECC check to the write/read result, it then will feedback the ECC check result to the upper layer |
 nand_flash_management | |
 nand_flash_map | |
 nand_flash_model | |
 nand_flash_raw | The raw NAND Flash layer drives hardware-specific Bus Read and Bus Write operations to communicate with the NAND Flash device |
 nand_flash_spare_scheme | |
 nand_flash_translation | |
 netbuf | |
 netif | Generic data structure used for all lwIP network interfaces |
 pbuf | |
 pdc_packet | PDC data packet for transfer |
 pll_config | Hardware-specific representation of PLL configuration |
 pwm_channel_t | Input parameters when configuring a PWM channel mode |
 pwm_clock_t | Input parameters when initializing PWM |
 qt_lib_sig_info_t | This will be used to get the library information from the library |
 qt_setup_block | Definitions for AT42QT2160 setup block |
 qt_status | Structure for QT2160 device-status, include: |
 QueueDefinition | |
 rtouch_calibration_point_struct | Storage structure for calibration point (actual and raw positions) |
 rtouch_calibration_points_struct | Collection of the five calibration points required to compute calibration |
 rtouch_event_struct | User touch event structure |
 rtouch_point_struct | Point definition |
 sam_uart_opt | Option list for UART peripheral initialization |
 sam_uotghs_dmach_t | Structure for DMA registers in a channel |
 sam_uotghs_dmadesc_t | Structure for DMA descriptor |
 sam_uotghs_uhdmach_t | Structure for DMA registers in a channel |
 sam_uotghs_uhdmadesc_t | Structure for DMA descriptor |
 sam_usart_opt_t | Micro definition for LIN mode of SAMV71 |
 sbc_caching_mode_page | SBC-2 Caching mode page |
 sbc_rdwr_error_recovery_mode_page | SBC-2 Read-Write Error Recovery mode page |
 sbc_read_capacity10_data | SBC-2 READ CAPACITY (10) parameter data |
 sbc_slba_block_desc | SBC-2 Short LBA mode parameter block descriptor |
 scsi_inquiry_data | SCSI Standard Inquiry data structure |
 scsi_mode_page_0_header | SCSI Page_0 Mode Page header (SPF not set) |
 scsi_mode_param_header10 | SCSI Mode Parameter Header used by MODE SELECT(10) and MODE SENSE(10) |
 scsi_mode_param_header6 | SCSI Mode Parameter Header used by MODE SELECT(6) and MODE SENSE(6) |
 scsi_request_sense_data | SCSI Standard Request sense data structure |
 sd_mmc_card | SD/MMC card information structure |
 sdramc_memory_dev | |
  sdramc_cr | |
   sdramc_cr_bm | |
 SEMAPHORE_PARAMETERS | |
 servent | |
 sn65hvd234_ctrl_t | |
 spc_control_page_info_execpt | SPC-2 Informational exceptions control page See chapter 8.3.8 |
 spi_device | Polled SPI device definition |
 sswt_cb | Struct used for sys_sem_wait_timeout() to tell wether the time has run out or the semaphore has really become available |
 st_lin_message | This structure allows to handle a LIN message and, at the end of the received/transmitted message, allows to call a function associated to this message, the update or the capture of "signals" |
 status_block_t | |
 StructCPtr | Structure of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 StructCVPtr | Structure of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 StructPtr | Structure of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 StructVPtr | Structure of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 sys_timeo | |
 sys_timeouts | |
 tag_qt_touch_lib_config_data_t | Post processing configuration data that is received from the debug interface |
 tag_qt_touch_lib_measure_data_t | Measured touch data that is sent for the debugging and fine tunning |
 tag_qt_touch_status_t | The state of the library sensors |
 tag_sensor_t | |
 tcpip_msg | |
 test_case | A test case |
 test_suite | A test suite |
 tftphdr | |
 TimeoutlistPerThread | |
 timers_info | |
 tskTaskControlBlock | |
 twi_module | |
 twi_options | Input parameters when initializing the TWI module mode |
 twi_packet | Information concerning the data transmission |
 uart_rs232_options | Input parameters when initializing RS232 and similar modes |
 udc_config_speed_t | Configuration descriptor and UDI link for one USB speed |
 udc_config_t | All information about the USB Device |
 udc_desc_t | Structure for USB Device Configuration Descriptor |
 udc_string_desc_t | USB device string descriptor Structure used to transfer ASCII strings to USB String descriptor structure |
 udd_ctrl_request_t | Global variable to give and record information of the setup request management |
 udi_api_t | UDI API |
 udi_cdc_comm_desc_t | Communication Class interface descriptor |
 udi_cdc_data_desc_t | Data Class interface descriptor |
 udi_hid_generic_desc_t | Interface descriptor structure for HID generic |
 udi_hid_generic_report_desc_t | Report descriptor for HID generic |
 udi_hid_kbd_desc_t | Interface descriptor structure for HID keyboard |
 udi_hid_kbd_report_desc_t | Report descriptor for HID keyboard |
 udi_hid_mouse_desc_t | Interface descriptor structure for HID mouse |
 udi_hid_mouse_report_desc_t | Report descriptor for HID mouse |
 udi_hid_multi_touch_desc_t | Interface descriptor structure for HID multi-touch |
 udi_hid_multi_touch_report_desc_t | Report descriptor for HID multi-touch |
 udi_msc_desc_t | Interface descriptor structure for MSC |
 udi_phdc_desc_t | |
 udi_phdc_fnctext_desc_t | |
 udi_phdc_metadata_t | |
 udi_vendor_desc_t | Interface descriptor structure for vendor Class interface |
 uhc_device_t | Structure to store device information |
 uhd_ctrl_request_t | Structure to store the high level setup request |
 uhd_pipe_job_t | Structure definition to store registered jobs on a pipe |
 uhi_aoa_dev_t | Stores relevant information about the USB connection |
 uhi_api_t | UHI API |
 uhi_cdc_buf_t | Internal buffer information |
 uhi_cdc_dev_t | USB CDC device information |
 uhi_cdc_line_t | Communication line information |
 uhi_cdc_port_t | Communication port information |
 uhi_hid_mouse_dev_t | |
 uhi_msc_dev_t | USB MSC device information |
 uhi_msc_lun_t | LUN structure information |
 uhi_vendor_dev_t | |
 Union16 | 16-bit union |
 Union32 | 32-bit union |
 Union64 | 64-bit union |
 UnionCPtr | Union of pointers to constant 64-, 32-, 16- and 8-bit unsigned integers |
 UnionCVPtr | Union of pointers to constant volatile 64-, 32-, 16- and 8-bit unsigned integers |
 UnionPtr | Union of pointers to 64-, 32-, 16- and 8-bit unsigned integers |
 UnionVPtr | Union of pointers to volatile 64-, 32-, 16- and 8-bit unsigned integers |
 uotghs_dma_control_t | Structure for DMA control register |
 uotghs_dma_nextdesc_t | Access points to the UOTGHS device DMA memory map with arrayed registers |
 uotghs_dma_status_t | Structure for DMA status register |
 uotghs_uhdma_control_t | Structure for DMA control register |
 uotghs_uhdma_nextdesc_t | Access points to the UOTGHS host DMA memory map with arrayed registers |
 uotghs_uhdma_status_t | Structure for DMA status register |
 usart_iso7816_opt_t | |
 usart_spi_device | Polled SPI device definition |
 usart_spi_opt_t | |
 usb_association_desc_t | Standard USB Interface Association Descriptor structure |
 usb_cdc_acm_desc_t | CDC ACM Functional Descriptor |
 usb_cdc_call_mgmt_desc_t | CDC Call Management Functional Descriptor |
 usb_cdc_control_signal_t | Control signal structure |
 usb_cdc_hdr_desc_t | CDC Header Functional Descriptor |
 usb_cdc_line_coding_t | Line Coding structure |
 usb_cdc_notify_msg_t | |
 usb_cdc_notify_serial_state_t | Hardware handshake support (cdc spec 1.1 chapter 6.3.5) |
 usb_cdc_union_desc_t | CDC Union Functional Descriptor |
 usb_conf_desc_t | Standard USB configuration descriptor structure |
 usb_dev_bos_desc_t | USB Device BOS descriptor structure |
 usb_dev_capa_ext_desc_t | USB Device Capabilities - USB 2.0 Extension Descriptor structure |
 usb_dev_desc_t | Standard USB device descriptor structure |
 usb_dev_lpm_desc_t | USB Device LPM Descriptor structure |
 usb_dev_qual_desc_t | Standard USB device qualifier descriptor structure |
 usb_ep_desc_t | Standard USB endpoint descriptor structure |
 usb_hid_descriptor_t | HID Descriptor |
 usb_iad_desc_t | Standard USB association descriptor structure |
 usb_iface_desc_t | Standard USB interface descriptor structure |
 usb_msc_cbw | |
 usb_msc_csw | |
 usb_phdc_classfnct_desc_t | PHDC Class Function Descriptor |
 usb_phdc_fnctext_desc_t | PHDC Function Extension Descriptor Note: The wDevSpecializations fields must follow this struct |
 usb_phdc_fnctext_singlespec_desc_t | PHDC Function Extension Descriptor with single specification |
 usb_phdc_meta_data_1_desc_t | |
 usb_phdc_meta_data_desc_t | PHDC Meta-Data Descriptor Note: The optional meta-data field (0 to 253B) can follow this struct |
 usb_phdc_metadata_msg_1_t | |
 usb_phdc_metadata_msg_t | PHDC Meta-Data Message Note: The optional meta-data field (0 to EPx_size-21) can follow this struct |
 usb_phdc_qos_desc_t | PHDC QoS Descriptor |
 usb_setup_req_t | A USB Device SETUP request |
 usb_str_desc_t | A standard USB string descriptor structure |
 usb_str_lgid_desc_t | |
 wav_header | |
 waveconfig_t | [tc_capture_selection] |
 win_area | Geometric type describing an area on screen |
 win_attributes | Window attribute data |
 win_clip_region | Geometric type describing a clipping region, used when drawing windows |
 win_command_event | Event data for command events, e.g |
 win_event | Event data for all events |
 win_event_queue | Event queue control struct |
 win_keyboard_event | Event data for all keyboard events, e.g |
 win_point | Geometric type describing a point or vector on screen, relative or absolute |
 win_pointer_event | Event data for all pointer events, e.g |
 win_window | Window control data |
 wtk_basic_frame | Basic frame control struct |
 wtk_button | This is the button control struct |
 wtk_check_box | This is the check box control struct |
 wtk_frame | Frame control struct |
 wtk_icon_button | This is the icon button control struct |
 wtk_icon_group | This is the icon button group control struct |
 wtk_label | This is the label control struct |
 wtk_plot | Plot control struct |
 wtk_progress_bar | Progress bar control struct |
 wtk_radio_button | This is the radio button control struct |
 wtk_radio_group | This is the radio button group control struct |
 wtk_slider | Slider control struct |
 xCOMMAND_INPUT_LIST | |
 xCOMMAND_LINE_INPUT | |
 xEventGroupDefinition | |
 xLIST | |
 xLIST_ITEM | |
 xMEMORY_REGION | |
 xMINI_LIST_ITEM | |
 xRTOS_HEAP | |
 xSTATIC_EVENT_GROUP | |
 xSTATIC_LIST | |
 xSTATIC_LIST_ITEM | |
 xSTATIC_MINI_LIST_ITEM | |
 xSTATIC_QUEUE | |
 xSTATIC_STREAM_BUFFER | |
 xSTATIC_TCB | |
 xSTATIC_TIMER | |
 xSTREAM_BUFFER | |
 xTASK_PARAMETERS | |
 xTASK_PARAMTERS | |
 xTASK_STATUS | |
 xTIME_OUT | |
 xyz_g_t | |
 xyz_t | |