Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Modules
Here is a list of all modules:
[detail level 123456]
oApplications and Examples
oUnit Tests
oSAM3A/3N/3S/3U/3X/4E/4N/4S/G Peripheral DMA Controller (PDC) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the the Peripheral Direct Memory Access (DMA) Controller (PDC) module
oBusy-Wait Delay RoutinesThis module provides simple loop-based delay routines for those applications requiring a brief wait during execution
oCommon IOPORT APISee Quick start guide for the common IOPORT service
oTwo Wire-interface(TWI)This is the common API for TWIs
oDisplay - ILI9325 ControllerLow-level driver for the ILI9325 LCD controller
oUSART in SPI (Serial Peripheral Interface) modeThis is the common API for USART in SPI mode
oUSB device descriptors for a single interfaceThe following structures provide the USB device descriptors required for USB Device with a single interface MSC
oSerial Peripheral Interface (SPI)See Quickstart guide for SAM SPI driver
oStandard I/O (stdio)Common standard I/O driver that implements the stdio read and write functions on AVR and SAM devices
oCompiler abstraction layer and code utilitiesCompiler abstraction layer and code utilities for AT91SAM
oPeripheral Parallel Input/Output (PIO) Controller
oFirst-In-First-Out Buffer (FIFO)See Quick start guide for First-In-First-Out Buffer (FIFO)
oUSB device descriptors for a single interfaceThe following structures provide the USB device descriptors required for USB Device with a single interface PHDC
oTRNG - True Random Number GeneratorDriver for the TRNG (True Random Number Generator)
oSerial Peripheral Interface (SPI)This is the common API for SPI interface
oGlobal interrupt managementThis is a driver for global enabling and disabling of interrupts
oImplementation of SD/MMC/SDIO Stack
oSD/MMC/SDIO common stackSD/MMC/SDIO basic APIs used by SD/MMC/SDIO memory APIs (sd_mmc_stack_mem_group)
oPower Management Controller (PMC)
oPower Manager (PM)This is a stub on the SAM Power Manager Control (PMC) for the sleepmgr service
oHigh Speed MultiMedia Card Interface (HSMCI)This driver interfaces the HSMCI module
oSleep managerThe sleep manager is a service for ensuring that the device is not put to sleep in deeper sleep modes than the system (e.g., peripheral drivers, services or the application) allows at any given time
oEEPROM AT24Cxx SeriesLow-level driver for the AT24CXX Series EEPROM controller
oSynchronous Serial Controller (SSC)The Synchronous Serial Controller (SSC) provides a synchronous communication link with external devices
oUSB device descriptors for a single interfaceThe following structures provide the USB device descriptors required for USB Device with a single interface Vendor Class
oUniversal Asynchronous Receiver Transceiver (UART)The Universal Asynchronous Receiver Transmitter features a two-pin UART that can be used for communication and trace purposes and offers an ideal medium for in-situ programming solutions
oSerial Interface (Serial)See Quick start guide for Serial Interface service
oAtmel part identification macrosThis collection of macros identify which series and families that the various Atmel parts belong to
oGeneral Purpose Backup Registers (GPBR)Driver for the General Purpose Backup Registers
oChip Identifier (CHIPID)
oWM8731 Audio CodecSee Quick start guide for the SAM WM8731 module
oSDRAM MT48LC16M16A2This is a configuration for the MT48LC16M16A2 SDRAM from Micron
oXMODEM transfer protocol serviceThe XMODEM transfer protocol service provides function to receive/send a file from USART/UART using XMODEM protocol
oSDRAMC - SDRAM ControllerSee Quickstart guide for SDRAMC driver.
oSAM3A/3U/3X/4E DMA Controller (DMAC) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Direct Memory Access DMA Controller (DMAC) functionality
oCAN - SN65HVD234Transceiver
oUniversal Synchronous AsynchronousReceiver Transmitter (USART)
oUniversal Synchronous Asynchronous ReceiverTransmitter (USART)
oxMessageBufferCreateMessage_buffer.h
oxMessageBufferCreateStaticMessage_buffer.h
oxMessageBufferSendMessage_buffer.h
oxMessageBufferSendFromISRMessage_buffer.h
oxMessageBufferReceiveMessage_buffer.h
oxMessageBufferReceiveFromISRMessage_buffer.h
oxMessageBufferResetMessage_buffer.h
oxMessageBufferSpaceAvailableMessage_buffer.h
oxMessageBufferSendCompletedFromISRMessage_buffer.h
oxMessageBufferReceiveCompletedFromISRMessage_buffer.h
oxQueueCreateQueue
oxQueueCreateStaticQueue
oxQueueSendQueue
oxQueueOverwriteQueue
oxQueuePeekQueue
oxQueuePeekFromISRQueue
oxQueueReceiveQueue
ouxQueueMessagesWaitingQueue
ovQueueDeleteQueue
oxQueueSendFromISRQueue
oxQueueOverwriteFromISRQueue
oxQueueReceiveFromISRQueue
oTaskHandle_tTask
otaskYIELDTask
otaskENTER_CRITICALTask
otaskEXIT_CRITICALTask
otaskDISABLE_INTERRUPTSTask
otaskENABLE_INTERRUPTSTask
oxTaskCreateTask
oxTaskCreateStaticTask
oxTaskCreateRestrictedTask
oxTaskCreateRestrictedStaticTask
ovTaskDeleteTask
ovTaskDelayTask
ovTaskDelayUntilTask
oxTaskAbortDelayTask
ouxTaskPriorityGetTask
ovTaskGetInfoTask
ovTaskPrioritySetTask
ovTaskSuspendTask
ovTaskResumeTask
ovTaskResumeFromISRTask
ovTaskStartSchedulerTask
ovTaskEndSchedulerTask
ovTaskSuspendAllTask
oxTaskResumeAllTask
oxTaskGetTickCountTask
oxTaskGetTickCountFromISRTask
ouxTaskGetNumberOfTasksTask
opcTaskGetNameTask
opcTaskGetHandleTask
ovTaskListTask
ovTaskGetRunTimeStatsTask
oxTaskNotifyTask
oxTaskNotifyWaitTask
oxTaskNotifyGiveTask
oulTaskNotifyTakeTask
oxTaskNotifyStateClearTask
oxStreamBufferCreateMessage_buffer.h
oxStreamBufferCreateStaticStream_buffer.h
oxStreamBufferSendStream_buffer.h
oxStreamBufferSendFromISRStream_buffer.h
oxStreamBufferReceiveStream_buffer.h
oxStreamBufferReceiveFromISRStream_buffer.h
ovStreamBufferDeleteStream_buffer.h
oxStreamBufferIsFullStream_buffer.h
oxStreamBufferIsEmptyStream_buffer.h
oxStreamBufferResetStream_buffer.h
oxStreamBufferSpacesAvailableStream_buffer.h
oxStreamBufferBytesAvailableStream_buffer.h
oxStreamBufferSetTriggerLevelStream_buffer.h
oxStreamBufferSendCompletedFromISRStream_buffer.h
oxStreamBufferReceiveCompletedFromISRStream_buffer.h
oxCoRoutineCreateCroutine
ovCoRoutineScheduleCroutine
ocrSTARTCroutine
ocrDELAYCroutine
ocrQUEUE_SEND
ocrQUEUE_RECEIVECroutine
ocrQUEUE_SEND_FROM_ISRCroutine
ocrQUEUE_RECEIVE_FROM_ISRCroutine
ovSemaphoreCreateBinarySemphr
oxSemaphoreCreateBinarySemphr
oxSemaphoreCreateBinaryStaticSemphr
oxSemaphoreTakeSemphr
oxSemaphoreTakeRecursiveSemphr
oxSemaphoreGiveSemphr
oxSemaphoreGiveRecursiveSemphr
oxSemaphoreGiveFromISRSemphr
oxSemaphoreCreateMutexSemphr
oxSemaphoreCreateMutexStaticSemphr
oxSemaphoreCreateRecursiveMutexSemphr
oxSemaphoreCreateRecursiveMutexStaticSemphr
oxSemaphoreCreateCountingSemphr
oxSemaphoreCreateCountingStaticSemphr
ovSemaphoreDeleteSemphr
oEventGroupAn event group is a collection of bits to which an application can assign a meaning
oWatchdog Timer (WDT)Driver for the WDT (Watchdog Timer)
oVirtual Memory in RAMThe component manages a disk on a volatile memory (internal RAM)
oController Area Network (CAN) DriverSee Quickstart guide for SAM CAN module.
oFatFS file system serviceService of FatFS file system
oGeneral Purpose Input/OutputThis is the common API for GPIO
oGeneric board supportThe generic board support module includes board-specific definitions and function prototypes, such as the board initialization function
oReal-time Timer (RTT)The Real-time Timer is built around a 32-bit counter used to count roll-over events of the programmable 16-bit prescaler, which enables counting elapsed seconds from a 32 kHz slow clock source
oMCP980X Temperature SensorSee Quickstart guide for MCP980X module
oEmbedded Flash ServiceThe Embedded Flash service provides functions for internal flash operations
oSAM3/4C/4CM/4CP/4E/4N/4S/G/V71/V70/S70/E70 Reset Controller (RSTC) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Reset Controller functionality
ovSemaphoreCreateMutexSemphr
oFreeRTOS Peripheral ControlASF specific FreeRTOS functionality that integrates ASF driver libraries with FreeRTOS services to provide a set of highly efficient peripheral interface functions
oPort of low level driver for FatFSLow level driver for FatFS
oAnalog-to-digital Converter (ADC)See Quickstart guide for SAM ADC driver
oEnhanced Embedded Flash Controller (EEFC)The Enhanced Embedded Flash Controller ensures the interface of the Flash block with the 32-bit internal bus
oAT25DFx SerialFlash component driver.See Quickstart guide for AT25DFx component.
oSAM3/4S/4L/4E/4N/4CM/4C/G Timer Counter (TC) DriverThis driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Timer Counter functionality
oTwo-Wire Interface (TWI)Driver for the TWI (Two-Wire Interface)
oUSB device descriptors for a single interfaceThe following structures provide the USB device descriptors required for USB Device with a single interface CDC
oUSB StackThis stack includes the USB Device Stack, USB Host Stack and common definitions
oMEMS Sensors - Accelerometer MMA7341LLow-level driver for the Accelerometer MMA7341L
oMatrix (MATRIX)
oTest Suite FrameworkThis module is the test suite framework, which provides a set of standard functions and macros for defining and running test suites
omaXTouch low-level componentSee Quick start guide for the maXTouch component
oStatic Memory Controller (SMC)Driver for the Static Memory Controller
oDisplay - AAT31XX ControllerLow-level driver for the AAT31XX LCD backlight controller
oILI9225 ControllerLow-level driver for the ILI9225 LCD controller
oResistive Touch ServiceThis service provides an interface for handling resistive touch component
oILI9341 Display Controller Component DriverSee Quick Start Guide for the ILI9341 Display Controller Component Driver
oDescriptors for a USB DeviceComposite
oSIO2HOST - USBThis module performs serial input/output functionalities via USB
oClock Management
oDigital-to-Analog Converter Controller (DACC)
oCOMPONENT - Display - HX8347A ControllerLow-level driver for the HX8347A LCD controller
oSupply Controller (SUPC)Driver for the SUPC (Supply Controller)
oDisplay - ILI93XX ControllerLow-level driver for the ILI93XX LCD controller
oNAND Flash on EBISee Quick start guide for the
oEthernet PhyThis is the common API for Ethernet Phy on ARMs
oGraphical display systemThis service provides an interface to drawing graphics on a graphical display
oSIO2HOST - UARTThis module performs serial input/output functionalities via UART
oSmart Card ServiceThe smart card service provides functions for cards supporting ISO7816 protocol
oResistive Touch - ADS7843 ControllerLow-level driver for the ADS7843 touch controller
opcTaskGetTaskNameTask
oMemory Control AccessCommon abstraction layer for memory interfaces
oQTouch device driver for I2C interfaceSee Quick start guide for QTouch component
oInterface with USB Device Core (UDC)Structures and functions required by UDC
oImplementation of UDI HID multi-touchClass internal implementation
oQTouch Library for AVR & AVR32 devicesThis is the QTouch Library for AVR and AVR32 devices that consists of one api header file(touch_api.h) and respective pre-compiled libraries
oLocal Interconnect Network (LIN)See Quick start guide for the SAM LIN module
oPHY component (DM9161A)Driver for the dm9161a component
oPulse Width Modulation (PWM)See Quickstart guide for SAM PWM module
oNVM serviceSee Quick Start quide for common NVM driver
oAT45dbx DataFlash component driver.This is a driver for the AT45dbX series DataFlash memories
oMemory Bag AllocatorThe Membag allocator is a optimized, fragmentationless general purpose memory allocator utility module designed to replace the standard C library malloc() and free() functions in resource constrained environments
oReal-Time Clock (RTC)See Quickstart guide for SAM RTC driver
oEthernet Media Access ControllerSee Quickstart guide for EMAC driver.
oUdi_hid_mtouch_group_udc
\Eth_phy_mii