The UDC provides a high-level abstraction of the usb device.
You can use these functions to control the main device state (start/attach/wakeup).
The following USB Device configuration must be included in the conf_usb.h file of the application.
USB_DEVICE_VENDOR_ID (Word)
Vendor ID provided by USB org (ATMEL 0x03EB).
USB_DEVICE_PRODUCT_ID (Word)
Product ID (Referenced in usb_atmel.h).
USB_DEVICE_MAJOR_VERSION (Byte)
Major version of the device
USB_DEVICE_MINOR_VERSION (Byte)
Minor version of the device
USB_DEVICE_MANUFACTURE_NAME (string)
ASCII name for the manufacture
USB_DEVICE_PRODUCT_NAME (string)
ASCII name for the product
USB_DEVICE_SERIAL_NAME (string)
ASCII name to enable and set a serial number
USB_DEVICE_POWER (Numeric)
(unit mA) Maximum device power
USB_DEVICE_ATTR (Byte)
USB attributes available:
USB_DEVICE_LOW_SPEED (Only defined)
Force the USB Device to run in low speed
USB_DEVICE_HS_SUPPORT (Only defined)
Authorize the USB Device to run in high speed
USB_DEVICE_MAX_EP (Byte)
Define the maximum endpoint number used by the USB Device.
This one is already defined in UDI default configuration. Ex:
Modules | |
USB Device Controller (UDC) - Prerequisites | |
Common prerequisites for all USB devices. | |
USB Device Controller (UDC) - Example code | |
Common example code for all USB devices. | |
USB Device Controller (UDC) - Workflow | |
Common workflow for all USB devices. | |
USB Device Descriptor | |
Implementation of UDC | |
Internal implementation. | |
Data Structures | |
struct | udc_desc_t |
Structure for USB Device Configuration Descriptor. More... | |
struct | udc_string_desc_t |
USB device string descriptor Structure used to transfer ASCII strings to USB String descriptor structure. More... | |
Functions | |
static void | udc_attach (void) |
Attach device to the bus when possible. More... | |
static void | udc_detach (void) |
Detaches the device from the bus. More... | |
usb_iface_desc_t UDC_DESC_STORAGE * | udc_get_interface_desc (void) |
Returns a pointer on the current interface descriptor. More... | |
static bool | udc_iface_disable (void) |
Disables an usb device interface (UDI) This routine call the UDI corresponding to interface number. More... | |
static bool | udc_iface_enable (void) |
Enables an usb device interface (UDI) This routine calls the UDI corresponding to the interface and setting number. More... | |
static bool | udc_include_vbus_monitoring (void) |
Authorizes the VBUS event. More... | |
bool | udc_process_setup (void) |
Main routine to manage the USB SETUP request. More... | |
static void | udc_remotewakeup (void) |
The USB driver sends a resume signal called "Upstream Resume" This is authorized only when the remote wakeup feature is enabled by host. More... | |
static bool | udc_req_iface (void) |
Send the SETUP interface request to UDI. More... | |
static bool | udc_req_std_dev_get_configuration (void) |
Standard device request to get configuration number. More... | |
static bool | udc_req_std_dev_get_descriptor (void) |
Standard device request to get descriptors about USB device. More... | |
static bool | udc_req_std_dev_get_status (void) |
Standard device request to get device status. More... | |
static bool | udc_req_std_dev_get_str_desc (void) |
Standard device request to get device string descriptor. More... | |
static bool | udc_req_std_dev_set_address (void) |
Standard device request to set device address. More... | |
static bool | udc_req_std_dev_set_configuration (void) |
Standard device request to enable a configuration. More... | |
static bool | udc_reqstd (void) |
Main routine to manage the standard USB SETUP request. More... | |
void | udc_reset (void) |
Reset the current configuration of the USB device, This routines can be called by UDD when a RESET on the USB line occurs. More... | |
void | udc_sof_notify (void) |
To signal that a SOF is occurred. More... | |
void | udc_start (void) |
Start the USB Device stack. More... | |
void | udc_stop (void) |
Stop the USB Device stack. More... | |
static void | udc_valid_address (void) |
Change the address of device Callback called at the end of request set address. More... | |
Internal variables to manage the USB device | |
static le16_t | udc_device_status |
Device status state (see enum usb_device_status in usb_protocol.h) More... | |
static uint8_t | udc_num_configuration = 0 |
Device Configuration number selected by the USB host. More... | |
UDC_DESC_STORAGE usb_dev_desc_t | udc_device_desc |
Pointer on the selected speed device configuration. More... | |
UDC_DESC_STORAGE udc_desc_t | udc_desc_fs |
USB Device Configuration Descriptor filled for FS. More... | |
Internal structure to store the USB device main strings | |
static UDC_DESC_STORAGE struct udc_string_desc_t | udc_string_desc |
static UDC_DESC_STORAGE usb_str_lgid_desc_t | udc_string_desc_languageid |
Language ID of USB device (US ID by default) More... | |
#define | USB_DEVICE_MANUFACTURE_NAME_SIZE 0 |
USB device manufacture name storage String is allocated only if USB_DEVICE_MANUFACTURE_NAME is declared by usb application configuration. More... | |
#define | USB_DEVICE_PRODUCT_NAME_SIZE 0 |
USB device product name storage String is allocated only if USB_DEVICE_PRODUCT_NAME is declared by usb application configuration. More... | |
#define | USB_DEVICE_SERIAL_NAME_SIZE 0 |
USB device serial number storage String is allocated only if USB_DEVICE_SERIAL_NAME is declared by usb application configuration. More... | |
#define USB_DEVICE_MANUFACTURE_NAME_SIZE 0 |
USB device manufacture name storage String is allocated only if USB_DEVICE_MANUFACTURE_NAME is declared by usb application configuration.
Referenced by udc_req_std_dev_get_str_desc().
#define USB_DEVICE_PRODUCT_NAME_SIZE 0 |
USB device product name storage String is allocated only if USB_DEVICE_PRODUCT_NAME is declared by usb application configuration.
Referenced by udc_req_std_dev_get_str_desc().
#define USB_DEVICE_SERIAL_NAME_SIZE 0 |
USB device serial number storage String is allocated only if USB_DEVICE_SERIAL_NAME is declared by usb application configuration.
Referenced by udc_req_std_dev_get_str_desc().
|
inlinestatic |
Attach device to the bus when possible.
References udd_attach().
|
inlinestatic |
Detaches the device from the bus.
The driver must remove pull-up on USB line D- or D+.
References udd_detach().
usb_iface_desc_t UDC_DESC_STORAGE* udc_get_interface_desc | ( | void | ) |
Returns a pointer on the current interface descriptor.
References udc_ptr_iface.
Referenced by udi_hid_reqstdifaceget_descriptor(), and udi_vendor_enable().
|
static |
Disables an usb device interface (UDI) This routine call the UDI corresponding to interface number.
iface_num | Interface number to disable |
References udi_dfu_atmel_disable().
Referenced by udc_reset().
|
static |
Enables an usb device interface (UDI) This routine calls the UDI corresponding to the interface and setting number.
iface_num | Interface number to enable |
setting_num | Setting number to enable |
References udi_dfu_atmel_enable().
Referenced by udc_req_std_dev_set_configuration().
|
inlinestatic |
Authorizes the VBUS event.
The VBus monitoring is used only for USB SELF Power application.
References udd_include_vbus_monitoring().
Referenced by run_usb_cdc_test(), run_usb_keyboard_test(), run_usb_mouse_test(), and run_usb_msc_test().
bool udc_process_setup | ( | void | ) |
Main routine to manage the USB SETUP request.
Decodes and manages a setup request.
This function parses a USB SETUP request and submits an appropriate response back to the host or, in the case of SETUP OUT requests with data, sets up a buffer for receiving the data payload.
The main standard requests defined by the USB 2.0 standard are handled internally. The interface requests are sent to UDI, and the specific request sent to a specific application callback.
Referenced by udd_ctrl_setup_received().
|
inlinestatic |
The USB driver sends a resume signal called "Upstream Resume" This is authorized only when the remote wakeup feature is enabled by host.
References udd_send_remotewakeup().
|
static |
Send the SETUP interface request to UDI.
References udi_dfu_atmel_setup().
Referenced by udc_process_setup().
|
static |
Standard device request to get configuration number.
References udc_num_configuration, and udd_set_setup_payload().
Referenced by udc_reqstd().
|
static |
Standard device request to get descriptors about USB device.
References usb_dev_desc_t::bLength, le16_to_cpu, udd_ctrl_request_t::payload_size, udd_ctrl_request_t::req, udc_device_desc, udc_req_std_dev_get_str_desc(), udd_g_ctrlreq, udd_set_setup_payload(), USB_DT_CONFIGURATION, USB_DT_DEVICE, USB_DT_STRING, usb_setup_req_t::wLength, and usb_setup_req_t::wValue.
Referenced by udc_reqstd().
|
static |
Standard device request to get device status.
References udc_device_status, and udd_set_setup_payload().
Referenced by udc_reqstd().
|
static |
Standard device request to get device string descriptor.
References usb_str_desc_t::bLength, cpu_to_le16, udc_string_desc_t::header, udd_ctrl_request_t::req, udc_string_desc_t::string, udc_string_desc, udc_string_desc_languageid, udd_g_ctrlreq, udd_set_setup_payload(), USB_DEVICE_MANUFACTURE_NAME_SIZE, USB_DEVICE_PRODUCT_NAME_SIZE, USB_DEVICE_SERIAL_NAME_SIZE, and usb_setup_req_t::wValue.
Referenced by udc_req_std_dev_get_descriptor().
|
static |
Standard device request to set device address.
References udd_ctrl_request_t::callback, udc_valid_address(), and udd_g_ctrlreq.
Referenced by udc_reqstd().
|
static |
Standard device request to enable a configuration.
References udd_ctrl_request_t::req, udc_iface_enable(), udc_num_configuration, udc_reset(), udd_g_ctrlreq, and usb_setup_req_t::wValue.
Referenced by udc_reqstd().
|
static |
Main routine to manage the standard USB SETUP request.
References usb_setup_req_t::bRequest, udd_ctrl_request_t::req, udc_req_std_dev_get_configuration(), udc_req_std_dev_get_descriptor(), udc_req_std_dev_get_status(), udc_req_std_dev_set_address(), udc_req_std_dev_set_configuration(), udd_g_ctrlreq, Udd_setup_is_in, Udd_setup_recipient, USB_REQ_GET_CONFIGURATION, USB_REQ_GET_DESCRIPTOR, USB_REQ_GET_STATUS, USB_REQ_RECIP_DEVICE, USB_REQ_SET_ADDRESS, and USB_REQ_SET_CONFIGURATION.
Referenced by udc_process_setup().
void udc_reset | ( | void | ) |
Reset the current configuration of the USB device, This routines can be called by UDD when a RESET on the USB line occurs.
Reset the UDC.
Referenced by udc_req_std_dev_set_configuration(), udc_req_std_dev_set_feature(), udc_stop(), and udd_interrupt().
void udc_sof_notify | ( | void | ) |
To signal that a SOF is occurred.
The UDC must send the signal to all UDIs enabled
Referenced by udd_interrupt().
void udc_start | ( | void | ) |
Start the USB Device stack.
Referenced by ISR(), main(), otg_dual_enable(), run_usb_cdc_test(), run_usb_keyboard_test(), run_usb_mouse_test(), run_usb_msc_test(), and stdio_usb_init().
void udc_stop | ( | void | ) |
Stop the USB Device stack.
Referenced by ISR(), main_hid_set_feature(), run_usb_cdc_test(), run_usb_keyboard_test(), run_usb_mouse_test(), and run_usb_msc_test().
|
static |
Change the address of device Callback called at the end of request set address.
References udd_ctrl_request_t::req, udd_g_ctrlreq, udd_set_address(), and usb_setup_req_t::wValue.
Referenced by udc_req_std_dev_set_address().
UDC_DESC_STORAGE udc_desc_t udc_desc_fs |
USB Device Configuration Descriptor filled for FS.
USB Device Configuration Descriptor filled for FS.
UDC_DESC_STORAGE usb_dev_desc_t udc_device_desc |
Pointer on the selected speed device configuration.
Pointer on interface descriptor used by SETUP request.
Pointer on the selected speed device configuration.
Pointer on the selected speed device configuration.
USB Device Descriptor
Referenced by udc_req_std_dev_get_descriptor().
|
static |
Device status state (see enum usb_device_status in usb_protocol.h)
Referenced by udc_req_std_dev_get_status(), and udc_reset().
|
static |
Device Configuration number selected by the USB host.
Referenced by udc_req_std_dev_get_configuration(), udc_req_std_dev_set_configuration(), and udc_reset().
|
static |
Referenced by udc_req_std_dev_get_str_desc().
|
static |
Language ID of USB device (US ID by default)
Referenced by udc_req_std_dev_get_str_desc().